Part Number: DP83TD510E
I am having problems using DP83TD510E.
Environment:
DP83TD510E works in rmii slave mode. Soc provides a 50Mhz clock to the xi pod.
CRS_DV/RX_DV Pin 18 is configured as CRS_DV (default).
Receiver with tapping at 50 Ω (Recommended).
The id of the phy chip is set to 0.
linux system from the following github link.
https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/net/phy/dp83td510.c
The DP83TD510E is always in the Link is down state, and I don't know how to deal with it. The DP83TD510E has been registered.
I tried to test Loopback Modes, but I still don't know how to handle it.