This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: 连接便携式显示器,发现HDMI信号接口有共模电压冲击,导致芯片损坏

Part Number: SN65DP159

使用SN65DP159通过HDMI连接便携式显示器,显示功能正常,但是测量发现在开机过程和关机过程HDMI的4对儿差分信号有5.6V的电压尖峰,长期导致SN65DP159损坏,加不同型号共模电感和TVS无法抑制共模电压尖峰

使用其他板卡使用其他重定时器芯片连接至该便携式显示器,测量没有电压冲击,这种情况是否和SN65DP159模式配置有关?

x 出现错误。请重试或与管理员联系。