Part Number: SN65DP159
使用SN65DP159通过HDMI连接便携式显示器,显示功能正常,但是测量发现在开机过程和关机过程HDMI的4对儿差分信号有5.6V的电压尖峰,长期导致SN65DP159损坏,加不同型号共模电感和TVS无法抑制共模电压尖峰
使用其他板卡使用其他重定时器芯片连接至该便携式显示器,测量没有电压冲击,这种情况是否和SN65DP159模式配置有关?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,抱歉回复晚了,上掉电期间不建议直接使能输出。
建议上电期间,OE拉低,输出高阻态,等上电起来稳定之后,再将OE拉高,enable输出。
同样掉电期间,先将OE拉低,再掉电。