This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: Using 941 and 948, the id of 948 can be read through the i2c of 941, but the communication of 948 i2c fails

Part Number: DS90UB941AS-Q1


1)941 initialized registers as follows

ds90ub941_single_write(ds90ub941, 0x01, 0x0F);
msleep(3);
ds90ub941_single_write(ds90ub941, 0x03, 0xBA);
ds90ub941_single_write(ds90ub941, 0x1E, 0x01);
ds90ub941_single_write(ds90ub941, 0x5B, 0x21);
ds90ub941_single_write(ds90ub941, 0x4F, 0x8C);

ds90ub941_single_write(ds90ub941, 0x40, 0x04);
ds90ub941_single_write(ds90ub941, 0x41, 0x05);
ds90ub941_single_write(ds90ub941, 0x42, 0x14);
ds90ub941_single_write(ds90ub941, 0x01, 0x00);
msleep(3);
ds90ub941_single_write(ds90ub941, 0x07, 0x54);
ds90ub941_single_write(ds90ub941, 0x08, 0x54);

2) Operation 948, read register 0 of 948, failed

ds90ub948_i2c_read: transfer failed -6
ds90ub948_check_device: Can not read ds90ub948
ds90ub948: probe of 1-002c failed with error -5

3)941 register, as follows

 0=0x34  1=0x0  2=0x0  3=0xBA  4=0x0  5=0x0  6=0x58  7=0x54  8=0x54  9=0x1  10=0x6

 11=0x0  12=0x12  13=0x30  14=0x0  15=0x0  16=0x0  17=0x0  18=0x0  19=0x8F  20=0x0

 21=0x0  22=0xFE  23=0x1E  24=0x7F  25=0x7F  26=0x1  27=0x0  28=0xD  29=0x0  30=0x1  

31=0x0  32=0xB  33=0x0  34=0x25  35=0x0  36=0x0  37=0x0  38=0x0  39=0x0  40=0x1  

41=0x20  42=0x20  43=0xA0  44=0x0  45=0x0  46=0xA5  47=0x5A  48=0x1  49=0x9  50=0x0

 51=0x5  52=0xC  53=0x0  54=0x0  55=0x0  56=0x0  57=0x0  58=0x0  59=0x0  60=0x0  

61=0x0  62=0x81  63=0x2  64=0x4  65=0x5  66=0x14  67=0x0  68=0x0  69=0x0  70=0x0  

71=0x0  72=0x0  73=0x0  74=0x0  75=0x0  76=0x0  77=0x0  78=0x0  79=0x8C  80=0x16

 81=0x0  82=0x0  83=0x0  84=0x2  85=0x10  86=0x0  87=0x2  88=0x0  89=0x0  90=0x2

 91=0x61  92=0x7  93=0x6  94=0x44  95=0x0  96=0x22  97=0x2  98=0x0  99=0x0  100=0x5

 101=0xC  102=0xE  103=0x0  104=0x0  105=0x0  106=0x0  107=0x0  108=0x0  109=0x0  110=0x20

 111=0x0  112=0x0  113=0x0  114=0x0  115=0x0  116=0x0  117=0x0  118=0x0  119=0x0  120=0x0

 121=0x0  122=0x0  123=0x0  124=0x0  125=0x0  126=0x0  127=0x0  128=0x0  129=0x0  130=0x0

 131=0x0  132=0x0  133=0x0  134=0x0  135=0x0  136=0x0  137=0x0  138=0x0  139=0x0  140=0x0

 141=0x0  142=0x0  143=0x0  144=0x0  145=0x0  146=0x0  147=0x0  148=0x0  149=0x0  150=0x0

 151=0x0  152=0x0  153=0x0  154=0x0  155=0x0  156=0x0  157=0x0  158=0x0  159=0x0  160=0x0

 161=0x0  162=0x0  163=0x0  164=0x0  165=0x0  166=0x0  167=0x0  168=0x0  169=0x0  170=0x0

 171=0x0  172=0x0  173=0x0  174=0x0  175=0x0  176=0x0  177=0x0  178=0x0  179=0x0  180=0x0

 181=0x0  182=0x0  183=0x0  184=0x0  185=0x0  186=0x0  187=0x0  188=0x0  189=0x0  190=0x0

 191=0x0  192=0x0  193=0x0  194=0x82  195=0x0  196=0x50  197=0x0  198=0x0  199=0x44  200=0x40

 201=0x0  202=0x0  203=0x0  204=0x0  205=0x2  206=0xFF  207=0x0  208=0x0  209=0x0  210=0x0

 211=0x0  212=0x0  213=0x0  214=0x0  215=0x0  216=0x0  217=0x0  218=0x0  219=0x0  220=0x0

 221=0x0  222=0x0  223=0x0  224=0x0  225=0x0  226=0x82  227=0x0  228=0x40  229=0x8  230=0x0

 231=0x0  232=0x0  233=0x0  234=0x0  235=0x0  236=0x0  237=0x2  238=0x0  239=0x0  240=0x5F

241=0x55  242=0x42  243=0x39  244=0x34  245=0x31