This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1..输入的差分信号微单载波形式的信号,可作为芯片REF_IN的输入吗?
A: 可以,如果输入信号为单端信号,REF_IN 可以通过1Kohm电阻下拉到地。
2. 输入信号满足差分输入范围,但是不是严格的LVDS,LVPECL,LVCMOS信号,可行吗?
A: 差分输入只要满足Differental Input amplitude, (VIN+ – VIN–)为0.1V~1.3V的范围即可,不一定是严格的LVDS,LVPECL。
3.图中差分输入范围(VIN+—VIN-)表示的是单臂信号线上电平的摆幅VOD吗,即下图中400mV所示?差分后的摆幅(P-N)VPP=2VOD的关系对吗?
A: 是的,以LVDS为例,Vod即为400mV,Vpp=2Vod=800mV.
1.由于不同的电平标准之间需要一定的端接,满足输入范围信号能够直接接入,还需要设计端接电阻吗?
A: 由于CDCE62002输入内部没有端接,所以需要设计端接电阻,比如LVDS输入时,需要端接100ohm电阻。
1.满足差分输入范围的话,这种正弦波作为输入可行吗?
A:我认为只要满足差分输入范围即可。
2. 因为10M单载波功率可调,所以可以调整输入信��的摆幅(Vmax-Vmin),如果不作调整,这2bit怎么定义?
A,看了下,这两个bit设置是为了设置内部偏置Vbb电压的,像你这种情况,可以设置为00,或者是TERMSEL=1,也就是说,这两个bit无论怎么设置,内部输入buffer部分的终端电阻disable。 因为之前没遇到过你这种情况,最好先实验验证下。
非常感谢,现在就是给FPGA设计一个200M时钟(LVPECL,LVDS);
1.CDCE62002是WEBENCH给出的方案之一,对于这种正弦波信号,通常TI时钟的处理采用什么样的芯片?
demo上的参考输入应该是直接满足输入端的共模输入电压要求的,所以直接交流耦合,不需要外部偏置。
1.即使外部参考输入有合适的共模电平,但是通过AC耦合电容之后,不是将直流偏置给虑除了?
2.我的意思是,DEMO中的参考设计通过设置片上VBB来控制VCM的范围?