This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.框图中的2.5V的如何产生的,是否可以提供来源框图,若2.5V仅为CANH和CANL的共模电压,隐性时,上下MOS关闭,CANH和CANL为什么会有2.5V的电压呢?2.5V到CANH/CANL的电阻大概是多大呢
2.波形图黄色为CANH/绿色为CANL/蓝色为VCC供电,该图是将CANH短路到16.5V电源上的瞬间波形。此时CANL被下拉至约13V,根据芯片内部框图,CANL只是接到了一个二极管和MOS到地,是如何产生13V的电压的,是由于还有其他电阻未在框图画出,还是说是此时的MOS进入了放大区的状态?
3.根据CAN的标准,当显性电平时,CANH为3.5V,CANL为1.5V,但MOS饱和导通电压一般为0.25V,此时是否MOS也工作在放大区?
4.CANL短16.5V电源时,CAN芯片会检测到过流状态,使上下MOS会关闭,之后是由于CAN控制器检测到相应错误,关闭输出,还是CAN芯片一直在做过流保护,使MOS关闭
您好,
1.有一个单独的接收器偏置电路,在您分享的图表中没有显示。它本质上是一个来自VCC的电阻网络,用于将CAN总线偏置到VCC/2。它比数据表中显示的高级电路和我可以分享的图表复杂得多,但它不仅仅基于框图中显示的总线驱动器电路。
2.一旦发生16.5V短路,内部电路将根据CAN总线的电压设置共模。如果存在短路,则共模电压将偏移到该电压,并且主导位将基于该电压被驱动。
3.是的,但请记住,正如我之前所说,框图是对真实电路的高级估计。你可以假设MOS上大约有1V的压降,二极管上大约有0.5V的压降。不过,这些都是粗略的估计,电压不会完全达到这些水平。
4.在大多数CAN收发器中,都有过电流限制,在数据表中列为Ios。与此同时,如果过电流导致温度升高,设备将因过热而停机。