Part Number: TCAN1042-Q1



1.框图中的2.5V的如何产生的,是否可以提供来源框图,若2.5V仅为CANH和CANL的共模电压,隐性时,上下MOS关闭,CANH和CANL为什么会有2.5V的电压呢?2.5V到CANH/CANL的电阻大概是多大呢
2.波形图黄色为CANH/绿色为CANL/蓝色为VCC供电,该图是将CANH短路到16.5V电源上的瞬间波形。此时CANL被下拉至约13V,根据芯片内部框图,CANL只是接到了一个二极管和MOS到地,是如何产生13V的电压的,是由于还有其他电阻未在框图画出,还是说是此时的MOS进入了放大区的状态?
3.根据CAN的标准,当显性电平时,CANH为3.5V,CANL为1.5V,但MOS饱和导通电压一般为0.25V,此时是否MOS也工作在放大区?
4.CANL短16.5V电源时,CAN芯片会检测到过流状态,使上下MOS会关闭,之后是由于CAN控制器检测到相应错误,关闭输出,还是CAN芯片一直在做过流保护,使MOS关闭