This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: ds90UB943AS

Part Number: DS90UB941AS-Q1


链路: soc - 943+948 - dp

问题:偶现闪屏,且闪屏时会出现界面偏移

详细描述:所用timing自刷图是OK的,然后用此timing写入发现偶现闪屏,其中pclk经计算正常

想要get间接寄存器的值 但是获取的一值是0,应该是我方式不对

其中界面偏移的图片如下:

在不闪屏时 无偏移

  • 您好!

    谁是客户 Tier1/EOM
    这是哪个项目?
    有多少系统出现了此问题?
    故障率是多少?
    这是上电问题还是运行时问题(一段时间后发生?)
    您当前正在使用哪个脚本生成版本?
    您在使用哪种 SoC?
    请发送 SERDES 初始化代码以供审核。

  • 您好,


    我这边是移远 +t1四维+主机厂大通 共同咨询此问题

    这个是大通的项目

    目前有多个车机系统出现这个问题,非一个

    上电时就开始发生闪屏

    当前使用版本未知,但我直接提供了pll的设置

    使用的是6125芯片

     SERDES 初始化代码如下:

    ////////////////////////////////////////////////////////////////////////////.ds90ub943_apb_config

    REG_VALUE3(serAddr,0x01,0x40);

    REG_VALUE3(serAddr,0x48,0x1); //Enable APB Interface
    REG_VALUE3(serAddr,0x49,0x0); //Force HPD low to configure 983 DP settings
    REG_VALUE3(serAddr,0x4a,0x0);
    REG_VALUE3(serAddr,0x4b,0x0);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    REG_VALUE3(serAddr,0x49,0x74); //Set max advertised link rate = 2.7Gbps
    REG_VALUE3(serAddr,0x4a,0x0);
    REG_VALUE3(serAddr,0x4b,link_rate);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    REG_VALUE3(serAddr,0x49,0x70); //Set max advertised lane count = 2
    REG_VALUE3(serAddr,0x4a,0x0);
    REG_VALUE3(serAddr,0x4b,link_lanes);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    REG_VALUE3(serAddr,0x49,0x14); //Request min VOD swing of 0x02
    REG_VALUE3(serAddr,0x4a,0x2);
    REG_VALUE3(serAddr,0x4b,0x2);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    REG_VALUE3(serAddr,0x49,0x18); //Set SST/MST mode and DP/eDP Mode
    REG_VALUE3(serAddr,0x4a,0x0);
    REG_VALUE3(serAddr,0x4b,0x14);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    REG_VALUE3(serAddr,0x49,0x0); //Force HPD high to trigger link training
    REG_VALUE3(serAddr,0x4a,0x0);
    REG_VALUE3(serAddr,0x4b,0x1);
    REG_VALUE3(serAddr,0x4c,0x0);
    REG_VALUE3(serAddr,0x4d,0x0);
    REG_VALUE3(serAddr,0x4e,0x0);

    //////////////////////////////////////////////////////////////////////////.ds90ub943_set_port_config

    REG_VALUE3(serAddr,0x07,0x89); // Set FPD III Mode
    REG_VALUE3(serAddr,0x05,0x80); // Set FPD III Mode
    REG_VALUE3(serAddr,0x59,0x3);

    ////////////////////////////////////////////////////////////////////////.ds90ub943_set_pll_config

    den=16776936

    num=6617569

    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x05),
    REG_VALUE3(serAddr, 0x42, 0x74), //#write to register 0x05
    REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x06
    //#Denominator set to 16776990
    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x18),
    REG_VALUE3(serAddr, 0x42, (den>>0)&0xff), //#write to register 0x18
    REG_VALUE3(serAddr, 0x42, (den>>8)&0xff), //#write to register 0x19
    REG_VALUE3(serAddr, 0x42, (den>>16)&0xff), //#write to register 0x1a
    //#Numerator set to 1180603
    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x1e),
    REG_VALUE3(serAddr, 0x42, (num>>0)&0xff), //#write to register 0x1e
    REG_VALUE3(serAddr, 0x42, (num>>8)&0xff), //#write to register 0x1f
    REG_VALUE3(serAddr, 0x42, (num>>16)&0xff), //#write to register 0x20
    //#Post-divider set to 8 and auto VCO selection enabled
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x13),
    REG_VALUE3(serAddr, 0x42, 0xf0), //#write to register 0x13 default auto
    //#SSCG disabled
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x17),
    REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x17
    //#SSCG spread type set to center-spread (required when SSCG is disabled),
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x14),
    REG_VALUE3(serAddr, 0x42, 0x80), //#write to register 0x14
    //#PLL order set to fractional
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x04),
    REG_VALUE3(serAddr, 0x42, 0x09), //#write to register 0x04

    //#Programs FPD-Link PLL for 98x device to 1.567 Gbps (PCLK is 44.770 MHz),
    //#PLL script revision: 0
    //#Configuring PLL1 (Port 1),
    //#uses fixed I2C address

    //#N-divider set to 116
    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x45),
    REG_VALUE3(serAddr, 0x42, 0x74), //#write to register 0x45
    REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x46
    //#Denominator set to 16776990
    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x58),
    REG_VALUE3(serAddr, 0x42, (den>>0)&0xff), //#write to register 0x18
    REG_VALUE3(serAddr, 0x42, (den>>8)&0xff), //#write to register 0x19
    REG_VALUE3(serAddr, 0x42, (den>>16)&0xff), //#write to register 0x1a
    //#Numerator set to 1180603
    REG_VALUE3(serAddr, 0x40, 0x0a),
    REG_VALUE3(serAddr,0x41, 0x5e),
    REG_VALUE3(serAddr, 0x42, (num>>0)&0xff), //#write to register 0x1e
    REG_VALUE3(serAddr, 0x42, (num>>8)&0xff), //#write to register 0x1f
    REG_VALUE3(serAddr, 0x42, (num>>16)&0xff), //#write to register 0x20
    //#Post-divider set to 8 and auto VCO selection enabled
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x53),
    REG_VALUE3(serAddr, 0x42, 0xf0), //#write to register 0x53
    //#SSCG disabled
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x57),
    REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x57
    //#SSCG spread type set to center-spread (required when SSCG is disabled),
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x54),
    REG_VALUE3(serAddr, 0x42, 0x80), //#write to register 0x54
    //#PLL order set to fractional
    REG_VALUE3(serAddr, 0x40, 0x08),
    REG_VALUE3(serAddr,0x41, 0x44),
    REG_VALUE3(serAddr, 0x42, 0x09), //#write to register 0x44


    REG_VALUE3(serAddr,0x1,0x30); //PLL Reset
    MSLEEP(10);
    REG_VALUE3(serAddr,0x40,0x4); //Set FPD Page to configure BC Settings for Port 0 and Port 1
    REG_VALUE3(serAddr,0x41,0x6);
    REG_VALUE3(serAddr,0x42,0xff);
    REG_VALUE3(serAddr,0x41,0xd);
    REG_VALUE3(serAddr,0x42,0x70);
    REG_VALUE3(serAddr,0x41,0xe);
    REG_VALUE3(serAddr,0x42,0x70);
    REG_VALUE3(serAddr,0x41,0x26);
    REG_VALUE3(serAddr,0x42,0xff);
    REG_VALUE3(serAddr,0x41,0x2d);
    REG_VALUE3(serAddr,0x42,0x70);
    REG_VALUE3(serAddr,0x41,0x2e);
    REG_VALUE3(serAddr,0x42,0x70);
    REG_VALUE3(serAddr,0x1,0x30); //Reset PLLs

    ////////////////////////////////////////////////////////////////////ds90ub943_set_vp_timing

    REG_VALUE3(serAddr,0x40,0x32);
    REG_VALUE3(serAddr,0x41,0x1);
    REG_VALUE3(serAddr,0x42,0x20); //Set VP_SRC_SELECT to Stream 0 for SST Mode
    REG_VALUE3(serAddr,0x41,0x2);
    REG_VALUE3(serAddr,0x42,0x80); //VID H Active
    REG_VALUE3(serAddr,0x42,0x7); //VID H Active
    REG_VALUE3(serAddr,0x41,0x10);
    REG_VALUE3(serAddr,0x42,0x80); //Horizontal Active
    REG_VALUE3(serAddr,0x42,0x7); //Horizontal Active
    REG_VALUE3(serAddr,0x42,0x30); //Horizontal Back Porch
    REG_VALUE3(serAddr,0x42,0x0); //Horizontal Back Porch
    REG_VALUE3(serAddr,0x42,0x28); //Horizontal Sync
    REG_VALUE3(serAddr,0x42,0x0); //Horizontal Sync
    REG_VALUE3(serAddr,0x42,0x8); //Horizontal Total
    REG_VALUE3(serAddr,0x42,0x8); //Horizontal Total
    REG_VALUE3(serAddr,0x42,0xd0); //Vertical Active
    REG_VALUE3(serAddr,0x42,0x2); //Vertical Active
    REG_VALUE3(serAddr,0x42,0x2); //Vertical Back Porch
    REG_VALUE3(serAddr,0x42,0x0); //Vertical Back Porch
    REG_VALUE3(serAddr,0x42,0x2); //Vertical Sync
    REG_VALUE3(serAddr,0x42,0x0); //Vertical Sync
    REG_VALUE3(serAddr,0x42,0x4); //Vertical Front Porch
    REG_VALUE3(serAddr,0x42,0x0); //Vertical Front Porch
    REG_VALUE3(serAddr,0x41,0x27);
    REG_VALUE3(serAddr,0x42,0x06); //HSYNC Polarity = -, VSYNC Polarity = -

    ///////////////////////////////////////////////////////////////////////ds90ub943_enable_vp

    REG_VALUE3(serAddr,0x43,0x0); //Set number of VPs used = 1
    REG_VALUE3(serAddr,0x44,0x1); //Enable video processors

    ////////////////////////////////////////////////////////////////////////////ds90ub943_set_stream

    REG_VALUE3(serAddr,0x2d,0x1); //Select FPD TX Port 0
    REG_VALUE3(serAddr,0x57,0x0); //Set FPD TX Port 0 Stream Source = VP0
    REG_VALUE3(serAddr,0x2d,0x12); //Select FPD TX Port 1
    REG_VALUE3(serAddr,0x57,0x0); //Set FPD TX Port 1 Stream Source = VP0

    REG_VALUE3(serAddr,0x5b,0x2b); //Enable FPD III FIFO

    REG_VALUE3(serAddr,0x2,0xf0); //CRC Error Reset
    REG_VALUE3(serAddr,0x2,0xd1); //CRC Error Reset Clear
    REG_VALUE3(serAddr,0x2d,0x1);

  • 您好!

    您能否提供此处使用的视频时序?

    THW[0] = ?
    TVW[0] = ?
    AHW[0] = ?
    AVW[0] = ?
    HBP[0] = ?
    VBP[0] = ?
    HSW[0] = ?
    VSW[0] = ?
    HFP[0] = ?
    VFP[0] = ?
    HSP[0] = ?
    VSP[0] = ?
    PCLK[0] =?
    Bits_per_pixel[0] = ?

    这是单路还是双路 FPD 模式? 这里的 FPD 比率是多少?
    您是否尝试过运行 SERDES Patgen? 相同的问题是出现在 SER 和 DES PATGEN 中还是仅出现在 SoC 视频中?
    您发现此问题的频率如何? 总是、有时、很少?