Part Number: DS90UB941AS-Q1
链路: soc - 943+948 - dp
问题:偶现闪屏,且闪屏时会出现界面偏移
详细描述:所用timing自刷图是OK的,然后用此timing写入发现偶现闪屏,其中pclk经计算正常
想要get间接寄存器的值 但是获取的一值是0,应该是我方式不对
其中界面偏移的图片如下:


在不闪屏时 无偏移
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
链路: soc - 943+948 - dp
问题:偶现闪屏,且闪屏时会出现界面偏移
详细描述:所用timing自刷图是OK的,然后用此timing写入发现偶现闪屏,其中pclk经计算正常
想要get间接寄存器的值 但是获取的一值是0,应该是我方式不对
其中界面偏移的图片如下:


在不闪屏时 无偏移
您好!
谁是客户 Tier1/EOM
这是哪个项目?
有多少系统出现了此问题?
故障率是多少?
这是上电问题还是运行时问题(一段时间后发生?)
您当前正在使用哪个脚本生成版本?
您在使用哪种 SoC?
请发送 SERDES 初始化代码以供审核。
您好,
我这边是移远 +t1四维+主机厂大通 共同咨询此问题
这个是大通的项目
目前有多个车机系统出现这个问题,非一个
上电时就开始发生闪屏
当前使用版本未知,但我直接提供了pll的设置
使用的是6125芯片
SERDES 初始化代码如下:
////////////////////////////////////////////////////////////////////////////.ds90ub943_apb_config
REG_VALUE3(serAddr,0x01,0x40);
REG_VALUE3(serAddr,0x48,0x1); //Enable APB Interface
REG_VALUE3(serAddr,0x49,0x0); //Force HPD low to configure 983 DP settings
REG_VALUE3(serAddr,0x4a,0x0);
REG_VALUE3(serAddr,0x4b,0x0);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
REG_VALUE3(serAddr,0x49,0x74); //Set max advertised link rate = 2.7Gbps
REG_VALUE3(serAddr,0x4a,0x0);
REG_VALUE3(serAddr,0x4b,link_rate);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
REG_VALUE3(serAddr,0x49,0x70); //Set max advertised lane count = 2
REG_VALUE3(serAddr,0x4a,0x0);
REG_VALUE3(serAddr,0x4b,link_lanes);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
REG_VALUE3(serAddr,0x49,0x14); //Request min VOD swing of 0x02
REG_VALUE3(serAddr,0x4a,0x2);
REG_VALUE3(serAddr,0x4b,0x2);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
REG_VALUE3(serAddr,0x49,0x18); //Set SST/MST mode and DP/eDP Mode
REG_VALUE3(serAddr,0x4a,0x0);
REG_VALUE3(serAddr,0x4b,0x14);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
REG_VALUE3(serAddr,0x49,0x0); //Force HPD high to trigger link training
REG_VALUE3(serAddr,0x4a,0x0);
REG_VALUE3(serAddr,0x4b,0x1);
REG_VALUE3(serAddr,0x4c,0x0);
REG_VALUE3(serAddr,0x4d,0x0);
REG_VALUE3(serAddr,0x4e,0x0);
//////////////////////////////////////////////////////////////////////////.ds90ub943_set_port_config
REG_VALUE3(serAddr,0x07,0x89); // Set FPD III Mode
REG_VALUE3(serAddr,0x05,0x80); // Set FPD III Mode
REG_VALUE3(serAddr,0x59,0x3);
////////////////////////////////////////////////////////////////////////.ds90ub943_set_pll_config
den=16776936
num=6617569
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x05),
REG_VALUE3(serAddr, 0x42, 0x74), //#write to register 0x05
REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x06
//#Denominator set to 16776990
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x18),
REG_VALUE3(serAddr, 0x42, (den>>0)&0xff), //#write to register 0x18
REG_VALUE3(serAddr, 0x42, (den>>8)&0xff), //#write to register 0x19
REG_VALUE3(serAddr, 0x42, (den>>16)&0xff), //#write to register 0x1a
//#Numerator set to 1180603
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x1e),
REG_VALUE3(serAddr, 0x42, (num>>0)&0xff), //#write to register 0x1e
REG_VALUE3(serAddr, 0x42, (num>>8)&0xff), //#write to register 0x1f
REG_VALUE3(serAddr, 0x42, (num>>16)&0xff), //#write to register 0x20
//#Post-divider set to 8 and auto VCO selection enabled
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x13),
REG_VALUE3(serAddr, 0x42, 0xf0), //#write to register 0x13 default auto
//#SSCG disabled
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x17),
REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x17
//#SSCG spread type set to center-spread (required when SSCG is disabled),
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x14),
REG_VALUE3(serAddr, 0x42, 0x80), //#write to register 0x14
//#PLL order set to fractional
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x04),
REG_VALUE3(serAddr, 0x42, 0x09), //#write to register 0x04
//#Programs FPD-Link PLL for 98x device to 1.567 Gbps (PCLK is 44.770 MHz),
//#PLL script revision: 0
//#Configuring PLL1 (Port 1),
//#uses fixed I2C address
//#N-divider set to 116
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x45),
REG_VALUE3(serAddr, 0x42, 0x74), //#write to register 0x45
REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x46
//#Denominator set to 16776990
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x58),
REG_VALUE3(serAddr, 0x42, (den>>0)&0xff), //#write to register 0x18
REG_VALUE3(serAddr, 0x42, (den>>8)&0xff), //#write to register 0x19
REG_VALUE3(serAddr, 0x42, (den>>16)&0xff), //#write to register 0x1a
//#Numerator set to 1180603
REG_VALUE3(serAddr, 0x40, 0x0a),
REG_VALUE3(serAddr,0x41, 0x5e),
REG_VALUE3(serAddr, 0x42, (num>>0)&0xff), //#write to register 0x1e
REG_VALUE3(serAddr, 0x42, (num>>8)&0xff), //#write to register 0x1f
REG_VALUE3(serAddr, 0x42, (num>>16)&0xff), //#write to register 0x20
//#Post-divider set to 8 and auto VCO selection enabled
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x53),
REG_VALUE3(serAddr, 0x42, 0xf0), //#write to register 0x53
//#SSCG disabled
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x57),
REG_VALUE3(serAddr, 0x42, 0x00), //#write to register 0x57
//#SSCG spread type set to center-spread (required when SSCG is disabled),
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x54),
REG_VALUE3(serAddr, 0x42, 0x80), //#write to register 0x54
//#PLL order set to fractional
REG_VALUE3(serAddr, 0x40, 0x08),
REG_VALUE3(serAddr,0x41, 0x44),
REG_VALUE3(serAddr, 0x42, 0x09), //#write to register 0x44
REG_VALUE3(serAddr,0x1,0x30); //PLL Reset
MSLEEP(10);
REG_VALUE3(serAddr,0x40,0x4); //Set FPD Page to configure BC Settings for Port 0 and Port 1
REG_VALUE3(serAddr,0x41,0x6);
REG_VALUE3(serAddr,0x42,0xff);
REG_VALUE3(serAddr,0x41,0xd);
REG_VALUE3(serAddr,0x42,0x70);
REG_VALUE3(serAddr,0x41,0xe);
REG_VALUE3(serAddr,0x42,0x70);
REG_VALUE3(serAddr,0x41,0x26);
REG_VALUE3(serAddr,0x42,0xff);
REG_VALUE3(serAddr,0x41,0x2d);
REG_VALUE3(serAddr,0x42,0x70);
REG_VALUE3(serAddr,0x41,0x2e);
REG_VALUE3(serAddr,0x42,0x70);
REG_VALUE3(serAddr,0x1,0x30); //Reset PLLs
////////////////////////////////////////////////////////////////////ds90ub943_set_vp_timing
REG_VALUE3(serAddr,0x40,0x32);
REG_VALUE3(serAddr,0x41,0x1);
REG_VALUE3(serAddr,0x42,0x20); //Set VP_SRC_SELECT to Stream 0 for SST Mode
REG_VALUE3(serAddr,0x41,0x2);
REG_VALUE3(serAddr,0x42,0x80); //VID H Active
REG_VALUE3(serAddr,0x42,0x7); //VID H Active
REG_VALUE3(serAddr,0x41,0x10);
REG_VALUE3(serAddr,0x42,0x80); //Horizontal Active
REG_VALUE3(serAddr,0x42,0x7); //Horizontal Active
REG_VALUE3(serAddr,0x42,0x30); //Horizontal Back Porch
REG_VALUE3(serAddr,0x42,0x0); //Horizontal Back Porch
REG_VALUE3(serAddr,0x42,0x28); //Horizontal Sync
REG_VALUE3(serAddr,0x42,0x0); //Horizontal Sync
REG_VALUE3(serAddr,0x42,0x8); //Horizontal Total
REG_VALUE3(serAddr,0x42,0x8); //Horizontal Total
REG_VALUE3(serAddr,0x42,0xd0); //Vertical Active
REG_VALUE3(serAddr,0x42,0x2); //Vertical Active
REG_VALUE3(serAddr,0x42,0x2); //Vertical Back Porch
REG_VALUE3(serAddr,0x42,0x0); //Vertical Back Porch
REG_VALUE3(serAddr,0x42,0x2); //Vertical Sync
REG_VALUE3(serAddr,0x42,0x0); //Vertical Sync
REG_VALUE3(serAddr,0x42,0x4); //Vertical Front Porch
REG_VALUE3(serAddr,0x42,0x0); //Vertical Front Porch
REG_VALUE3(serAddr,0x41,0x27);
REG_VALUE3(serAddr,0x42,0x06); //HSYNC Polarity = -, VSYNC Polarity = -
///////////////////////////////////////////////////////////////////////ds90ub943_enable_vp
REG_VALUE3(serAddr,0x43,0x0); //Set number of VPs used = 1
REG_VALUE3(serAddr,0x44,0x1); //Enable video processors
////////////////////////////////////////////////////////////////////////////ds90ub943_set_stream
REG_VALUE3(serAddr,0x2d,0x1); //Select FPD TX Port 0
REG_VALUE3(serAddr,0x57,0x0); //Set FPD TX Port 0 Stream Source = VP0
REG_VALUE3(serAddr,0x2d,0x12); //Select FPD TX Port 1
REG_VALUE3(serAddr,0x57,0x0); //Set FPD TX Port 1 Stream Source = VP0
REG_VALUE3(serAddr,0x5b,0x2b); //Enable FPD III FIFO
REG_VALUE3(serAddr,0x2,0xf0); //CRC Error Reset
REG_VALUE3(serAddr,0x2,0xd1); //CRC Error Reset Clear
REG_VALUE3(serAddr,0x2d,0x1);
您好!
您能否提供此处使用的视频时序?
THW[0] = ?
TVW[0] = ?
AHW[0] = ?
AVW[0] = ?
HBP[0] = ?
VBP[0] = ?
HSW[0] = ?
VSW[0] = ?
HFP[0] = ?
VFP[0] = ?
HSP[0] = ?
VSP[0] = ?
PCLK[0] =?
Bits_per_pixel[0] = ?
这是单路还是双路 FPD 模式? 这里的 FPD 比率是多少?
您是否尝试过运行 SERDES Patgen? 相同的问题是出现在 SER 和 DES PATGEN 中还是仅出现在 SoC 视频中?
您发现此问题的频率如何? 总是、有时、很少?