Hello Team,
I am using TCAN1145EVM, could you please share sample c code.
Thanks and regards
Hello Team,
I am using TCAN1145EVM, could you please share sample c code.
Thanks and regards
I control the CANFD chip with the DSP28335 and send 5 packets of data to the outside, with the following corresponding cycle and frame ID: 0x11A, 10ms cycle; 0x11C, 20ms cycle; 0x50D, 1280ms cycle; 0x6F5, 1280ms cycle; 0x6F7…
条件:
车上CAN总线有一百多个ID,当有新的消息存进RX FIFI 0的时候,掉用TCAN4x5x_MCAN_ReadNextFIFO读取数据,读回来的MsgHeader.ID和dataPayload的数可能会对应不上,也就是收到MsgHeader.ID是ID(A),但是dataPayload可能是data(B)或者其他ID的数据,我想尝试用过滤ID的方法解决这个问题,但是过滤器没起作用,我任然能收到CAN总线上的所有ID。
使用TCAN1044ADRQ1芯片进行CAN 通信,发现1M 可以测试通过,5M,8M 无法测试通过,请帮忙分析一下原因
断开另一端的CAN 抓取波形如下:
在1M 数据下可以正常通信