在使用sigcon配置完器件后,在EEPROM配置界面点击update slot from device后,导出HEX文件。将HEX文件写入外部EEPROM并将器件配置为SMBus slave mode,重新上下电后发现器件加载的配置与原本设计的配置不同,应该如何正确导出HEX文件?
在使用sigcon配置完器件后,在EEPROM配置界面点击update slot from device后,导出HEX文件。将HEX文件写入外部EEPROM并将器件配置为SMBus slave mode,重新上下电后发现器件加载的配置与原本设计的配置不同,应该如何正确导出HEX文件?
您好!
我们的设计方案如下,出现问题是屏幕接在948-1口就可以正常点亮,接在948-2就电不亮且在948-2口一直在显示红、蓝和白的颜色跳变,请帮忙看看是什么问题?
测试过把DSI0和DSI1交换,还是948-2无法正常显示DSI的输出图像,只显示红、蓝和白的跳变;
Dear TI
目前我们采用UH983一拖二接两个UB948的方案,
其中Port0的分辨率为1920×480,Port1的分辨率为1280×720,我们想咨询一下这种情况超级帧应该怎么配置?可以允许Port0的宽比Port1小吗?
我们采用ALP_98XPROFILE_UPDATE_v03.zip对ALP进行更新,但是打开UH…
背景:
有12.9寸屏:PCLK 136Mhz,DE屏
15寸屏: PCLK 178Mhz ,sync HV屏
高通SOC 8155输出DSI,DS90UB941AS-Q1匹配948芯片,15寸屏使用refer clk显示出现水波纹。(外部时钟是LMK3H0102)
941的外部时钟jitter要求0.28UI的要求:88pS。外部时钟的jitter max…
TI专家们好:
附件是RGB 24位转LVDS的图纸,请帮忙审查一下。
其中有个问题需要咨询,规格书参考设计RGB信号需要4.7K上拉,但是我在论坛查找相关说明,似乎不需要上拉,这个具体怎么确定?
另外图纸问题帮忙审核下。Dashboard_V1.pdf
您好!
使用的TCA9546APWR芯片,在使用时想要查看开关切换到通道几了 ,去读取0x00返回的还是00不正常,我切换通道使用却又都是正常,且我写入0x00寄存器也正常,这是为什么?
I found the MDI design requirement in the schematic checklist for DP83TC812S
1.termination resistor is recommended as 1kohm , 0.75W -> in the open alliance the power rate is 0.4W , I want to know which test requires the…
steps for reproduce the failure:
1,configure the system into sleep mode
2,reduce power supply to 0
3,power supply increase again above UVsup
4,the LDO ramping up is not observed as marked in state machine , RST is also keep low…
When conducting communication tests, there is a chance that 988 will not forward IIC messages. When we separately connect the IIC tool to 988 and the MCU, the tool can send messages to the MCU. Therefore, it is determined that…
We want to try to use External Reference Clock Mode mode to light up the display on the DS90UB941 (the Ref Clk clock source comes from OUTPUT0 of the LMK3H0102-Q1 chip…
您好:
我们正在调试983的链路训练功能,发现CR训练有很大概率的训练失败,导致EQ也会训练失败。请问这个会是什么原因导致的呢?这个有什么办法解决和规避吗?我们使用的是8.1Gbps 4-lane工作模式。
The usb 2.0 hub design is follow TUSB4041PAPEVM Schematic. And use the external eeprom for PID/VID setting. The eeprom bin file is showed as picture.
In our application, the Host is the Mac mini (mac OS system). The hub is…
参考《National Semiconductor Ethernet PHYTER Software Development Guide》文档,首先通过写DP83640 0x13寄存器的值为0x5 选中page5,然后再写0x14寄存器的值为0xC201,配置完成后,使用示波器测量GPIO2管脚无PPS输出。
请教下各位老师,除上述寄存器配置外,还需要配置其他寄存器吗?
PS:目前通过通过写DP83640 0x1C寄存器的值为0x0,CLK_OUT管脚是有25MHz频率输出的…
1:根据这份文件Application Report SLLA314,USB信号线TI建议串联阻抗匹配电阻,请问TUSB2046BI这颗HUB的内阻多大?需要串联多大阻值的电阻?谢谢!
2:请问晶体的频率是否只能选择6MHz这个频率?我们的空间有限,6MHz的晶体体积过大。其他比如8MHz、12MHz是否可以?
在TCAN1043A-Q1启动时必须按照图上的步骤,先拉高nSTB从standby模式进入Silent模式吗?直接将nSTB和EN同时拉高使之进入正常模式不行吗?
在远端唤醒时,为什么要先进入Silent模式再去读取nFAULT,那么如果我在Standby模式下,我怎么知道发生了远端唤醒,然后将nSTB拉高进入Silent模式。
你好,有几个问题需要您解答
1、SN65C3222EPWR是否可以替代MAX3222
2、实际使用此芯片时,波特率设置为921600,通信大概半小时后,开始出现错误码,请问有可能是什么原因
Hi:
Can you please provide the PCB design files for the XIO2001EVM reference design? We are targeting the ZWS169 package.
Thanks.
Hi team:
If my design does not require the use of VEXCC and only needs VCC1 and VCC2, how should the VEXMON, VEXCTRL, and VEXCC pins be handled? In the schematic design, can they be left floating? If left floating, what issues…
Our design will add the TUSB211A at 20 inch after USB Host,however,we want to know how long PCB routing can be supported after TUSB211A ? Assuming the use of FR4 PCB material。
Alternatively,how long PCB routing do you suggest addi…
我目前正在尝试通过intel i210来同步一台Aes67音频设备输出的PTP时钟,i210输出的参考时钟再通过LMK05318B过滤/倍频后输出I2S时钟给下游设备。
i210由一台x86 linux pc控制,通过linux的ptp4l同步外部时钟,testptp程序来控制i210的sdp引脚输出2Khz的方波信号作为LMK05318B的参考时钟,LMK05318B的XO晶振是12.288M的TCXO
测试用的PCB是我自己绘制的,目前测试所使用的寄存器配置如下…
您好:
测试tcan1146的选择唤醒功能时,写入0x81到0x10地址进入休眠模式,之后需要发送多次唤醒数据才
可以让INH电平变化(变成待机模式),请问这个测试结果是否正确? 如果是正确的,那需要发送多次
唤醒数据的原因是什么? 能否只发送一个数据包使tcan1146从休眠唤醒?
谢谢!
1.我想用DS320PR1601搭配Broadcom PEX89104,是否合适?
2.能否给我一份DS320PR1601RSCEVM的EEPROM的镜像文件。