Other Parts Discussed in Thread: TFP401
Hello, may I ask if TI has an HDMI to RGB converter similar to TFP401 that supports it 4K@60HZ Is it a chip for image input. The manual states that TFP401 only supports 1080p and WUXGA at 60…
请问TI有没有将12G SDI、DVI、HDMI3种接口转MIPI-CSI的方案?还有HDMI扩展,1进同步2出的?有的话请告知芯片型号或链接,谢谢!
我先介绍一下当前的结构:用一个带有HDMI输出的摄像头,连接到tfp401,再将tfp401输出信号,连接到TI的buffer(74AVC16T245)实现3.3v转换1.8v,再直连到fpga芯片,之后再让fpga送给tfp410,由于fpga输出也是1.8v,于是将410的vref连接一个0.9v电压。tfp410的输出连接到显示器的HDMI端口。当前测试在fpga里面直接将输入和输出短接。
1、麻烦帮忙看看,我们的电路是否有问题,如下4个截图;
2、测试一下401输出时钟大约150MHz,选择几根信号线也有变化…