This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC4245A: 几款芯片相关问题咨询

Part Number: 74LVC245A
Other Parts Discussed in Thread: SN74LVC8T245, SN74LVC4245A,

芯片74LVC245A
问题
1、这款芯片能否用于并口通信(AD转换芯片输出的是5V的并口信号,而数据接收的MCU是3.3V的,需要相关的芯片进行转换匹配,74LVC245A是否满足要求)?

2 并口通讯时,例如AD转换芯片的并口输出为三态,在转换过程中输出是高阻态,那么此时对于74LVC245A芯片来说,其输入就变成了了高阻态,
,那么这种情况该怎么处理?是忽视还是加上下拉电阻?

3、不用的引脚可以通过10K的下拉电阻下拉到GND吗?

4、OE引脚能否直接接到GND?(查看手册来看,要求上电瞬间通过上拉电阻接到VCC);

5、DIR引脚,能否通过10K的上拉电阻接到3.3V;

芯片SN74LVC8T245
问题:

1、3.3V的MCU的I/O口设置为推挽输出,通过芯片SN74LVC8T245转换后输出5V控制电平,在芯片SN74LVC8T245输入端口是否需要加下拉电阻(10K)?

2、如果MCU的I/O口输出为低电平时,芯片SN74LVC8T245是否会对MCU的I/O口产生倒灌电流,有的话是多大?

3、芯片的电平转换引脚都是独立工作的吗,引脚之间互相有影响吗?

4、OE引脚能否直接接到GND?(查看手册来看,要求上电瞬间通过上拉电阻接到VCC);

芯片SN74LVC4245A
问题:
1、这款芯片能否用于并口通信(AD转换芯片输出的是5V的并口信号,而数据接收的MCU是3.3V的,需要相关的芯片进行转换匹配,74LVC245A是否满足要求)?

2、通过查手册发现这个芯片有个上电时序问题,就是VCCA先上电,VCCB后上电(VCCA端接5V,VCCB端接3.3V),因为我板子上的3.3V电源是通过AMS1117芯片(LDO)
5V转换过来的,想问一下能通过这种方式来解决芯片上电时序问题吗(因为没有看到AMS1117的数据手册中明确的标明此芯片有延时的功能或参数)?

  • 您好,

    对于芯片SN74LVC245A

    1、看SN74LVC245A数据手册中Table 1. Function Table,其PortA和PortB 8通道都是同时传输的,因此可以并行工作。是否可以满足电平转换要求,需看输入和输出是否电平兼容,对于SN74LVC245A,其A口和B口都可以5V输入,输出电平与供电电压和输出电流有关,具体您需要根据接收端的MCU可以识别的电平范围去判断,我把SN74LVC245A的输出电平截图如下:

    另外还需考虑信号的速率是否满足要求,您ADC输出的最大频率是多少?

    2、看百度百科,高组态既不是高电平也不是低电平,如果高阻态再输入下一级电路的话,对下级电路无任何影响,和没接一样,如果用万用表测的话有可能是高电平也有可能是低电平,随它后面接的东西定的。因此这个需要取决于您的应用。

    3、可以的,数据手册中有描述“All unused inputs of the device must be held at VCC or GND to ensure proper device operation.”

    或参考下面建议:

    e2e.ti.com/.../faq-how-do-i-terminate-any-unused-channels-of-a-logic-device

    4、上下电瞬间接高电平是为了确保其三态输出,如果您对上下电瞬间电平有要求的话,那么上下电期间就需要接高电平

    5、可以的,DIR是控制方向的

  • 芯片SN74LVC8T245
    问题:

    1、3.3V的MCU的I/O口设置为推挽输出,通过芯片SN74LVC8T245转换后输出5V控制电平,在芯片SN74LVC8T245输入端口是否需要加下拉电阻(10K)?

    2、如果MCU的I/O口输出为低电平时,芯片SN74LVC8T245是否会对MCU的I/O口产生倒灌电流,有的话是多大?

    3、芯片的电平转换引脚都是独立工作的吗,引脚之间互相有影响吗?

    4、OE引脚能否直接接到GND?(查看手册来看,要求上电瞬间通过上拉电阻接到VCC);

    1、推挽输出也许有、也许没有高阻态,如果您想要SN74LVC8T245一个确定输入的话,是建议加上的

    2、SN74LVC8T245是可以双向控制,如果您MCU的输出接SN74LVC8T245的输出的话,其电流就取决于它们之间输出接口的阻抗了

    3、SN74LVC8T245其电平转换管脚有8通通,是同时受OE和DIR控制的,相互之间没有影响

    4、OE是使能管脚,如果您对上电瞬间其输出状态没有要求,可以直接接地

  • 芯片SN74LVC4245A
    问题:
    1、这款芯片能否用于并口通信(AD转换芯片输出的是5V的并口信号,而数据接收的MCU是3.3V的,需要相关的芯片进行转换匹配,74LVC245A是否满足要求)?

    2、通过查手册发现这个芯片有个上电时序问题,就是VCCA先上电,VCCB后上电(VCCA端接5V,VCCB端接3.3V),因为我板子上的3.3V电源是通过AMS1117芯片(LDO)
    5V转换过来的,想问一下能通过这种方式来解决芯片上电时序问题吗(因为没有看到AMS1117的数据手册中明确的标明此芯片有延时的功能或参数)?

    1、同上,需要考虑是否与前级和后级芯片的电平是否兼容,以及数据速率是否满足;

    2、 应该可以的,不放心的话,您可以用示波器实测一下其上电波形