This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We use 74hcs serie chips to solve the slow rise/fall time issue, because RC(R:30K C:0.22uf) is designed as the input of 74hcs08 to have a certain delay time.
We belive that the solw rise time is suitable for hcs chips as the datesheet described:
However, the slow rise/fall siganl may failue to triggle the 74hcs08.
What is the problem of this design?
Thanks very much!
与门输入输出连接情况:
1、与门输入端接的是74HC14输出,接了30k和0.22uf的电容,期望该信号能够有一定的延迟输入;
2、与门输出是直连到该与门芯片的另外一路输入端。
3、输入的高电平接近5V,低电平接近0V
我也注意到了,与门要求输出电容负载要小于50pf,74hc14输出负载要求小于70pf,我看手册理解这个应该不是强制要求,只是希望有更好的波形给下一级的输入,如果下一级 输入是施密特输入,为增加一定的延时,增加电容负载我理解是可以的,不知道我的理解是否正确,谢谢!
SN74HCS08的供电电压是5V吗?另一输入端接的是什么?输出端走线长吗?建议您附上同时测量的输入和输出信号的波形以便进行问题分析。
在SN74HCS08输入端加RC滤波电路我认为也是可以的:
这里的50pf和70pf是指逻辑IC输出端的容性负载,容性负载太大,会增加数字信号的上升时间,这样输出波形的上升沿就会存在明显失真。
电路图您可以将图片直接拖入回复对话框来上传。