This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS08: Slow rise/fall time issue

Part Number: SN74HCS08


Hi,

    We use 74hcs serie chips to solve the slow rise/fall time issue,  because  RC(R:30K C:0.22uf)  is designed  as the input of 74hcs08   to  have a  certain delay time. 

  We belive that the solw rise time is suitable for hcs chips as the datesheet described:

    However,   the slow rise/fall siganl  may failue to triggle the 74hcs08.

    What is the problem of this design?

    Thanks very much!

    

  • 您好,

    您可以附上应用的 SN74HCS08电路图吗?

    供电电压是多少?工作中供电电压正常吗?

    输出端负载接的是什么?输出端走线长吗?请确保输出端的电容负载 ≤ 50 pF;

    输入信号是怎样的?您可以同时附上输入和输出信号波形吗?请注意,虽然 SN74HCS08对输入信号变化率没有要求,但是对输入信号上的噪声幅度仍有一定的要求,振幅足够大的噪音仍会导致问题。请注意datasheet中的ΔVT、VT-(min)、 VT+(max) 参数。

  • 与门输入输出连接情况:

    1、与门输入端接的是74HC14输出,接了30k和0.22uf的电容,期望该信号能够有一定的延迟输入;

    2、与门输出是直连到该与门芯片的另外一路输入端。

    3、输入的高电平接近5V,低电平接近0V

    我也注意到了,与门要求输出电容负载要小于50pf,74hc14输出负载要求小于70pf,我看手册理解这个应该不是强制要求,只是希望有更好的波形给下一级的输入,如果下一级 输入是施密特输入,为增加一定的延时,增加电容负载我理解是可以的,不知道我的理解是否正确,谢谢!

  • SN74HCS08的供电电压是5V吗?另一输入端接的是什么?输出端走线长吗?建议您附上同时测量的输入和输出信号的波形以便进行问题分析。

    在SN74HCS08输入端加RC滤波电路我认为也是可以的:

    这里的50pf和70pf是指逻辑IC输出端的容性负载,容性负载太大,会增加数字信号的上升时间,这样输出波形的上升沿就会存在明显失真。

    电路图您可以将图片直接拖入回复对话框来上传。