• 为什么TXB0104不能用于IIC

    Other Parts Discussed in Thread: TXS0102, LSF0102, TXB0104

    好的!那我更有意向选TX0102(我们只需要两路),至少可以不用外接上拉电阻(其实我的项目需要PIN共用问题,就是这个PIN 既要作为SPI通讯用也要作为IIC,如果不需要上拉动作,也就不需要切换到SPI要求断开的额外操作),再说TXS0102 比较LSF0102更便宜。

    另外能否顺便告诉下为什么TXB0104不能用于IIC,从规格书上的描述我还是没明白,另外IIC单端接上主设备(没接从设备的时候…

  • TXB0104: 电平转换应用问题(同时用于SPI& IIC)是否可行

    Part Number: TXB0104

    我有一个线路需要用同样大管脚,实现SPI和IIC通讯,我是否可以用他来实现(SPI 模式下不上拉, IIC模式下通过两边上拉实现),如果说有问题,是否有其他型号替换? 例如TXS01XX, 另外如果用TXS01系列是不是在IIC通讯的时候也要两边上拉,如果可以,上拉电阻多大合适?请帮忙

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
  • LSF0102: 如何设置芯片外围条件,使其可传输100MHz频率信号

    Part Number: LSF0102

    如何设置芯片外围条件(电容和电阻值),使其可传输100MHz频率信号

  • LSF0204: 电压抬升范围问题

    Part Number: LSF0204
    Other Parts Discussed in Thread: LSF0102

    你好,我在评估LSF0204在我们电路设计中的可行性,该器件datasheet首页说明其支持1.2V向1.8V等电平升压转换,且7.9节Switching Characteristics给出了1.2V向1.8V升压转换时的开关特性,然而手册第14页Design Requirements却要求Vref_B ≥ Vref_A + 0.8V,并推荐Vref_B ≥ Vref_A…

  • LSF0102-Q1: LSF0102的参考电压问题

    Part Number: LSF0102-Q1

    Hi,E2E

         请教个问题,看了TI关于LSF系列芯片介绍的视频,网址如下,Understanding the LSF family of bidirectional, multi-voltage level translators | TI.com

         视频中有个问题不太理解,如下截图,200K电阻会形成一个限流,然后强制形成一个FET的阈值电压,想问一下,这个是怎么形成的呀

  • LSF0102-Q1: 关于手册中提到的信号质量问题

    Part Number: LSF0102-Q1
    Other Parts Discussed in Thread: LSF0102

    Hi,E2E,请教个问题

         关于LSF0102芯片手册中提到的Vref_B和VI(EN)建议比Vref_A高1.0 V,以获得最佳的信号完整性,想问一下,如果不满足这个条件会影响信号质量么,是怎么影响的呀

  • LSF0102: 双向电平转换芯片实现网络MDC/MDIO电平转换,只能1对1么,是否可以实现一对多转换方式

    Part Number: LSF0102

    双向电平转换芯片LSF0102实现网络MDC/MDIO电平转换,只能1对1么,

    是否可以使用双向电平转换芯片LSF0102实现如下转换方式功能

    连接方式1:

    连接方式2:

    连接方式3:

  • LSF0102: Can it be design as hot-swap design without any else protect component?

    Part Number: LSF0102

    As described in zhct070a(logic guide 2014 ) article, LSF series support hot swap. While the LSF series is not described in the article of sdyu001ab-(logic guide rev.ab).

    Now, we are designing  a system with a mother card and a daughter…

  • TXS0102: 快速掉电上电后会发振

    Part Number: TXS0102
    Other Parts Discussed in Thread: LSF0102

    我们如上图使用了TXS0102,在测试时发现,快速的off/on电源后会在A2测到9.8MHz的波形。于是我将A2和B2的电阻断开,测试发现震荡波形是从TXS0102本身发出的。

    于是我去掉了1.8V与OE之间的10k电阻。发振的再现率变低了,但是仍然存在。

    请教是什么引起的发振,如何解决。

    谢谢