This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C1292NCPDT:SPI 代码对 SSI3不起作用

Guru**** 2392915 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1238866/tm4c1292ncpdt-spi-code-not-working-for-ssi3

器件型号:TM4C1292NCPDT

您好!

我的 SPI (使用 SSI0)示例代码在 TI Launchpad 上工作。 请参阅以下代码

#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_ssi.h>
#include "inc/hw_memmap.h"
#include <driverlib/gpio.h>
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include <string.h>
//#include "main.h"


// Number of bytes to Send.
//
//*****************************************************************************
#define NUM_SSI_DATA 4
#define HB_ENABLE 0x0080
#define HB_CONFIG 0x0002


#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif


uint32_t ui32SysClocks;
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void InitConsole(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 9600, ui32SysClocks);
}

void InitSPI0(void){

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3|GPIO_PIN_2|GPIO_PIN_4);
GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PIN_5);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE, GPIO_PIN_5);
GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP

GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_4);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_4, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_4, GPIO_PIN_4);//PULL UP

GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);//Tx
GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);//Rx
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 | GPIO_PIN_2);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_2, SSI_MODE_MASTER, 40000000, 16);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1500000, 16);
SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 1500000, 16);//negative edge triggered
}

void SPI_write(const uint8_t* dataBuffer, uint8_t count){

while(count--){
SSIDataPut(SSI0_BASE, *dataBuffer++);
}
while(SSIBusy(SSI0_BASE));
}

//*****************************************************************************
//Main function Entry.
//
//*****************************************************************************
int
main(void)
{
bool pDO_Status[24];
uint8_t ui8Do_Source_Sink;

// spiConfigbus stSpiConfig;
// i2cConfigbus stI2cConfig;
uint16_t aui16SpiTxBuffer[2];
uint16_t aui16SpiRxBuffer[2][2];
uint8_t aui8I2cTxBuffer[3];
uint8_t aui8I2cRxBuffer[3];
uint8_t i;

uint8_t dataTX[4] = {0x40, 0x4F, 0x4F, 0x04};
//uint8_t dataTX = 0x40;
uint8_t count;

//ui32SysClocks = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_240), 120000000);
ui32SysClocks = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
InitConsole();

UARTprintf("SPI -> Master to Slave\n");
UARTprintf("SPI Bit_Rate: 16-bit\n\n");
InitSPI0();
SSIEnable(SSI0_BASE);

// GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5); //enable


dataTX[0] = (HB_ENABLE << 0 )| (HB_CONFIG << 0);//output high

SysCtlDelay(100);

SPI_write(dataTX, 1);

SysCtlDelay(100);//delay of

}

UARTprintf("Done transferring the data\r\n");
UARTprintf("----------------------------------------------------------------------");
UARTprintf("\r\n\n");

while(1);
}

但当我根据我的要求(使用 SSI3)对其进行修改时、它在 Launchpad 上不起作用。 请参见下面针对 SSI3修改的代码。

#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_ssi.h>
#include "inc/hw_memmap.h"
#include <driverlib/gpio.h>
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include <string.h>
//#include "main.h"


// Number of bytes to Send.
//
//*****************************************************************************
#define NUM_SSI_DATA 4
#define HB_ENABLE 0x0080
#define HB_CONFIG 0x0002


#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif


uint32_t ui32SysClocks;
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void InitConsole(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 9600, ui32SysClocks);
}

void InitSPI0(void){

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3|GPIO_PIN_2|GPIO_PIN_4);
GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PIN_5);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE, GPIO_PIN_5);
GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP

GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_4);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_4, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_4, GPIO_PIN_4);//PULL UP

GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);//Tx
GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);//Rx
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 | GPIO_PIN_2);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_2, SSI_MODE_MASTER, 40000000, 16);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1500000, 16);
SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 1500000, 16);//negative edge triggered
}

void InitSPI3(void){

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);

GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_2 | GPIO_PIN_0);
GPIOPinTypeGPIOInput(GPIO_PORTQ_BASE, GPIO_PIN_3);

GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, GPIO_PIN_1);//cs

GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE, GPIO_PIN_5);
GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP

// GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
// GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP

// GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_4);
GPIOPadConfigSet(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU );
GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_PIN_1);//PULL UP

GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
//GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);//Tx
GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);//Rx
GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_0 | GPIO_PIN_3 | GPIO_PIN_2);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_2, SSI_MODE_MASTER, 40000000, 16);
//SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1500000, 16);
SSIConfigSetExpClk(SSI3_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 1500000, 16);//negative edge triggered
}

/*void SPI_write(const uint8_t* dataBuffer, uint8_t count){

while(count--){
SSIDataPut(SSI0_BASE, *dataBuffer++);
}
while(SSIBusy(SSI0_BASE));
}*/

void SPI_write_SSI3(const uint8_t* dataBuffer, uint8_t count){

while(count--){
SSIDataPut(SSI3_BASE, *dataBuffer++);
}
while(SSIBusy(SSI3_BASE));
}

//*****************************************************************************
//Main function Entry.
//
//*****************************************************************************
int
main(void)
{
bool pDO_Status[24];
uint8_t ui8Do_Source_Sink;

volatile uint32_t ui32Loop;

uint16_t aui16SpiTxBuffer[2];
uint16_t aui16SpiRxBuffer[2][2];
uint8_t aui8I2cTxBuffer[3];
uint8_t aui8I2cRxBuffer[3];
uint8_t i;

uint8_t dataTX[4] = {0x40, 0x4F, 0x4F, 0x04};
//uint8_t dataTX = 0x40;
uint8_t count;

//ui32SysClocks = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_240), 120000000);
ui32SysClocks = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
InitConsole();

UARTprintf("SPI -> Master to Slave\n");
UARTprintf("SPI Bit_Rate: 16-bit\n\n");

InitSPI3();
SSIEnable(SSI3_BASE);

dataTX[0] = (HB_ENABLE << 0 )| (HB_CONFIG << 0);//output high
GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_1, 0);

SysCtlDelay(100);

SPI_write_SSI3(dataTX, 1);

SysCtlDelay(100);//delay of

GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_PIN_1);



UARTprintf("Done transferring the data\r\n");
UARTprintf("----------------------------------------------------------------------");
UARTprintf("\r\n\n");

while(1);
}

SSI3在我的原理图中用于如下所示

如果代码中有任何内容需要更改才能运行 SSI3、您能否提供指导?

谢谢。

Kiran

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     我认为这是 BoosterPack 上的 R19和 R20 0欧姆电阻造成的。 一个选择是 移除 R19和 R20。 另一个选项是确保当您是 PQ2和 PQ3时、PA3和 PA2仅配置为 GPIO 输入。 当 PA2和 PQ3用于 SPI 时、您无法驱动 PA3和 PA2。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Charles:

    将尝试在修改后的代码中删除 R19和 R20、PA2和 PA3、因为我不会调用函数 InitSPI0、其中 PA2和 PA3作为输出驱动。

    此致、

    Kiran

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    为什么不使用分线板连接器 X11代替 BoosterPack? 它有什么不同?

    在示波器上、您看到了什么?

    我看到您的代码中的以下行。 如果您正在为 SPI 使用 PQ0/2/3、则需要将其删除。 您需要针对 GPIO 配置这些引脚。  

    GPIOPinTypeGPIOOutput (GPIO_PORTQ_BASE、GPIO_PIN_2 | GPIO_PIN_0);
    GPIOPinTypeGPIOInput (GPIO_PORTQ_BASE、GPIO_PIN_3);

    在您的代码中、为什么您不使用以下类似代码来为 SPI 函数配置 PQ0/P22/PQ3。  

    //
    //为 PQ2配置 GPIO 引脚多路复用器
    //对于 SSI3XDAT0
    //
    MAP_GPIOPinConfigure (GPIO_PQ2_SSI3XDAT0);
    MAP_GPIOPinTypeSSI (GPIO_PORTQ_BASE、GPIO_PIN_2);

    //
    //为 PQ3配置 GPIO 引脚多路复用器
    //对于 SSI3XDAT1
    //
    MAP_GPIOPinConfigure (GPIO_PQ3_SSI3XDAT1);
    MAP_GPIOPinTypeSSI (GPIO_PORTQ_BASE、GPIO_PIN_3);

    //
    //为 PQ0配置 GPIO 引脚多路复用器
    //对于 SSI3CLK
    //
    MAP_GPIOPinConfigure (GPIO_PQ0_SSI3CLK);
    MAP_GPIOPinTypeSSI (GPIO_PORTQ_BASE、GPIO_PIN_0);

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Charles:

    我根据您的建议修改了代码。 在 LaunchPad 上仍然无法正常工作。

    请参阅以下内容:

    void InitSPI3(void){
    
            SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
            SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
            SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
    
            //GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_2 | GPIO_PIN_0);
            //GPIOPinTypeGPIOInput(GPIO_PORTQ_BASE, GPIO_PIN_3);
    
            GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, GPIO_PIN_1);//cs
    
            GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE, GPIO_PIN_5);
            GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU  );
            GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP
    
    //        GPIOPadConfigSet(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU  );
      //      GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_5, GPIO_PIN_5);//PULL UP
    
           // GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_4);
            GPIOPadConfigSet(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD_WPU  );
            GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_PIN_1);//PULL UP
    
            //GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
            //GPIOPinConfigure(GPIO_PA3_SSI0FSS);
            //GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);//Tx
            //GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);//Rx
    
            //
            // Configure the GPIO Pin Mux for PQ2
            // for SSI3XDAT0
            //
            GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);
            GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_2);
    
            //
            // Configure the GPIO Pin Mux for PQ3
            // for SSI3XDAT1
            //
            GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);
            GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_3);
    
            //
            // Configure the GPIO Pin Mux for PQ0
            // for SSI3CLK
            //
            GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
            GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_0);
    
            GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_0 | GPIO_PIN_3 | GPIO_PIN_2);
            //SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_2, SSI_MODE_MASTER, 40000000, 16);
            //SSIConfigSetExpClk(SSI0_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1500000, 16);
            SSIConfigSetExpClk(SSI3_BASE, ui32SysClocks, SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 1500000, 16);//negative edge triggered
    }

    请告知。

    谢谢。

    Kiran

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我根据您的建议修改了代码。 在 LaunchPad 上仍然无法正常工作。

    [/报价]

    您的示波器波形显示了什么? SPICLK 和 SPITX 是否只是平坦的线且完全没电? 这到底是件令人难以置信的事情吗? 是否可以显示 SSI3的 Clk、FSS、Tx 和 Rx 引脚?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Charles:

    是的、这是一条完全平坦的线、根本没有信号。

    请告知。

    谢谢。

    Kiran

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     您能试试这段代码吗? 在此代码中、SSI3向 SSI1发送4个字节的数据。 我在我的 LaunchPad 上成功运行它。 请注意、我使用 X11分线板上的 PQ2和 PQ3。 如果运行正常、它应在"Terminal"窗口中生成以下结果。  您是否有其他 LaunchPad? 您是否可以在另一个 LaunchPad 上重现该问题?

    CH1:SSI3CLK

    通道2:SSI3Fss

    通道3:SSI3TX

    通道4:SSI3RX

    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_memmap.h"
    #include "inc/hw_ints.h"
    #include "driverlib/debug.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/rom.h"
    #include "driverlib/rom_map.h"
    #include "driverlib/ssi.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>SSI Master-to-Slave Transfer (spi_master_slave_xfer)</h1>
    //!
    //! This example demonstrates how to configure SSI3 as a SSI Master and SSI1
    //! as a SSI slave.  The master will send four characters on the master to the 
    //! slave using the legacy mode.  In legacy mode, one bit is sent on each
    //! SSI Clock pulse.  Once the SSI slave receives the four characters in the
    //! receive FIFO it will generate an interrupt.
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - SSI3 peripheral
    //! - GPIO Port A peripheral (for SSI3 pins)
    //! - SSI3Clk    - PQ0
    //! - SSI3Fss    - PQ1
    //! - SSI3TX     - PQ2
    //! - SSI3RX     - PQ3
    //!
    //! - SSI1 peripheral
    //! - GPIO Port B & E peripheral (for SSI1 pins)
    //! - SSI1Clk    - PB5
    //! - SSI1Fss    - PB4
    //! - SSI1TX     - PE4
    //! - SSI1RX     - PE5
    //!
    //! This example requires board level connection between SSI3 and SSI1.
    //!
    //! UART0, connected to the Virtual Serial Port and running at 115,200, 8-N-1,
    //! is used to display messages from this application.
    //
    //*****************************************************************************
    
    //****************************************************************************
    //
    // The variable g_ui32SysClock contains the system clock frequency in Hz.
    //
    //****************************************************************************
    uint32_t g_ui32SysClock;
    
    //*****************************************************************************
    //
    // Global flag to indicate data has been received.
    //
    //*****************************************************************************
    volatile uint32_t g_breceiveFlag = 0;
    
    //*****************************************************************************
    //
    // Number of bytes to send and receive.
    //
    //*****************************************************************************
    #define NUM_SSI_DATA            4
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // Configure the UART and its pins. This must be called before UARTprintf().
    //
    //*****************************************************************************
    void
    ConfigureUART(void)
    {
        //
        // Enable the GPIO Peripheral used by the UART.
        //
        ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Enable UART0.
        //
        ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
        //
        // Configure GPIO Pins for UART mode.
        //
        ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
        ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
        ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, g_ui32SysClock);
    }
    
    //*****************************************************************************
    //
    // When the received FIFO is half-full, an interrupt will be generated.
    //
    //*****************************************************************************
    void
    SSI1IntHandler(void)
    {
        uint32_t ui32Status;
    
        //
        // Read SSIMIS (SSI Masked Interrupt Status).
        //
        ui32Status = MAP_SSIIntStatus(SSI1_BASE, true);
    
        //
        // Clear the SSI interrupt.
        //
        MAP_SSIIntClear(SSI1_BASE, ui32Status);
    
        //
        // Turn off the RX FIFO interrupt.
        //
        MAP_SSIIntDisable(SSI1_BASE, SSI_RXFF);
    
        g_breceiveFlag = 1;
    }
    
    //*****************************************************************************
    //
    // Configure SSI3 in Quad-SSI master Freescale (SPI) mode and SSI1 in Quad-SSI
    // slave mode.  The SSI3 will send out 4 bytes of data in advanced Quad mode
    // and the SSI1 slave will receive the 4 bytes of data also in Quad-mode.  The
    // slave will generate interrupt upon receiving the 4 bytes of data.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t pui32DataTx[NUM_SSI_DATA];
        uint32_t pui32DataTx1[NUM_SSI_DATA];
        uint32_t pui32DataRx[NUM_SSI_DATA];
        uint32_t ui32Index;
    
        //
        // Run from the PLL at 120 MHz.
        // Note: SYSCTL_CFG_VCO_240 is a new setting provided in TivaWare 2.2.x and
        // later to better reflect the actual VCO speed due to SYSCTL#22.
        //
        g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                                 SYSCTL_OSC_MAIN |
                                                 SYSCTL_USE_PLL |
                                                 SYSCTL_CFG_VCO_240), 120000000);
    
        //
        // Set up the serial console to use for displaying messages.
        //
        ConfigureUART();
    
        //
        // Display the setup on the console.
        //
        UARTprintf("SSI Master-Slave Transfer Example.\n");
        UARTprintf("Mode: Legacy SPI\n");
        UARTprintf("Data: 8-bit\n\n");
    
        //
        // The SSI3 and SSI1 peripheral must be enabled for use.
        //
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
    
        //
        // For this example SSI3 is used with PortQ[3:0].  The SSI1 uses
        // PortB and PortE for the SSICLK, SSIFss and the TX/RX pins.
        // GPIO ports need to be enabled so those pins can be used.
        //
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
        MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    
        //
        // Configure the pin muxing for SSI3 functions on PQ[3:0].
        // Configure the pin muxing for SSI1 functions on PB and PE.
        //
        MAP_GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
        MAP_GPIOPinConfigure(GPIO_PQ1_SSI3FSS);
        MAP_GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);
        MAP_GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);
    
        MAP_GPIOPinConfigure(GPIO_PB5_SSI1CLK);
        MAP_GPIOPinConfigure(GPIO_PB4_SSI1FSS);
        MAP_GPIOPinConfigure(GPIO_PE4_SSI1XDAT0);
        MAP_GPIOPinConfigure(GPIO_PE5_SSI1XDAT1);
    
        //
        // Configure the GPIO settings for the SSI pins.  This function also gives
        // control of these pins to the SSI hardware.  Consult the data sheet to
        // see which functions are allocated per pin.
        // The pins are assigned as follows:
        //      SSI3
        //      PQ3 - SSI3RX
        //      PQ2 - SSI3TX
        //      PQ1 - SSI3Fss
        //      PQ0 - SSI3CLK
        //      SSI1
        //      PE5 - SSI1RX
        //      PE4 - SSI1TX
        //      PB4 - SSI1Fss
        //      PB5 - SSI1CLK
        //
        MAP_GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_3 |
                       GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);
        MAP_GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_5 | GPIO_PIN_4 );
        MAP_GPIOPinTypeSSI(GPIO_PORTE_BASE, GPIO_PIN_5 | GPIO_PIN_4 );
    
        //
        // Configure and enable the SSI3 port for SPI master mode.  Use SSI3,
        // system clock supply, idle clock level low and active low clock in legacy
        // Freescale SPI mode, master mode, 2MHz SSI frequency, and 8-bit data.
        // For SPI mode, you can set the polarity of the SSI clock when the SSI
        // unit is idle.  You can also configure what clock edge you want to
        // capture data on.  Please reference the datasheet for more information on
        // the different SPI modes.
        //
        MAP_SSIConfigSetExpClk(SSI3_BASE, g_ui32SysClock, SSI_FRF_MOTO_MODE_0,
                           SSI_MODE_MASTER, 2000000, 8);
    
        //
        // Configure and enable the SSI1 port for SPI slave mode with matching
        // SPI mode, clock speed, and data size parameters as the master.
        //
        MAP_SSIConfigSetExpClk(SSI1_BASE, g_ui32SysClock, SSI_FRF_MOTO_MODE_0,
                           SSI_MODE_SLAVE, 2000000, 8);
    
        //
        // Enable processor interrupts.
        //
        IntMasterEnable();
    
        //
        // Enable SSI1 interrupt on RX FIFO full.
        //
        MAP_SSIIntEnable(SSI1_BASE, SSI_RXFF);
    
        //
        // Enable the SSI1 interrupts on the processor (NVIC).
        //
        IntEnable(INT_SSI1);
    
        //
        // Enable the SSI3 and SSI1 modules.
        //
        MAP_SSIEnable(SSI3_BASE);
        MAP_SSIEnable(SSI1_BASE);
    
        //
        // Read any residual data from the SSI port.  This makes sure the receive
        // FIFOs are empty, so we don't read any unwanted junk.  This is done here
        // because the SPI SSI mode is full-duplex, which allows you to send and
        // receive at the same time.  The SSIDataGetNonBlocking function returns
        // "true" when data was returned, and "false" when no data was returned.
        // The "non-blocking" function checks if there is any data in the receive
        // FIFO and does not "hang" if there isn't.
        //
        while(MAP_SSIDataGetNonBlocking(SSI3_BASE, &pui32DataRx[0]))
        {
        }
        while(MAP_SSIDataGetNonBlocking(SSI1_BASE, &pui32DataRx[0]))
        {
        }
    
        //
        // Initialize the data to send.
        //
        pui32DataTx[0] = 'T';
        pui32DataTx[1] = 'I';
        pui32DataTx[2] = 'V';
        pui32DataTx[3] = 'A';
        pui32DataTx1[0] = 'Q';
        pui32DataTx1[1] = 'S';
        pui32DataTx1[2] = 'S';
        pui32DataTx1[3] = 'I';
    
        //
        // Display indication that the SSI3/SSI1 is transmitting data.
        //
        UARTprintf("SSI3 Sent:\n  ");
        UARTprintf("'T' 'I' 'V' 'A' \n");
        UARTprintf("SSI1 Sent:\n  ");
        UARTprintf("'Q' 'S' 'S' 'I' \n");
    
        //
        // Send 4 bytes of data.
        //
        for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
        {
            //
            // Prepare data to send from the slave.
            //
            MAP_SSIDataPut(SSI1_BASE, pui32DataTx1[ui32Index]);
    
            //
            // Send the data using the "blocking" put function.  This function
            // will wait until there is room in the send FIFO before returning.
            // This allows you to assure that all the data you send makes it into
            // the send FIFO.
            //
            MAP_SSIDataPut(SSI3_BASE, pui32DataTx[ui32Index]);
        }
    
        //
        // Wait until SSI1 receives the half-full interrupt on the RX FIFO.
        //
        while (g_breceiveFlag == 0);
    
        //
        // Display indication that the SSI3 is receiving data.
        //
        UARTprintf("\nSSI3 Received:\n  ");
    
        //
        // Receive 4 bytes of data.
        //
        for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
        {
            //
            // Receive the data using the "blocking" Get function.  This function
            // will wait until there is data in the receive FIFO before returning.
            //
            MAP_SSIDataGet(SSI3_BASE, &pui32DataRx[ui32Index]);
    
            //
            // Since we are using 8-bit data, mask off the MSB.
            //
            pui32DataRx[ui32Index] &= 0x00FF;
    
            //
            // Display the data that SSI3 received.
            //
            UARTprintf("'%c' ", pui32DataRx[ui32Index]);
        }
    
        //
        // Display indication that the SSI1 is receiving data.
        //
        UARTprintf("\nSSI1 Received:\n  ");
    
        //
        // Receive 4 bytes of data.
        //
        for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
        {
            //
            // Receive the data using the "blocking" Get function.  This function
            // will wait until there is data in the receive FIFO before returning.
            //
            MAP_SSIDataGet(SSI1_BASE, &pui32DataRx[ui32Index]);
    
            //
            // Since we are using 8-bit data, mask off the MSB.
            //
            pui32DataRx[ui32Index] &= 0x00FF;
    
            //
            // Display the data that SSI1 received.
            //
            UARTprintf("'%c' ", pui32DataRx[ui32Index]);
        }
    
        //
        // Display indication that the SSI1 is receiving data.
        //
        UARTprintf("\n\nMaster-Slave Transfer Complete.\n");
    
        //
        // Return no errors.
        //
        while (1);
    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢您的支持、Charles!