This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TM4C123GH6PM:在 Tiva-c 中获取时间的最佳方法

Guru**** 2928980 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1419167/tm4c123gh6pm-best-way-for-obtaining-time-in-the-tiva-c

器件型号:TM4C123GH6PM

工具与软件:

您好!

如何在不使用调试模式计数器的情况下获取 CPU 节拍?

以编程方式获取计时的最佳方式是什么? 我所说的时序是指亚秒级高精度计数器。

我让我的 SysTick 每秒执行1024次。 下面是 systickkinthandler。

void SysTickIntHandler (void){

   G_ui32SysTickCount++;

   if (g_ui32SysTickCount % 1024 => 0){
       g_ui32PosixTime++;
       G_ui32SysTickCount = 0;
   }

}

当我需要对所得到的东西进行时间戳记时(g_ui32SysTickCount * dt_period)+(dt_period - SysTickValueGet ())

有什么更好的方法可以做到这一点吗? 是否有更实用的方法来跟踪时间?

此致、

CAN

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 CAN、

    qiang zhang 说:
    有什么更好的方法可以做到这一点吗? 是否有更实用的方法来跟踪时间?

    我建议您查看 RTC (实时计数器)计数器、其主要目的是跟踪时间。  

    7.3.5 Real-Time Clock
    The RTC module is designed to keep wall time. The RTC can operate in seconds counter mode. A
    32.768 kHz clock source along with a 15-bit predivider reduces the clock to 1 Hz. The 1 Hz clock
    is used to increment the 32-bit counter and keep track of seconds. A match register can be configured
    to interrupt or wake the system from hibernate. In addition, a software trim register is implemented
    to allow the user to compensate for oscillator inaccuracies using software.


    7.3.5.1 RTC Counter - Seconds/Subseconds Mode
    The clock signal to the RTC is provided by either of the 32.768-kHz clock sources available to the
    Hibernation module. The Hibernation RTC Counter (HIBRTCC) register displays the seconds
    value. The Hibernation RTC Sub Seconds register (HIBRTCSS) is provided for additional time
    resolution of an application requiring less than one-second divisions.
    The RTC is enabled by setting the RTCEN bit of the HIBCTL register. The RTC counter and
    sub-seconds counters begin counting immediately once RTCEN is set. Both counters count up. The
    RTC continues counting as long as the RTC is enabled and a valid VBAT is present, regardless of
    whether VDD is present or if the device is in hibernation.
    The HIBRTCC register is set by writing the Hibernation RTC Load (HIBRTCLD) register. A write
    to the HIBRTCLD register clears the 15-bit sub-seconds counter field, RTCSSC, in the HIBRTCSS
    register. To ensure a valid read of the RTC value, the HIBRTCC register should be read first, followed
    by a read of the RTCSSC field in the HIBRTCSS register and then a re-read of the HIBRTCC register.
    If the two values for the HIBRTCC are equal, the read is valid. By following this procedure, errors
    in the application caused by the HIBRTCC register rolling over by a count of 1 during a read of the
    RTCSSC field are prevented. The RTC can be configured to generate an alarm by setting the RTCAL0
    bit in the HIBIM register. When an RTC match occurs, an interrupt is generated and displayed in
    the HIBRIS register. Refer to “RTC Match - Seconds/Subseconds Mode” on page 499 for more
    information.


    If the RTC is enabled, only a cold POR, where both VBAT and VDD are removed, resets the RTC
    registers. If any other reset occurs while the RTC is enabled, such as an external RST assertion or
    BOR reset, the RTC is not reset. The RTC registers can be reset under any type of system reset
    as long as the RTC and external wake pins are not enabled.


    7.3.5.2 RTC Match - Seconds/Subseconds Mode
    The Hibernation module includes a 32-bit match register, HIBRTCM0, which is compared to the
    value of the RTC 32-bit counter, HIBRTCC. The match functionality also extends to the sub-seconds
    counter. The 15-bit field (RTCSSM) in the HIBRTCSS register is compared to the value of the 15-bit
    sub-seconds counter. When a match occurs, the RTCALT0 bit is set in the HIBRIS register. For
    applications using Hibernate mode, the processor can be programmed to wake from Hibernate
    mode by setting the RTCWEN bit in the HIBCTL register. The processor can also be programmed to
    generate an interrupt to the interrupt controller by setting the RTCALT0 bit in the HIBIM register.
    The match interrupt generation takes priority over an interrupt clear. Therefore, writes to the RTCALT0
    bit in the Hibernation Interrupt Clear (HIBIC) register do not clear the RTCALT0 bit if the HIBRTCC
    value and the HIBRTCM0 value are equal. There are several methodologies to avoid this occurrence,
    such as writing a new value to the HIBRTCLD register prior to writing the HIBIC to clear the RTCALT0.
    Another example, would be to disable the RTC and re-enable the RTC by clearing and setting the
    RTCEN bit in the HIBCTL register.