Other Parts Discussed in Thread: TAA3040
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAA3040 工具/软件:
尊敬的团队:
客户希望使用 TAA3040实现单通道音频输入、并输出 I2S 格式数据、如下图所示、您能否帮助提供此用例的示例配置代码?

谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、
请参阅示例配置(这源自数据表中给出的4通道配置):
# # Power up IOVDD and AVDD power supplies keeping SHDNZ pin voltage LOW # Wait for IOVDD and AVDD power supplies to settle to steady state operating voltage range. # Release SHDNZ to HIGH. # Wait for 1ms. # # Wake-up device by I2C write into P0_R2 using internal AREG w 98 02 81 # #Configure the device for 24-bit I2S operation by I2C write into P0_R7 w 98 07 60 # # Enable Input Ch-1 by I2C write into P0_R115 w 98 73 80 # # Enable ASI Output for Ch-1 slots by I2C write into P0_R116 w 98 74 80 # # Power-up ADC, MICBIAS and PLL by I2C write into P0_R117 w 98 75 E0
也可以使用适用于 TAA3040的 PPC3 GUI 推导出所需的配置、我建议客户可以从产品文件夹申请访问 GUI:
TAA3040数据表、产品信息和支持|德州仪器 TI.com

谢谢。此致、
Lakshmi Narasimhan