Other Parts Discussed in Thread: TPA3128D2
您好,
客户需要振荡器频率400kHz和1200Hz上TPA3128D2的频率与THD+N图。
如果TI没有这些数据,您是否会通过以下条件来测量这些数据?
PVCC=24V,增益=26dB,RL=4Ω Ω,BTL,PO=1W / 15W
用于测量的LC滤波器和LPF的截止频率 应设置 在50kHz左右。
此致,
Akio Ito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.