This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28388D:CLB_OUTPUT_XBAR 连接到 GPIO

Guru**** 2979400 points

Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1515065/tms320f28388d-clb_outputs-to-gpio-via-clb_output_xbar

器件型号:TMS320F28388D
主题:SysConfig 中讨论的其他器件

工具/软件:

您好、

 尝试 通过 LUT4然后将 CLB_OUTPUT_XBAR 路由到 GPIO92。  我使用逐位寄存器配置来执行此操作。问题是 GPIO92保持为零。

1. 我使用的代码如下:

  100MHz 的 CLB 时钟从25MHz 晶体振荡器的 AUXPLL 生成。

    InitAuxPll(XTAL_OSC, AUX_IMULT, AUX_REFDIV, AUX_ODIV, AUX_DIV, SYSCTL_DCC_BASE1);

    //
    // Set up CMCLK to use AUXPLL as the clock source and set the
    // clock divider to 1.
    //
    EALLOW;
    ClkCfgRegs.CMCLKCTL.bit.CMCLKDIV = 0;    // 0 : Divide by 1
    ClkCfgRegs.CMCLKCTL.bit.CMDIVSRCSEL = 0; // 0 : AuxPLL is the source for the CM clock divider.
    ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV      =   0x1;                            /*  EPWM Clock Division Select (EPWMCLKDIV): "00" - /1 of PLLSYSCLK, "01"-/2 of PLLSYSCLK(default) */
    ClkCfgRegs.PERCLKDIVSEL.bit.EMIF1CLKDIV     =   0x1;                            /*  EMIF1 module  Clock division select : "0" - /1 of PLLSYSCLK is selected "1"- /2 of PLLSYSCLK is selected */
    ClkCfgRegs.CLKSRCCTL3.bit.XCLKOUTSEL        =   0X4;
    ClkCfgRegs.CLBCLKCTL.bit.CLKMODECLB2        =   0x1;                            /* "0" - CLB2 is synchronous to SYSCLK,  1 : CLB2 runs of asynchronous clock*/
    asm(" RPT #69 || NOP");                                                         /* Delay of 69 nop cycles ,Refer TRM */
    ClkCfgRegs.CLBCLKCTL.bit.CLBCLKDIV          =   0x0;                            /* CLB Module clock division select : "0"- /1 of AUXPLL is selected "1"- /2 of AUXPLL is selected */
    asm(" RPT #69 || NOP");                                                         /* Delay of 69 nop cycles ,Refer TRM */
    ClkCfgRegs.CLBCLKCTL.bit.TILECLKDIV         =   0x0;                            /* "0" - /1, "1" - /2*/
    DevCfgRegs.CPUSEL15.bit.CLB2                =   0x0;                            /* "0" - CLB2 is connected to CPU1,  1 : CLB2 is connected to CPU2*/
 
   

  使用  CpuSysRegs.PCLKCR17寄存器启用 CLB 时钟。

  CLB2 PRESCALR 时钟作为输入信号通过本地多路复用器选择提供给逻辑块、然后提供给 LUT4。                                                                                                            

{
  EALLOW;
  Clb2LogicCtrlRegs.CLB_LOCK.all                   = 0x5A5A0000;                                 /* Unlock CLB1 registers*/
/*---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------*/
/* PRESCALER REGISTER CONTROL */
/*---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------*/
  Clb2LogicCtrlRegs.CLB_PRESCALE_CTRL.bit.CLKEN    = 0x1;                                        /* Enable the prescale clock/strobe generator.*/
  Clb2LogicCtrlRegs.CLB_PRESCALE_CTRL.bit.STRB     = 0x1;                                        /* When set to 1, the output of the counter register bit position as selected by TAP_SELECT_VALUE will be sent out.*/
  Clb2LogicCtrlRegs.CLB_PRESCALE_CTRL.bit.TAP      = 0x2;                                        /* When set to 2,0010 selects Counter Bit position 2 = 12.5MHz*/
  Clb2LogicCtrlRegs.CLB_PRESCALE_CTRL.bit.PRESCALE = 0x0009;                                     /* 10 Counts is set for generating 10MHz clock from 100MHz*/
/*---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------*/
/* CLB2_PRESCALE_CLK TO GPIO */
/*---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------*/
  Clb2LogicCtrlRegs.CLB_LCL_MUX_SEL_1.bit.LCL_MUX_SEL_IN_0    = 31;//21;                         /* Connecting CLB2_PRESCALAR CLOCK as Input0 */
  Clb2LogicCtrlRegs.CLB_LCL_MUX_SEL_1.bit.MISC_INPUT_SEL_0    = 0;//0;                           /* Setting this bit to 0 will select Local Mux for Input 0  instead of MISC_INPUT*/
  Clb2LogicCtrlRegs.CLB_INPUT_FILTER.bit.SYNC0                = 1;                               /* Synchronizer is selected for INPUT 0(which adds 2 or 3 cycles delay)*/
  Clb2LogicCtrlRegs.CLB_INPUT_FILTER.bit.FIN0                 = 0x0;                             /* No filtering*/
  Clb2LogicCtrlRegs.CLB_IN_MUX_SEL_0.bit.SEL_GP_IN_0          = 0x0;                             /* Input comes from selected external input,This register Select control for Input 0 to decide between external input and CLB_GP_REG[0]*/
  Clb2LogicCtrlRegs.CLB_GP_REG.bit.REG                        = 0x01;                            /* Writing a value of 1*/
  Clb2LogicCtrlRegs.CLB_INPUT_FILTER.bit.PIPE0                = 0x0;                             /* Disabling pipelining for the input asynchronous signal*/
  Clb2LogicCfgRegs.CLB_LUT4_IN0.bit.SEL_0                     = 24;                              /* Routing the CLB2_IN0 to LUT4_IN0 through static switch block*/
  Clb2LogicCfgRegs.CLB_LUT4_IN1.bit.SEL_0                     = 0;                               /* Output low for the 2nd input of LUT4*/
  Clb2LogicCfgRegs.CLB_LUT4_IN2.bit.SEL_0                     = 0;                               /* Output low for the 3rd input of LUT4*/
  Clb2LogicCfgRegs.CLB_LUT4_IN3.bit.SEL_0                     = 0;                               /* Output low for the 4th input of LUT4*/
  Clb2LogicCfgRegs.CLB_LUT4_FN1_0.bit.FN0                     = 0xAAAA;                          /* Look up Table Output function,Output follows input*/
  Clb2LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.IN0                   = 7;                               /* In static switch block,LUT4_4_OUTPUT*/
  Clb2LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.IN1                   = 0;                               /* Input 1 is tied to 0*/
  Clb2LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.IN2                   = 0;                               /* Input 2 is tied to 0*/
  Clb2LogicCfgRegs.CLB_OUTPUT_LUT_0.bit.FN                    = 0xAA;                            /* Look up Table Output function,Output follows input*/
  Clb2LogicCfgRegs.CLB_MISC_ACCESS_CTRL.bit.BLKEN             = 0;                               /* "0" Writes to CLB_OUT_EN are allowed*/
  Clb2LogicCtrlRegs.CLB_OUT_EN                                = 1<<0;                            /* Bit "0" is set for OUTLUT0 TO CLB2_OUT0 */

CLB2_OUT0通过 CLB_OUTPUTXBAR 连接到 GPIO92              

  EALLOW;
  ClbOutputXbarRegs.OUTPUT2MUX0TO15CFG.bit.MUX8              = 0x0;                             /* 00 :  Select .0 input for Mux8*/
  ClbOutputXbarRegs.OUTPUT2MUXENABLE.bit.MUX8                = 1;                               /* Respective output of Mux8 is enabled to drive the OUTPUT0 of OUTPUT-XBAR2*/
  ClbOutputXbarRegs.OUTPUTLATCHENABLE.bit.OUTPUT2            = 0;                               /* 0: Output Latch is not selected to driven the respective output*/

 

问题1 -是否需要其他寄存器配置、或者是否缺少某些寄存器?

问题 2 -  LUT 16位函数寄存器的工作原理是什么?

问题 3 -如何从32位 CLB_OUT_EN 寄存器中选择 CLB_OUT 信号?

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    您能否测试仅将 OUTLUT 配置为1或0是否成功修改 GPIO 输出? 这将排除任何 GPIO 多路复用或 CLB 启用/禁用问题。

    谢谢您、

    Luke

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Luke、

    已从 GPIO 配置 OUTLUT 的输入、该输入 通过输入 X-BAR 用作开关作为全局输入信号。仍然 GPIO 输出 保持零。我们是否可以绕过其他子模块直接将输入提供给 OUTLUT?是否有任何其他选项?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您能否测试我们的一个 CLB 软件示例? 我怀疑未正确启用 CLB。 我们的示例基于 SysConfig、但至少会指导您创建正确的位字段代码。

    谢谢您、

    Luke