This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025C:问题 CMPSS/ADC (我猜是配置错误?)

Guru**** 2943350 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1068840/tms320f280025c-issue-cmpss-adc-configuration-mistake-i-suppose

部件号:TMS320F280025C
“线程:测试”中讨论的其它部件

您好,专家,

我的 cmps. 我在微控制器上设置了不同的 ADC 条目,以通过 ISR 以及其他连接到 cmpss 的条目覆盖其读数,从而剪切我的 ePWM。 但是,我注意到,通过测试,我的所有条目,即使是在 ADC 读取中使用的条目,都剪切了我不想要的 ePWM。

我是否未正确设置 cmpss 模块? 我加入了我的代码:

void cmpss_init()
{
    // Enable CMPSS and configure the negative input signal to come from the DAC
    CMPSS_enableModule(CMPSS1_BASE);
    CMPSS_enableModule(CMPSS2_BASE);
    CMPSS_enableModule(CMPSS3_BASE);
    CMPSS_enableModule(CMPSS4_BASE);

    // Use VDDA as the reference for the DAC and set DAC value to midpoint for arbitrary reference.
    CMPSS_configDAC(CMPSS1_BASE, CMPSS_DACREF_VDDA);
    CMPSS_configDAC(CMPSS2_BASE, CMPSS_DACREF_VDDA);
    CMPSS_configDAC(CMPSS3_BASE, CMPSS_DACREF_VDDA);
    CMPSS_configDAC(CMPSS4_BASE, CMPSS_DACREF_VDDA);

    // To use CMP1_HP2 pin A6 for MU_TRAC_BATT_PCH
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1, 2);
    // To use CMP1_LP3 pin A15/C7 for MU_FUEL_CELL_PCH
    ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_1, 3);
    // To use CMP3_HP1 pin A5/C2 for MI_L_W
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_3, 1);
    // To use CMP2_HP1 pin A12/C1 for MI_L_U
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_2, 1);
    // To use CMP2_LP4 pin A8/C11 for MI_L_V
    ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_2, 4);
    // To use CMP4_HP1 pin A7/C3 for MI_TRAC_BATT
    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_4, 1);

    // Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.
    //1
    CMPSS_configHighComparator(CMPSS1_BASE, CMPSS_INSRC_DAC);              // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS1_BASE, max_dac_cmpss);                     // Define threshold
    CMPSS_configOutputsHigh(CMPSS1_BASE, CMPSS_TRIP_SYNC_COMP);            // Set output comparator (synchronous or asynchronous)
    //2
    CMPSS_configLowComparator(CMPSS1_BASE, CMPSS_INSRC_DAC);               // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueLow(CMPSS1_BASE, max_dac_cmpss);                      // Define threshold
    CMPSS_configOutputsLow(CMPSS1_BASE, CMPSS_TRIP_SYNC_COMP);             // Set output comparator (synchronous or asynchronous)

    // Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.
    //1
    CMPSS_configHighComparator(CMPSS2_BASE, CMPSS_INSRC_DAC);              // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS2_BASE, max_dac_cmpss);                     // Define threshold
    CMPSS_configOutputsHigh(CMPSS2_BASE, CMPSS_TRIP_SYNC_COMP);            // Set output comparator (synchronous or asynchronous)
    //2
    CMPSS_configLowComparator(CMPSS2_BASE, CMPSS_INSRC_DAC);               // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueLow(CMPSS2_BASE, max_dac_cmpss);                      // Define threshold
    CMPSS_configOutputsLow(CMPSS2_BASE, CMPSS_TRIP_SYNC_COMP);             // Set output comparator (synchronous or asynchronous)

    // Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.
    //1
    CMPSS_configHighComparator(CMPSS3_BASE, CMPSS_INSRC_DAC);              // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS3_BASE, max_dac_cmpss);                     // Define threshold
    CMPSS_configOutputsHigh(CMPSS3_BASE, CMPSS_TRIP_SYNC_COMP);            // Set output comparator (synchronous or asynchronous)

    // Configure the output signals. Both CTRIPH will be fed by the asynchronous comparator output.
    //1
    CMPSS_configHighComparator(CMPSS4_BASE, CMPSS_INSRC_DAC);              // Threshold drive by GPIO or input DAC
    CMPSS_setDACValueHigh(CMPSS4_BASE, max_dac_cmpss);                     // Define threshold
    CMPSS_configOutputsHigh(CMPSS4_BASE, CMPSS_TRIP_SYNC_COMP);            // Set output comparator (synchronous or asynchronous)

    // Configure TRIP4 to be CTRIP1H using the ePWM X-BAR. Attach CMPSS output to TRIPINx via EPWMXBAR module
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX01_CMPSS1_CTRIPL);
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX04_CMPSS3_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX02_CMPSS2_CTRIPH);
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX03_CMPSS2_CTRIPL);
    XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX06_CMPSS4_CTRIPH);

    // See the ePWM X-BAR Mux configuration table, see Crossbar(X-BAR) doc for more informations
    XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00 | XBAR_MUX01 | XBAR_MUX04 | XBAR_MUX02 | XBAR_MUX03 | XBAR_MUX06);
}

void cmpss_actions(base)
{
    // Configure ePWMx to output low on TZx TRIP
    EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
    EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW);

    // Trigger event when DCBH is high
    EPWM_setTripZoneDigitalCompareEventCondition(base, EPWM_TZ_DC_OUTPUT_B1, EPWM_TZ_EVENT_DCXH_HIGH);

    // Configure DCBH to use TRIP4 as an input
    EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN4, EPWM_DC_TYPE_DCBH);

    // Enable DCB as OST
    EPWM_enableTripZoneSignals(base, EPWM_TZ_SIGNAL_DCBEVT1);

    // Clear trip flags
    EPWM_clearTripZoneFlag(base, EPWM_TZ_FLAG_DCBEVT1);
}
void adc_config(uint32_t adc_base)
{
    // Enable ADC
    ADC_setVREF(adc_base, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V);

    ADC_setPrescaler(adc_base, ADC_CLK_DIV_1_0);

    // Set pulse ADCINTx at the end of conversion
    ADC_setInterruptPulseMode(adc_base, ADC_PULSE_END_OF_CONV);

    if(adc_base == ADCA_BASE)
    {
        // Configure the SOC to occur on the first up-count event
        EPWM_setADCTriggerSource(EPWM1_BASE, EPWM_SOC_A, EPWM_SOC_TBCTR_U_CMPA);
        // To set ADCCLK
        EPWM_setADCTriggerEventPrescale(EPWM1_BASE, EPWM_SOC_A, ADC_PRESCALE);

        EPWM_enableADCTrigger(EPWM1_BASE, EPWM_SOC_A);
    }

    ADC_enableConverter(adc_base);

    //Delay to allow ADC time to power up
    DEVICE_DELAY_US(adc_powerup_us);
}

void adc_init_soc(void)
{
    // Corresponding module ADCx -> SOC -> pin. Enchainement des SOC une fois la conversion terminée sur un SOC.SOC0 will start at 1 / PWM_FREQ and an another SOC0 at 1 / PWM_FREQ after.

    // MU_TRAC_BATT_FLT with pin ADCINA3
    ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN3, ADC_ACQPS_WINDOW);

    // MU_FUEL_CELL_FLT with pin ADCINA2
    ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER1, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN2, ADC_ACQPS_WINDOW);

    // MI_TRAC_BATT_FLT with pin ADCINA14
    ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER2, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN14, ADC_ACQPS_WINDOW);

    // MU_FUEL_CELL_PCH_FLT with pin ADCINA0
    ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER3, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN0, ADC_ACQPS_WINDOW);

    // MU_TRAC_BATT_PCH_FLT with pin ADCINC6
    ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN6, ADC_ACQPS_WINDOW);

    // MT_COLD_PLATE_FLT with pin ADCINC0
    ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER1, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN0, ADC_ACQPS_WINDOW);

    // MI_L_U_FLT with pin ADCINC14
    ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER2, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN14, ADC_ACQPS_WINDOW);

    // MI_L_V_FLT with pin ADCINC8
    ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER3, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN8, ADC_ACQPS_WINDOW);

    // MI_L_W_FLT with pin ADCINC10
    ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER4, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN10, ADC_ACQPS_WINDOW);

    // Corresponding EOC to ADCINTX pulse to enter on interrupt for read ADCRESULTx registers. Refer to ADCINTSEL1N2 and ADCRESULTx registers.
    ADC_setInterruptSource(ADCC_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER4);

    ADC_enableInterrupt(ADCC_BASE, ADC_INT_NUMBER1);

    ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
}

__interrupt void isr_adc(void) // Enter on interrupt when SOC3 on ADCC will end.
{
    MU_TRAC_BATT_PCH_FLT_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER0);
    MT_COLD_PLATE_FLT_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER1);
    MI_L_U_FLT_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER2);
    MI_L_V_FLT_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER3);
    MI_L_W_FLT_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER4);

    MU_TRAC_BATT_FLT_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER0);
    MU_FUEL_CELL_FLT_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER1);
    MI_TRAC_BATT_FLT_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER2);
    MU_FUEL_CELL_PCH_FLT_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER3);

    adc_convert_samples_digit_to_analog();

    // Clear the interrupt flag
    ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);

    // Check if overflow has occurred
    if(ADC_getInterruptOverflowStatus(ADCC_BASE, ADC_INT_NUMBER1) == true)
    {
        ADC_clearInterruptOverflowStatus(ADCC_BASE, ADC_INT_NUMBER1);
        ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
    }

    // Acknowledge the interrupt, see PIE Interrupt Vectors  table
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}

谢谢

达米恩

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Damien,

    我看到您配置了 ePWM 以触发 ADC 对某些信道进行采样,而 CMPSSS 配置为跳闸 ePWM。 但是,我不清楚你所面临的问题。 您能解释什么不起作用吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,弗兰克,

    我采样了9 个 ADC 通道,我还拥有 6个连接到 cmpss 的条目。 我想在触发 cmpss 时关闭 PWM,比较是通过 DAC 阈值(我的代码中为“max_DAC_cmpss”)进行的。 当我只测试电流时,触发器已正确完成,但当我对 ADC 输入施加电压时,ADC 的读数已正确完成,但如果超过 DAC 的阈值,我认为 PWM 将通过电流电流关闭。 但是,这不应该是因为它是 ADC 的简单读数。 但是,我已经检查了我的代码,没有发现任何错误。 这是否是地图绘制问题? 或者... ?

    谢谢

    达米恩

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    我解决了我的问题,当我测试我的所有输入与潜力无关。  所以我有一些浮势引脚,这些引脚必须干扰微控制器(ADC 读取的值高于关闭阈值)。  现在,通过在我的 cmpss 输入以及用于读取 ADC 的输入上应用电位,一切都可以正常工作。

    感谢你的回复

    达米恩

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Damien,

    很高兴听到您解决了这个问题。 如果出现更多问题,请告诉我们。