尊敬的C2000团队:
我正在尝试使用F2.8034万旋转电机,但连接电机后,仿真器(XDS100)无法工作。 我认为这可能是由于噪音造成的,因为如果电机断开,XDS100工作正常。
我看到TI的所有控制卡都实现了隔离器,它可以隔离F2803x和XDS100之间的信号,我想使用类似的方法来查看它是否工作。 是否有任何隔离模块可以隔离芯片和XDS100?
此致,
千斤顶
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的C2000团队:
我正在尝试使用F2.8034万旋转电机,但连接电机后,仿真器(XDS100)无法工作。 我认为这可能是由于噪音造成的,因为如果电机断开,XDS100工作正常。
我看到TI的所有控制卡都实现了隔离器,它可以隔离F2803x和XDS100之间的信号,我想使用类似的方法来查看它是否工作。 是否有任何隔离模块可以隔离芯片和XDS100?
此致,
千斤顶
Jack,您好!
使用铁氧体是一个很好的选择。
正如您所建议的,还有可用的隔离适配器,例如Blackhawk-DSP的BH-ADP-ISO14:
http://www.ti.com/tool/TMDSADP
谢谢!
Brett
您好,Gautam:
我不确定这是不是自定义主板。 我从互联网上购买了XDS100 wiki页面推荐的产品。 此USB隔离适配器的全速为12MHz。
processors.wiki.ti.com/.../XDS100
此致,
杰克丹