请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TMS320F2.8379万D 读者好!
参考主题微控制器,我对使用PWM模块11和12感到困惑。根据数据表,它们在GPIO 165-168上可用。但如果我们看到F2.8379万D坞站的引脚布局, 此处不存在120-160的GPIO。如果我们的应用需要使用此控制器的所有12个PWM模块,我们如何访问这些模块。
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
读者好!
参考主题微控制器,我对使用PWM模块11和12感到困惑。根据数据表,它们在GPIO 165-168上可用。但如果我们看到F2.8379万D坞站的引脚布局, 此处不存在120-160的GPIO。如果我们的应用需要使用此控制器的所有12个PWM模块,我们如何访问这些模块。
谢谢你