我有F2.8069万M启动板,它最初运行良好,我可以进行代码处理,没有任何问题。 现在当我尝试在MATLAB中转储代码时,它会给我一个错误,说XDS100未通电。 我注意到,当我正确连接主板D4和D1时, D10会闪烁一次,D1和D4 LED的亮度立即降低。 所以我用万用表检查了5V和3.3V电源,两个都显示为1.7V。
我还为您的reference.e2e.ti.com/.../VID_2D00_2018.011万_2D00_WA0001.mp4附加0001.附加了视频
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有F2.8069万M启动板,它最初运行良好,我可以进行代码处理,没有任何问题。 现在当我尝试在MATLAB中转储代码时,它会给我一个错误,说XDS100未通电。 我注意到,当我正确连接主板D4和D1时, D10会闪烁一次,D1和D4 LED的亮度立即降低。 所以我用万用表检查了5V和3.3V电源,两个都显示为1.7V。
我还为您的reference.e2e.ti.com/.../VID_2D00_2018.011万_2D00_WA0001.mp4附加0001.附加了视频
您好Mark
很抱歉回复太晚。 当我移除JP1和JP2时,D4 LED正常闪烁,但当我连接JP1和JP2时,D4和D1会更亮一秒,然后D10会在此D4和D1变为低电平后闪烁。 所以我得出结论,XDS100端没有问题,微控制器端也有问题。 但是经过一天的测试,我对主板的JP1和JP2的性能很好,我没有做任何改变。
我不知道是什么让板工作正常,看到板工作时我很惊讶。
但是我在另一个launchxl f2.8069万M板上看到了同样的问题,即使在这个板上,XDS100在没有JP1和JP2的情况下也能正常工作。 我从过去3天开始尝试解决此问题。 如果您提供调试问题所需遵循的步骤,将会很有帮助。
谢谢
Vigneshwar