Other Parts Discussed in Thread: C2000WARE
主题中讨论的其他部件:C2000WARE
大家好,
使用CCS 10.4 ,我将I2C功能添加到一个项目中,这个项目以TIREX示例“Example_2802xScia_FFDLB.c”开始,如下所示:
//############################################################################# // // File: Example_F2802xSci_FFDLB.c // // Title: F2802x Device SCI FIFO Digital Loop Back Test. // //! \addtogroup example_list //! <h1>SCI FIFO Digital Loop Back</h1> //! //! This test uses the loopback test mode of the SCI module to send //! characters starting with 0x00 through 0xFF. The test will send //! a character and then check the receive buffer for a correct match. //! //! Watch Variables: //! - LoopCount - Number of characters sent //! - ErrorCount - Number of errors detected //! - SendChar - Character sent //! - ReceivedChar - Character received // //############################################################################# // $TI Release: $ // $Release Date: $ // $Copyright: // Copyright (C) 2009-2022 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include <stdio.h> #include <file.h> #include "common/include/adc.h" #include "common/include/clk.h" #include "common/include/flash.h" #include "common/include/gpio.h" #include "common/include/pie.h" #include "common/include/pll.h" #include "common/include/sci.h" #include "common/include/wdog.h" // // Function Prototypes // void scia_init(void); void scia_fifo_init(void); void scia_xmit(int a); void error(void); // // Globals // uint16_t LoopCount; uint16_t ErrorCount; ADC_Handle myAdc; CLK_Handle myClk; FLASH_Handle myFlash; GPIO_Handle myGpio; PIE_Handle myPie; SCI_Handle mySci; // // Main // void main(void) { uint16_t SendChar; uint16_t ReceivedChar; CPU_Handle myCpu; PLL_Handle myPll; WDOG_Handle myWDog; // // Initialize all the handles needed for this application // myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj)); myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj)); myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj)); myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj)); myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj)); myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj)); myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj)); mySci = SCI_init((void *)SCIA_BASE_ADDR, sizeof(SCI_Obj)); myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj)); // // Perform basic system initialization // WDOG_disable(myWDog); CLK_enableAdcClock(myClk); (*Device_cal)(); // // Select the internal oscillator 1 as the clock source // CLK_setOscSrc(myClk, CLK_OscSrc_Internal); // // Setup the PLL for x10 /2 which will yield 50Mhz = 10Mhz * 10 / 2 // PLL_setup(myPll, PLL_Multiplier_10, PLL_DivideSelect_ClkIn_by_2); // // Disable the PIE and all interrupts // PIE_disable(myPie); PIE_disableAllInts(myPie); CPU_disableGlobalInts(myCpu); CPU_clearIntFlags(myCpu); // // If running from flash copy RAM only functions to RAM // #ifdef _FLASH memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); #endif // // Setup GPIO // GPIO_setPullUp(myGpio, GPIO_Number_28, GPIO_PullUp_Enable); GPIO_setPullUp(myGpio, GPIO_Number_29, GPIO_PullUp_Disable); GPIO_setQualification(myGpio, GPIO_Number_28, GPIO_Qual_ASync); GPIO_setMode(myGpio, GPIO_Number_28, GPIO_28_Mode_SCIRXDA); GPIO_setMode(myGpio, GPIO_Number_29, GPIO_29_Mode_SCITXDA); // // Setup a debug vector table and enable the PIE // PIE_setDebugIntVectorTable(myPie); PIE_enable(myPie); LoopCount = 0; ErrorCount = 0; scia_init(); // Initialize SCI for digital loop back scia_fifo_init(); // Initialize the SCI FIFO // // Send a character starting with 0 // SendChar = 0; // // Send Characters forever starting with 0x00 and going through 0xFF. // After sending each, check the receive buffer for the correct value // for(;;) { SCI_putDataBlocking(mySci, SendChar); while(SCI_getRxFifoStatus(mySci) == SCI_FifoStatus_Empty) { } // // Check received character // ReceivedChar = SCI_getData(mySci); if(ReceivedChar != SendChar) { error(); } // // Move to the next character and repeat the test // SendChar++; // // Limit the character to 8-bits // SendChar &= 0x00FF; LoopCount++; } } // // Step 7. Insert all local Interrupt Service Routines (ISRs) and // functions here: // // // error - // void error(void) { ErrorCount++; __asm(" ESTOP0"); // Uncomment to stop the test here for (;;) { } } // // scia_init - // void scia_init() { CLK_enableSciaClock(myClk); // // 1 stop bit, No loopback, No parity,8 char bits, async mode, // idle-line protocol // SCI_disableParity(mySci); SCI_setNumStopBits(mySci, SCI_NumStopBits_One); SCI_setCharLength(mySci, SCI_CharLength_8_Bits); // // enable TX, RX, internal SCICLK, Disable RX ERR, SLEEP, TXWAKE // SCI_enableTx(mySci); SCI_enableRx(mySci); SCI_enableTxInt(mySci); SCI_enableRxInt(mySci); SCI_enableLoopBack(mySci); //SCI BRR = LSPCLK/(SCI BAUDx8) - 1 #if (CPU_FRQ_50MHZ) SCI_setBaudRate(mySci, SCI_BaudRate_9_6_kBaud); #elif (CPU_FRQ_40MHZ) SCI_setBaudRate(mySci, (SCI_BaudRate_e)129); #endif SCI_enable(mySci); return; } // // scia_fifo_init - Initialize the SCI FIFO // void scia_fifo_init() { SCI_enableFifoEnh(mySci); SCI_resetTxFifo(mySci); SCI_clearTxFifoInt(mySci); SCI_resetChannels(mySci); SCI_setTxFifoIntLevel(mySci, SCI_FifoLevel_Empty); SCI_resetRxFifo(mySci); SCI_clearRxFifoInt(mySci); SCI_setRxFifoIntLevel(mySci, SCI_FifoLevel_4_Words); return; } // // End of File //
此代码及其包含的项目是从以下路径中的资源资源管理器导入的:
/Software/C2000Ware (4.01 .00.00)/English/Devices/F2802x/F28020/Examples/DriverLib/scia_loopback/Example_2802xScia_FFDLB.c</s>2.802万 2802
SCIA通信运行良好,现在我尝试添加简单的I2C写入功能。
另外,我还修改了C2000Ware的Bitfiled Example_2802xI2C_EEPROM.c,以满足I2C需求,而且工作正常。 现在我将功能从I2C位域示例移到SCIA Driverlib示例代码中。
完成后,RS232命令将通过SCIA模块接收,解析,并通过I2C发送到外围设备。
第一步是将I2C初始化函数插入到SCIA Driverlib示例代码中。 下面是我创建并插入的功能:
//
// Start I2C_init() Initialization Routine
//
void
I2C_init()
{
EALLOW;
// Initialize I2C
I2caRegs.I2CMDR.bit.IRS = 0; // SEE BELOW - Put I2C module in reset while making changes
//
// Own Address Register
// // Bit 15: READ ONLY - Reserved
I2caRegs.I2COAR = 0x40; // Own address = 0x40
I2caRegs.I2CSAR = 0x44; // Bits 0-9: Address to which data will be transmitted (Master only)
/* // Bits 7-15: Reserved
//
// I2C Interrupt Enable Register
//
#ifdef BIT_SET_REGISTERS
// Bits 7-15: READ ONLY - Reserved
I2caRegs.I2CIER.bit.AAS = 0; // Bit 6: 1 = Addressed as slave interrupt request enabled
I2caRegs.I2CIER.bit.SCD = 0; // Bit 5: 1 = Stop condition detected interrupt request enabled
I2caRegs.I2CIER.bit.XRDY = 0; // Bit 4: 1 = Transmit data ready interrupt request disabled
I2caRegs.I2CIER.bit.RRDY = 0; // Bit 3: 1 = W1C - Receive data ready interrupt request enabled
I2caRegs.I2CIER.bit.ARDY = 0; // Bit 2: 1 = Master Only - Register access ready interrupt request enabled
I2caRegs.I2CIER.bit.NACK = 0; // Bit 1: 0 = W1C - No-ack interrupt request disabled
I2caRegs.I2CIER.bit.ARBL = 0; // Bit 0: 0 = W1C - Arbitration lost interrupt request disabled
#else
I2caRegs.I2CIER.all = 0x0000; // Per above bit settings
#endif
//
// I2C Status Register
//
#ifdef BIT_SET_REGISTERS
// Bit 15: READ ONLY - Reserved
I2caRegs.I2CSTR.bit.SDIR = 0; // Bit 14: W1C - Slave direction bit 0 = not addressed as slave transmitter
I2caRegs.I2CSTR.bit.NACKSNT = 0; // Bit 13: W1C - NACK sent bit 0 = NACK not sent
I2caRegs.I2CSTR.bit.BB = 0; // Bit 12: Bus Busy bit 0 = bus free
I2caRegs.I2CSTR.bit.RSFULL = 0; // Bit 11: 1 = receive shift register overrun condition detected
I2caRegs.I2CSTR.bit.XSMT = 0; // Bit 10: 0 = transmit shift register underflow detected (empty)
I2caRegs.I2CSTR.bit.AAS = 0; // Bit 9: 1 = I2C module recognized its own slave address
I2caRegs.I2CSTR.bit.AD0 = 0; // Bit 8: 1 = address of all zeros (general call) was detected
// Bits 6-7: READ ONLY - Reserved
I2caRegs.I2CSTR.bit.SCD = 0; // Bit 5: W1C - 1 = stop condition was detected
I2caRegs.I2CSTR.bit.XRDY = 0; // Bit 4: 1 = Ready for more transmit data to go in I2CDXR
I2caRegs.I2CSTR.bit.RRDY = 0; // Bit 3: W1C - Receive data ready int flag 1 = data is in I2CDRR
I2caRegs.I2CSTR.bit.ARDY = 0; // Bit 2: Master Only - Register access ready int flag
I2caRegs.I2CSTR.bit.NACK = 0; // Bit 1: W1C - 1 = NACK received
I2caRegs.I2CSTR.bit.ARBL = 0; // Bit 0: W1C - 1 = arbitration lost
#else
I2caRegs.I2CSTR.all = 0x0000; // Per above bit settings
#endif
//
// I2C Clock Prescale Register
//
// Setup I2C data rate
I2caRegs.I2CPSC.bit.IPSC = 5; // Prescaler value 60mHz SYSCLK / 6 = 10mHz (5+1=6)
//
// I2C Clock high-time and low-time Registers
//
// 10mHz / 200 = 50kHz for comm's with 2x16 debugging display
I2caRegs.I2CCLKL = 129; // 129 + 5 = 136
I2caRegs.I2CCLKH = 61; // 61 + 5 = 66
//
// Data Count Register
//
I2caRegs.I2CCNT = 0; // Bits 0-15: Set data count (ignored in RM mode)
// Is changed to actual number of bytes to transfer when in
// transmit mode.
//
// Slave Address Register
// // Bits 10-15: READ ONLY - Reserved
I2caRegs.I2CSAR = 0x44; // Bits 0-9: Address to which data will be transmitted (Master only)
//
// Data transmit register
//
I2caRegs.I2CDXR = 0x00;
//
// I2C Mode Register
//
#ifdef BIT_SET_REGISTERS
// Bits 14-15: READ ONLY - Reserved
I2caRegs.I2CMDR.bit.NACKMOD = 0; // Bit 15: NACK mode
I2caRegs.I2CMDR.bit.FREE = 0; // Bit 14: For debugging: 0 = I2C halts during interrupts
// I2caRegs.I2CMDR.bit.STT = 0; // Bit 13: Master only - Start bit Can't be written when IRS=0
// Bit 12: Reserved
// I2caRegs.I2CMDR.bit.STP = 0; // Bit 11: Master only - Stop bit Can't be written when IRS=0
I2caRegs.I2CMDR.bit.MST = 1; // Bit 10: Remains 0 for slave mode. 1 = Master mode
I2caRegs.I2CMDR.bit.TRX = 1; // Bit 9: 0 = Receive mode, 1 = Transmit mode
I2caRegs.I2CMDR.bit.XA = 0; // Bit 8: 0 = 7 bit address mode
I2caRegs.I2CMDR.bit.RM = 1; // Bit 7: 1 = repeat mode
I2caRegs.I2CMDR.bit.DLB = 0; // Bit 6: 0 = Digital loopback mode disabled
// I2caRegs.I2CMDR.bit.IRS = 1; // Bit 5: I2C module is re-enabled after making changes
I2caRegs.I2CMDR.bit.STB = 0; // Bit 4: Master only - Start Byte mode
I2caRegs.I2CMDR.bit.FDF = 0; // Bit 3: Keep at 0. Free data format mode
I2caRegs.I2CMDR.bit.BC = 0; // Bits 0-2: Set bit count to 8 bits (0 = 8)
#else
I2caRegs.I2CMDR.all = 0x06a0; // Per above bit settings
#endif
//
// I2C Extended Mode Register
// // Bits 1-15: READ ONLY - Reserved
I2caRegs.I2CEMDR.bit.BCM = 0; // Bit 0: Backwards compatibility mode
//
// Transmit FIFO Register
//
#ifdef BIT_SET_REGISTERS
// Bits 14-15: READ ONLY - Reserved
// Bit 15: Reserved
I2caRegs.I2CFFTX.bit.I2CFFEN = 0; // Bit 14: 1 = Enable transmit & receive FIFOs
I2caRegs.I2CFFTX.bit.TXFFRST = 0; // Bit 13: 1 = Take transmit FIFO out of reset
// I2caRegs.I2CFFTX.bit.TXFFST = 0; // Bits 8-12: READ ONLY - How many bytes are in the transmit FIFO
// I2caRegs.I2CFFTX.bit.TXFFINT = 0; // Bit 7: READ ONLY - 1 = interrupt occurred
I2caRegs.I2CFFTX.bit.TXFFINTCLR = 0; // Bit 6: W1C - Clears transmit interrupt flag (do again after irs = 1)
I2caRegs.I2CFFTX.bit.TXFFIENA = 0; // Bit 5: 0 = Disable transmit FIFO interrupt
I2caRegs.I2CFFTX.bit.TXFFIL = 0; // Bits 0-4: Set the transmit FIFO interrupt Threshold
#else
I2caRegs.I2CFFTX.all = 0x0000; // Per above bit settings
#endif
//
// Receive FIFO Register
//
#ifdef BIT_SET_REGISTERS
// Bits 14-15: READ ONLY - Reserved
I2caRegs.I2CFFRX.bit.RXFFRST = 0; // Bit 13: 1 = enable receive FIFO operation
// I2caRegs.I2CFFRX.bit.RXFFST = 0; // BitS 8-12: READ ONLY - Bytes in receive FIFO
// I2caRegs.I2CFFRX.bit.RXFFINT = 0; // Bit 7: READ ONLY - Receive interrupt flag 1 = int
I2caRegs.I2CFFRX.bit.RXFFINTCLR = 0; // Bit 6: Write 1 to clear receive int flag
I2caRegs.I2CFFRX.bit.RXFFIENA = 0; // Bit 5: 1 = receive interrupt is enabled
I2caRegs.I2CFFRX.bit.RXFFIL = 0; // Bits 0-4: Set the receive FIFO interrupt level
#else
I2caRegs.I2CFFRX.all = 0x0000; // Per above bit settings
#endif
*/
// Clean up and exit
I2caRegs.I2CMDR.bit.IRS = 1; // SEE ABOVE - I2C module is re-enabled after making changes
EDIS;
return;
}
/*
* End I2C_init()
*/
从上面的代码中可以看出,我尝试将每个寄存器设置为一个位,并尝试设置每个寄存器一个字。
该代码编译没有问题,上载到目标并正常运行,除了I2C寄存器没有更改。
代码运行,因此我在寄存器更改时设置了一个断点,然后逐步执行几行,这些行应该更改寄存器值。 观察“寄存器”视图和“内存浏览器”视图时,没有发生任何变化。
当我输入要写入寄存器的代码时,CCS将标识该寄存器的各种元素,我可以从列表中选择这些元素以自动填充:
问题:
1.此问题是否是由于将Bitfiled示例代码与Driverlib代码组合而导致的?
2.我是否遗漏了一些包含的内容?
3.在寄存器中写入数据以设置其值的正确方式是什么?
谢谢!
罗宾