我们计划将TMS320F2.8377万D用于我们的项目。
MCT6光耦合器连接到MCU的输出引脚,该引脚将为每个输出消耗10mA的输入正向电流,并且22个输出将持续接通。
在工作条件下,这是否安全?
如果不是,请帮助选择任何其他光耦合器IC,它们可用于替代MCT6,后者工作时所需的输入正向电流更少。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们计划将TMS320F2.8377万D用于我们的项目。
MCT6光耦合器连接到MCU的输出引脚,该引脚将为每个输出消耗10mA的输入正向电流,并且22个输出将持续接通。
在工作条件下,这是否安全?
如果不是,请帮助选择任何其他光耦合器IC,它们可用于替代MCT6,后者工作时所需的输入正向电流更少。
您好,Vineyesh,
根据我的理解,MCU输出(源4mA/引脚)作为隔离连接至MCT6,然后采用ULN2803A (吸收电流最大为1.35mA)-来自TI.com上提供的特定数据表信息。
根据您的要求,使用10mA中的22个输出将是不可行的。
如果在这种情况下,此应用可以使用<4mA/pin作为MCU输出和ULN2803A输出钳电流(最大 < 500mA)进行修改。 在大纲上,它似乎可以发挥作用。
最好先检查以下内容:
1.使用MCT6 (电流传输比率为50%)及其对ULN2803A的影响,无论是否达到负载电流要求。
2.就ULN2803A的应用提出意见。 请浏览以下备注:

如果您需要有关ULN2803A的更多特定于应用的详细信息。 我建议 就E2E论坛与ULN2803A专家联系。
如果您有任何与MCU (F2.8377万D)相关的具体问题,请告诉我。
最佳,
Uttam