This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F280049C:XDS110调试器错误错误-2131 @ 0x0

Guru**** 2538950 points
Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-F280049C

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1009099/launchxl-f280049c-xds110-debbuger-error-error--2131-0x0

器件型号:LAUNCHXL-F280049C
主题中讨论的其他器件:UNIFLASH

您好!

我获得了全新的 Launchpad F280049C、并尝试通过 CCS v10.3.1进行连接。 我总是收到此错误消息:

我尝试安装较旧的 EMU 包、如 https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/753823/faq-ccs-launchxl-f280049c-advisement-emupack-8-0-903-4-incompatible-with-launchxl-f280049c 上所示

但这不是解决方案。

我可以通过 Uniflash 对所有内容进行编程、擦除和读取、但 CCS 始终会抛出此错误。 TestOutput 如下所示:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\Flo\AppData\Local\TEXASI~1\CCS\
    ccs1031\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Apr 29 2021'.
The library build time was '17:49:40'.
The library package version is '9.3.0.00058'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End]

如何解决此问题?

谢谢!

弗洛里安