This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F280049C:XDS110调试器错误错误-2131 @ 0x0

Guru**** 2036780 points
Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-F280049C
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1009099/launchxl-f280049c-xds110-debbuger-error-error--2131-0x0

器件型号:LAUNCHXL-F280049C
主题中讨论的其他器件:UNIFLASH

您好!

我获得了全新的 Launchpad F280049C、并尝试通过 CCS v10.3.1进行连接。 我总是收到此错误消息:

我尝试安装较旧的 EMU 包、如 https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/753823/faq-ccs-launchxl-f280049c-advisement-emupack-8-0-903-4-incompatible-with-launchxl-f280049c 上所示

但这不是解决方案。

我可以通过 Uniflash 对所有内容进行编程、擦除和读取、但 CCS 始终会抛出此错误。 TestOutput 如下所示:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Flo\AppData\Local\TEXASI~1\CCS\
ccs1031\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Apr 29 2021'.
The library build time was '17:49:40'.
The library package version is '9.3.0.00058'.
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

如何解决此问题?

谢谢!

弗洛里安