This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28388D:配置目标时出错

Guru**** 2587345 points
Other Parts Discussed in Thread: TMDSHSECDOCK, C2000WARE, TMDSCNCD28388D

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/999015/tms320f28388d-error-when-configuring-target

器件型号:TMS320F28388D
主题中讨论的其他器件:TMDSHSECDOCKC2000WARETMDSCNCD28388D

大家好、

需要您对我们客户的问题提供专业知识。 他们使用 TMSF28388D 进行开发、并且在尝试在 CCS 中配置目标时遇到错误。 出现以下消息:

*请注意,最近日期的产品工作正常,但与主机 PC 的通信 突然中断。


提前感谢!


此致、

Jejomar




[Start: Texas Instruments XDS100v2 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\alexa\AppData\Local\TEXASI~1\CCS\
ccs1020\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Jan 31 2021'.
The library build time was '20:08:09'.
The library package version is '9.3.0.00042'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

There is no hardware for programming the JTAG TCLK frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

There is no hardware for measuring the JTAG TCLK frequency.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 64 32-bit words.

The test for the JTAG IR instruction path-length failed.
The JTAG IR instruction scan-path is stuck-at-ones.

The test for the JTAG DR bypass path-length failed.
The JTAG DR bypass scan-path is stuck-at-ones.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Test 2 Word 0: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 1: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 2: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 3: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 4: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 5: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 6: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 7: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 2, skipped: 0, failed: 1
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 2
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 3
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 4
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 5
Some of the values were corrupted - 83.3 percent.

The JTAG IR Integrity scan-test has failed.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Test 2 Word 0: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 1: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 2: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 3: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 4: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 5: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 6: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
Test 2 Word 7: scanned out 0x00000000 and scanned in 0xFFFFFFFF.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 2, skipped: 0, failed: 1
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 2
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 3
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 4
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 5
Some of the values were corrupted - 83.3 percent.

The JTAG DR Integrity scan-test has failed.

[End: Texas Instruments XDS100v2 USB Debug Probe_0]

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    此错误意味着扫描完整性检查失败、这是由于 JTAG 接头连接错误或电路板上的某些组件故障而发生的。 客户需要重新检查 JTAG 接头连接、如果一切正常、则检查电路板上所有 JTAG 信号(从器件引脚到 JTAG 接头)的信号完整性。

    此致、

    Vivek Singh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    实际上、我使用的是 USB。 如何验证  JTAG 信号的信号完整性 ?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     我假设您使用的是客户电路板、并使用一些 TI 设计作为参考。 您是否尝试过多个电路板、以查看问题是否出在所有电路板上、或者仅在某些特定电路板上、而这些电路板可能存在制造问题。 如果您在所有电路板上都遇到问题、请再次查看原理图以确保一切都正确。

    此致、

    Vivek Singh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我只有一个板。 带扩展坞的实验套件。 控制。  

    *卡 F28388D (www.ti.com/.../TMDSCNCD28388D)

    * TMDSHSECDOCK (www.ti.com/.../TMDSHSECDOCK)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    请为 C2000器件供电。

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/888411/tmdscncd28379d-trouble-connecting-a-new-controlcard/3285839#3285839

    此致、
    Cody  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好朋友、


    我为 C2000器件供电。 我连接了扩展坞并尝试通过 J17连接器供电、但它无法正常工作。 然后、我尝试将 Micro USB-B 连接器连接到 controlCARD 的 J8、但它仍然无法正常工作。

    电源 只有[LED D1]和[LED D2:A]在电路板中亮起。

        2.找到微型 USB 连接器后,计算机上不会出现任何问题,LED 指示灯不亮,也不会发出声音。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    亚历山大

    如果它以前正常工作、但没有更改配置、则连接突然断开、则电路板可能会损坏。 我发现这些板极具 ESD 耐受性、但看到客户损坏了它们。 由于连接到 controlCARD 的其他电路、电路板通常也会受到 EOS 的损坏。

    如果您有兴趣了解发生了什么故障、我建议首先调查 VDDIO 和 VDD 测试点、看看它们是否具有正确的电压。 如果 LDO 或 C2000器件变热、则可能其中一个器件出现故障。

    此致、
    Cody  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    实际上、在某些点、电压与板上显示的电压不同。

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    亚历山大

    我不理解以下陈述、请澄清您是否需要回复。 "板"是什么意思? 电压何时不同?

    [引用 userid="452912" url="~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/999015/tms320f28388d-error-when-configuring-target/3708402 #3708402"]在某些点、电压与板上显示的电压不同。

    PS、我建议断开连接到 controlCARD 或集线站的任何外部电路。

    此致、
    Cody  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我测量了电路板上的电压、其中一个电压与电路板上的电压不匹配。

    电源 我不知道" VDDIO 和 VDD"在哪里  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    亚历山大

    这些测试点连接到 VDD 和 VDDIO、有关每个测试点连接到什么的完整说明、请参考原理图。 原理图位于 C2000Ware:C:\ti\c2000\C2000Ware_3_03_00_00\boards\controlCARDs\TMDSCNCD28388D\Rev.B 中

    您似乎损坏了一些东西、可能是短的或部分短的。 它可以是3.3V 稳压器、也可以是连接到3.3V 电源轨的器件。 如果您尝试调试失败的"受热后"是最好的方法。 无论组件是热的、通常 都会灌入意外的电流、请注意、如果3.3V 稳压器仍在工作、即使不是短路的原因、它也会很热。 这是因为它将提供尽可能多的电流、以尝试将电源轨电压拉至3.3V。

    此致、
    Cody