This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:TMS320F28035PAGT 和 SE555DR#39;s ESD、MM 和 CDM

Guru**** 2387080 points
Other Parts Discussed in Thread: TMS320F28035, SE555
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1000655/tms320f28035-tms320f28035pagt-and-se555dr-s-esd-mm-and-cdm

器件型号:TMS320F28035
主题中讨论的其他器件:SE555

是否有人可以提供 TMS320F28035PAGT 和 SE555DR 的 PDF 报告

  • ESD (HBM mm CDM) HBM--人体放电模式--最小2kV
    MM --机器模式--最小200V
    CDM充电设备模式--最小1KV
     

谢谢