This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Code Composer Studio
您好!
我正在使用3个 CLA 任务处理一个项目、当代码达到一个重要的大小时、我开始出现错误:对于 Cla1Prog、"内存不足"、因此我将链接器命令文件中 RAMLS0的大小从0x800更改为0xE50、并相应地更改了 RAMLS1以减小其大小。 现在可以编译程序并将其复制到 f280049闪存、但 CLA 未运行、我为 RAMLS1减小了 RAMLS2提供了更大的空间、因为 RAMLS1是暂存区、但 CLA 尚不工作、如果我在3个 CLA 任务之一中注释代码、 CLA 正在运行、但我仍然能够让 CLA 为其中的3个运行。
可能会发生什么情况? 我有什么问题吗?
感谢你的帮助