This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F28379D:通过来自栅极驱动器(UCC21710)和 PWM 脉冲序列的 eCAP 模块测量直流总线

Guru**** 2748565 points

Other Parts Discussed in Thread: UCC21710, C2000WARE, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1173156/launchxl-f28379d-measure-dc-bus-via-the-ecap-module-from-gate-driver-ucc21710-pwm-pulse-train

器件型号:LAUNCHXL-F28379D
主题中讨论的其他器件:UCC21710C2000WARESysConfig

您好!

我们想使用来自 UCC21710生成的 PWM 脉冲序列的 eCAP 模块测量直流总线。我们需要对 eCAP 模块进行一些澄清。

首先、eCAP 能否测量400kHz PWM 脉冲序列的占空比?我问这个问题、因为查看 c2000ware 中的示例项目、我发现它正在测量几 kHz 的 PWM 脉冲序列。

我们尝试模拟同一个示例,但在较高的频率下,但随着我们增加 PWM 频率,占空比计算不断恶化。 变量 衍生 DT 是根据 eCAP 模块计算得出的结果。

  

__interrupt void INT_myECAP0_ISR(void)
{
    ecap_counter++;
    cap1_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_1);    //1st raising edge
    cap2_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_2);    //1st falling edge
    cap3_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_3);    //2nd raising edge
    cap4_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_4);    //2nd falling edge
    derivedDT = (float)(cap2_count-cap1_count)/(cap3_count-cap1_count);
    ECAP_reArm(myECAP0_BASE);
    ECAP_clearGlobalInterrupt(myECAP0_BASE);
    ECAP_clearInterrupt(myECAP0_BASE, ECAP_ISR_SOURCE_CAPTURE_EVENT_4);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP4);

}

在10kHz 时:

100kHz 时的频率

500kHz 时:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、AK、

    我将看到我能否再现您看到的内容、并在明天一天结束后尽快回复您!

    谢谢、

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、AK、

    我无法再现您在更高频率 PWM 下获得的占空比差异。

    这是随附的用于我的设置的代码。 我将其基于 C2000Ware 中 ECAP 示例2的内容。  

    这里还有一个屏幕截图、展示了我在500kHz 时获得的推导占空比。

    //#############################################################################
    //
    // FILE:    ecap_capture_pwm.c
    //
    // TITLE:   Capture ePWM3.
    //
    //! \addtogroup driver_example_list
    //! <h1>eCAP Capture PWM Example</h1>
    //!
    //! This example configures ePWM3A for:
    //! - Up count mode
    //! - Period starts at 500 and goes up to 8000
    //! - Toggle output on PRD
    //!
    //! eCAP1 is configured to capture the time between rising
    //! and falling edge of the ePWM3A output.
    //!
    //! \b External \b Connections \n
    //! - eCAP1 is on GPIO16
    //! - ePWM3A is on GPIO4
    //! - Connect GPIO4 to GPIO16.
    //!
    //! \b Watch \b Variables \n
    //! - \b ecap1PassCount - Successful captures.
    //! - \b ecap1IntCount - Interrupt counts.
    //
    //#############################################################################
    //
    // $Release Date: $
    // $Copyright:
    // Copyright (C) 2013-2022 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //#############################################################################
    
    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"
    
    //
    // Defines
    //
    #define PWM3_TIMER_MIN     100U
    #define PWM3_TIMER_MAX     8000U
    #define EPWM_TIMER_UP      1U
    #define EPWM_TIMER_DOWN    0U
    
    //
    // Globals
    //
    uint32_t ecap1IntCount;
    uint32_t ecap1PassCount;
    uint32_t epwm3TimerDirection;
    volatile uint16_t cap1Count;
    volatile uint16_t cap2Count;
    volatile uint16_t cap3Count;
    volatile uint16_t cap4Count;
    volatile uint16_t epwm3PeriodCount;
    float derivedDT;
    //
    // Function Prototypes
    //
    void error(void);
    void initECAP(void);
    void initEPWM(void);
    __interrupt void ecap1ISR(void);
    
    //
    // Main
    //
    void main(void)
    {
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Disable pin locks and enable internal pullups.
        //
        Device_initGPIO();
    
        //
        // Initialize PIE and clear PIE registers. Disables CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        //
        // Configure GPIO4/5 as ePWM3A/3B
        //
        GPIO_setPadConfig(4, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_4_EPWM3A);
        GPIO_setPadConfig(5, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_5_EPWM3B);
    
        //
        // Configure GPIO 16 as eCAP input
        //
        XBAR_setInputPin(XBAR_INPUT7, 16);
        GPIO_setPinConfig(GPIO_16_GPIO16);
        GPIO_setDirectionMode(16, GPIO_DIR_MODE_IN);
        GPIO_setQualificationMode(16, GPIO_QUAL_ASYNC);
    
        //
        // Interrupts that are used in this example are re-mapped to ISR functions
        // found within this file.
        //
        Interrupt_register(INT_ECAP1, &ecap1ISR);
    
        //
        // Configure ePWM and eCAP
        //
        initEPWM();
        initECAP();
    
        //
        // Initialize counters:
        //
        cap2Count = 0U;
        cap3Count = 0U;
        cap4Count = 0U;
        ecap1IntCount = 0U;
        ecap1PassCount = 0U;
        epwm3PeriodCount = 0U;
    
        //
        // Enable interrupts required for this example
        //
        Interrupt_enable(INT_ECAP1);
    
        //
        // Enable Global Interrupt (INTM) and Real time interrupt (DBGM)
        //
        EINT;
        ERTM;
    
        //
        // Loop forever. Suspend or place breakpoints to observe the buffers.
        //
        for(;;)
        {
           NOP;
        }
    }
    
    //
    // initEPWM - Configure ePWM
    //
    void initEPWM()
    {
        //
        // Disable sync(Freeze clock to PWM as well)
        //
        SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    
        //
        // Configure ePWM
        //       Counter runs in up-count mode.
        //       Action qualifier will toggle output on period match
        //
        EPWM_setTimeBaseCounterMode(EPWM3_BASE, EPWM_COUNTER_MODE_UP);
        EPWM_setTimeBasePeriod(EPWM3_BASE, PWM3_TIMER_MIN);
        EPWM_setPhaseShift(EPWM3_BASE, 0U);
        EPWM_setCounterCompareShadowLoadMode(EPWM3_BASE,
                                             EPWM_COUNTER_COMPARE_A,
                                             EPWM_COMP_LOAD_ON_CNTR_ZERO);
    
        EPWM_setCounterCompareValue(EPWM3_BASE, EPWM_COUNTER_COMPARE_A,
                                    PWM3_TIMER_MIN >> 1);
        EPWM_setActionQualifierAction(EPWM3_BASE,
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_HIGH,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
        EPWM_setActionQualifierAction(EPWM3_BASE,
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_LOW,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
        EPWM_setClockPrescaler(EPWM3_BASE,
                               EPWM_CLOCK_DIVIDER_1,
                               EPWM_HSCLOCK_DIVIDER_2);
    
        epwm3TimerDirection = EPWM_TIMER_UP;
    
        //
        // Enable sync and clock to PWM
        //
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    }
    
    //
    // initECAP - Configure eCAP
    //
    void initECAP()
    {
        //
        // Disable ,clear all capture flags and interrupts
        //
        ECAP_disableInterrupt(ECAP1_BASE,
                              (ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
                               ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
                               ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
                               ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
                               ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
                               ECAP_ISR_SOURCE_COUNTER_PERIOD   |
                               ECAP_ISR_SOURCE_COUNTER_COMPARE));
        ECAP_clearInterrupt(ECAP1_BASE,
                            (ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
                             ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
                             ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
                             ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
                             ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
                             ECAP_ISR_SOURCE_COUNTER_PERIOD   |
                             ECAP_ISR_SOURCE_COUNTER_COMPARE));
    
        //
        // Disable CAP1-CAP4 register loads
        //
        ECAP_disableTimeStampCapture(ECAP1_BASE);
    
        //
        // Configure eCAP
        //    Enable capture mode.
        //    One shot mode, stop capture at event 4.
        //    Set polarity of the events to rising, falling, rising, falling edge.
        //    Set capture in time difference mode.
        //    Select input from XBAR7.
        //    Enable eCAP module.
        //    Enable interrupt.
        //
        ECAP_stopCounter(ECAP1_BASE);
        ECAP_enableCaptureMode(ECAP1_BASE);
    
        ECAP_setCaptureMode(ECAP1_BASE, ECAP_ONE_SHOT_CAPTURE_MODE, ECAP_EVENT_4);
    
        ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_1, ECAP_EVNT_RISING_EDGE);
        ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_2, ECAP_EVNT_FALLING_EDGE);
        ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_3, ECAP_EVNT_RISING_EDGE);
        ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_4, ECAP_EVNT_FALLING_EDGE);
    
        ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_4);
    
        XBAR_setInputPin(XBAR_INPUT7, 16);
    
        ECAP_enableLoadCounter(ECAP1_BASE);
        ECAP_setSyncOutMode(ECAP1_BASE, ECAP_SYNC_OUT_SYNCI);
        ECAP_startCounter(ECAP1_BASE);
        ECAP_enableTimeStampCapture(ECAP1_BASE);
        ECAP_reArm(ECAP1_BASE);
    
        ECAP_enableInterrupt(ECAP1_BASE, ECAP_ISR_SOURCE_CAPTURE_EVENT_4);
    }
    
    //
    // eCAP 1 ISR
    //
    __interrupt void ecap1ISR(void)
    {
        //
        // Get the capture counts. Each capture should be 4x the ePWM count
        // because of the ePWM clock dividers.
        //
        uint32_t tb_ctr_ecap = ECAP_getTimeBaseCounter(ECAP1_BASE);
        cap1Count = ECAP_getEventTimeStamp(ECAP1_BASE, ECAP_EVENT_1);    //1st raising edge
        cap2Count = ECAP_getEventTimeStamp(ECAP1_BASE, ECAP_EVENT_2);    //1st falling edge
        cap3Count = ECAP_getEventTimeStamp(ECAP1_BASE, ECAP_EVENT_3);    //2nd raising edge
        cap4Count = ECAP_getEventTimeStamp(ECAP1_BASE, ECAP_EVENT_4);    //2nd falling edge
        derivedDT = (float)(cap2Count-cap1Count)/(cap3Count-cap1Count);
    
        //
        // Compare the period value with the captured count
        //
        epwm3PeriodCount = EPWM_getTimeBasePeriod(EPWM3_BASE);
    
        ecap1IntCount++;
    
        //
        // Keep track of the ePWM direction and adjust period accordingly to
        // generate a variable frequency PWM.
        //
    
        //
        // Count correct captures
        //
        ecap1PassCount++;
    
        //
        // Clear interrupt flags for more interrupts.
        //
        ECAP_clearInterrupt(ECAP1_BASE,ECAP_ISR_SOURCE_CAPTURE_EVENT_4);
        ECAP_clearGlobalInterrupt(ECAP1_BASE);
    
        //
        // Start eCAP
        //
        ECAP_reArm(ECAP1_BASE);
    
        //
        // Acknowledge the group interrupt for more interrupts.
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP4);
    }
    
    //
    // error - Error function
    //
    void error()
    {
        ESTOP0;
    }
    

    如果您仍遇到任何问题、请告诉我!

    最棒的

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ryan、

    你是否尝试在飞行中改变占空比,对我来说,它一直在波动。

    如果没有太多问题、请尝试以下设置并检查:

    PWM 生成基于 C2000WARE 中位于(\C2000Ware_4_01_00_00\driverlib\f2837xd\examples\cpu1\ePWM)的示例"ePWM_ex11_configure_signal"。

    可以动态更改结构"pwmSignal"、我将 GPIO0和 GPIO61连接在一起、GPIO0生成 PWM (使用 PWM1A)、并将 GPIO61配置为 eCAP。  只需在 main 中调用 ePWM_configureSignal (base、&pwmSignal)即可更新 PWM 值。

    /*
     * ecap_test.c
     *
     *  Created on: 18-Nov-2022
     *      Author: AK
     *
     *  Connect GPIO0 to GPIO 61
     */
    #include "ecap_test.h"
    
    uint32_t pwm_counter = 0;
    uint32_t ecap_counter = 0;
    uint32_t cap1_count = 0;
    uint32_t cap2_count = 0;
    uint32_t cap3_count = 0;
    uint32_t cap4_count = 0;
    
    float32_t derivedDT = 0.0;
    
    EPWM_SignalParams pwmSignal = {
                                   50000,                       //!< Desired Signal Frequency(in Hz)
                                   0.5f,                        //!< Desired ePWMxA Signal Duty
                                   0.5f,                        //!< Desired ePWMxB Signal Duty
                                   true,                        //!< Invert ePWMxB Signal if true
                                   DEVICE_SYSCLK_FREQ,          //!< SYSCLK Frequency(in Hz)
                                   SYSCTL_EPWMCLK_DIV_2,        //!< EPWM Clock Divider
                                   EPWM_COUNTER_MODE_UP_DOWN,   //!< Time Base Counter Mode
                                   EPWM_CLOCK_DIVIDER_1,        //!< Time Base Counter Clock Divider
                                   EPWM_HSCLOCK_DIVIDER_1       //!< Time Base Counter HS Clock Divider
    };
    //__interrupt void pwmISR(void)
    //{
    //    pwm_counter++;
    //    EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);
    //    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
    //}
    __interrupt void INT_myECAP0_ISR(void)
    {
        ecap_counter++;
        cap1_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_1);    //1st raising edge
        cap2_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_2);    //1st falling edge
        cap3_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_3);    //2nd raising edge
        cap4_count = ECAP_getEventTimeStamp(myECAP0_BASE, ECAP_EVENT_4);    //2nd falling edge
        derivedDT = (float)(cap2_count-cap1_count)/(cap3_count-cap1_count);
        ECAP_reArm(myECAP0_BASE);
        ECAP_clearGlobalInterrupt(myECAP0_BASE);
        ECAP_clearInterrupt(myECAP0_BASE, ECAP_ISR_SOURCE_CAPTURE_EVENT_4);
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP4);
    
    }
    
    void HAL_setupECAP()
    {
        // GPIO61->ECAP1
        GPIO_setMasterCore(61, GPIO_CORE_CPU1);
        GPIO_setPinConfig(GPIO_61_GPIO61);
        GPIO_setPadConfig(61, GPIO_PIN_TYPE_PULLUP);
        GPIO_setQualificationMode(61, GPIO_QUAL_ASYNC);
    }
    
    void pwm_init(uint32_t base)
    {
        // GPIO0->EPWM1A->UH_M1
        GPIO_setMasterCore(0, GPIO_CORE_CPU1);
        GPIO_setPinConfig(GPIO_0_EPWM1A);
        GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
    
        // GPIO1->EPWM1B->UL_M1
        GPIO_setMasterCore(1, GPIO_CORE_CPU1);
        GPIO_setPinConfig(GPIO_1_EPWM1B);
        GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
    
        EPWM_configureSignal(base, &pwmSignal);
        EPWM_setSyncOutPulseMode(base, EPWM_SYNC_OUT_PULSE_ON_COUNTER_ZERO);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
        //Interrupt_enable(INT_EPWM1);
    }
    void pwm_update_duty(uint32_t base)
    {
        switch (rec_data)
        {
        case 232:   //up arrow
        {
            pwmSignal.dutyValA += 0.05f;
            pwmSignal.dutyValB += 0.05f;
            rec_data = 0;
        }
            break;
        case 244:   //down arrow
        {
            pwmSignal.dutyValA -= 0.05f;
            pwmSignal.dutyValB -= 0.05f;
            rec_data = 0;
        }
            break;
        default:
            break;
        }
        if (pwmSignal.dutyValA > 1.0f)
        {
            pwmSignal.dutyValA = 0.99f;
        }
        else if (pwmSignal.dutyValA < 0)
        {
            pwmSignal.dutyValA = 0;
        }
        if (pwmSignal.dutyValB > 1.0f)
        {
            pwmSignal.dutyValB = 0.99f;
        }
        else if (pwmSignal.dutyValB < 0)
        {
            pwmSignal.dutyValB = 0;
        }
    
        EPWM_configureSignal(base, &pwmSignal);
    }
    
    //void HAL_setupMotorPWMs()
    //{
    //    float32_t switchingFreqKHz = 100.0;
    //    uint16_t halfPeriod = 0;
    //    EALLOW;
    //    // GPIO0->EPWM1A->UH_M1
    //    GPIO_setMasterCore(0, GPIO_CORE_CPU1);
    //    GPIO_setPinConfig(GPIO_0_EPWM1A);
    //    GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
    //
    //    // GPIO1->EPWM1B->UL_M1
    //    GPIO_setMasterCore(1, GPIO_CORE_CPU1);
    //    GPIO_setPinConfig(GPIO_1_EPWM1B);
    //    GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
    //
    //    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    //
    //    // Time Base SubModule Registers
    //    // set Immediate load
    //    EPWM_setPeriodLoadMode(EPWM1_BASE, EPWM_PERIOD_DIRECT_LOAD);
    //    EPWM_setTimeBasePeriod(EPWM1_BASE, 0);
    //    EPWM_setPhaseShift(EPWM1_BASE, 0);
    //    EPWM_setTimeBaseCounter(EPWM1_BASE, 0);
    //    EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP_DOWN);
    //
    //    EPWM_setClockPrescaler(EPWM1_BASE, EPWM_CLOCK_DIVIDER_1,
    //                           EPWM_HSCLOCK_DIVIDER_1);
    //
    //    // Counter Compare Submodule Registers
    //    // set duty 0% initially
    //    EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, 0);
    //    EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_A,
    //                                         EPWM_COMP_LOAD_ON_CNTR_ZERO);
    //
    //    // Action Qualifier SubModule Registers
    //    EPWM_setActionQualifierActionComplete(
    //            EPWM1_BASE,
    //            EPWM_AQ_OUTPUT_A,
    //            (EPWM_ActionQualifierEventAction) (EPWM_AQ_OUTPUT_LOW_UP_CMPA
    //                    | EPWM_AQ_OUTPUT_HIGH_DOWN_CMPA));
    //
    //    // Active high complementary PWMs - Set up the deadband
    //    EPWM_setRisingEdgeDeadBandDelayInput(EPWM1_BASE, EPWM_DB_INPUT_EPWMA);
    //    EPWM_setFallingEdgeDeadBandDelayInput(EPWM1_BASE, EPWM_DB_INPUT_EPWMA);
    //
    //    EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_RED, true);
    //    EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_FED, true);
    //    EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_RED,
    //                                  EPWM_DB_POLARITY_ACTIVE_HIGH);
    //    EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_FED,
    //                                  EPWM_DB_POLARITY_ACTIVE_LOW);
    //    /*
    //     * INFO: PWM Dead Time
    //     * Change this to change the pwm dead time.
    //     */
    //    EPWM_setRisingEdgeDelayCount(EPWM1_BASE, 50);
    //    EPWM_setFallingEdgeDelayCount(EPWM1_BASE, 50);
    //
    //    EPWM_enablePhaseShiftLoad(EPWM1_BASE);
    //
    //    EPWM_setCountModeAfterSync(EPWM1_BASE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
    //    // configure sync
    //    EPWM_setSyncOutPulseMode(EPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN);
    //
    //    //EPWM1->EWPM4
    //    SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM4,
    //                              SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    //
    /////-----------------------///
    //        halfPeriod = ((((DEVICE_SYSCLK_FREQ / 1000000U)/2.0)/switchingFreqKHz)*1000) / 2;     // 100MHz EPWMCLK
    //        EPWM_disablePhaseShiftLoad(EPWM1_BASE);
    //
    //        // sync "down-stream"
    //        EPWM_setSyncOutPulseMode(EPWM1_BASE,
    //                                 EPWM_SYNC_OUT_PULSE_ON_COUNTER_ZERO);
    //
    //        EPWM_setPhaseShift(EPWM1_BASE, 0);
    ////        EPWM_setPhaseShift(obj->pwmHandle[1], 2);
    ////        EPWM_setPhaseShift(obj->pwmHandle[2], 4);
    //
    //        EPWM_setTimeBasePeriod(EPWM1_BASE, halfPeriod);
    ////        EPWM_setTimeBasePeriod(obj->pwmHandle[1], halfPeriod);
    ////        EPWM_setTimeBasePeriod(obj->pwmHandle[2], halfPeriod);
    //
    /////-----------------------///
    //
    //    // Setting up link from EPWM to ADC
    //    // EPWM1/EPWM4 - Inverter currents at sampling frequency
    //    //               (@ PRD or @ (PRD&ZRO) )
    //    // Select SOC from counter at ctr = prd
    //    EPWM_setADCTriggerSource(EPWM1_BASE, EPWM_SOC_A,
    //                             EPWM_SOC_TBCTR_ZERO);
    //
    //    // Generate pulse on 1st event
    //    EPWM_setADCTriggerEventPrescale(EPWM1_BASE, EPWM_SOC_A, 1);
    //
    //    // Enable SOC on A group
    //    EPWM_enableADCTrigger(EPWM1_BASE, EPWM_SOC_A);
    //
    //    EPWM_setInterruptSource(EPWM1_BASE, EPWM_INT_TBCTR_ZERO);
    //    // Enable Interrupt Generation from the PWM module
    //    EPWM_enableInterrupt(EPWM1_BASE);
    //
    //    // This needs to be 1 for the INTFRC to work
    //    EPWM_setInterruptEventCount(EPWM1_BASE, 1);
    //
    //    // Clear ePWM Interrupt flag
    //    EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);
    //    EPWM_clearTripZoneFlag(EPWM1_BASE,
    //                           (EPWM_TZ_FLAG_OST | EPWM_TZ_FLAG_DCAEVT1));
    //
    //    Interrupt_register(INT_EPWM1, &pwmISR);
    //
    //    Interrupt_enable(INT_EPWM1);
    //    return;
    //}
    

    /*
     * ecap_test.h
     *
     *  Created on: 18-Nov-2022
     *      Author: AK
     */
    
    #ifndef ECAP_TEST_H_
    #define ECAP_TEST_H_
    
    #include "driverlib.h"
    #include "device.h"
    #include "board.h"
    #include "serial_driver.h"
    extern __interrupt void INT_myECAP0_ISR();
    //extern __interrupt void pwmISR();
    
    extern void HAL_setupECAP();
    extern void pwm_init(uint32_t);
    extern void pwm_update_duty(uint32_t);
    //extern void HAL_setupMotorPWMs();
    
    
    
    #endif /* ECAP_TEST_H_ */
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、AK、

    感谢您提供您的代码、我将查看此内容并在一天结束前回复。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、AK、

    因此、我一直在"Registers"选项卡(在 CCS 中)中更改 PWM 频率、以查看是否看到任何更改。

    这是 PWM 处于50kHz 时的情况:

    200KHz 时的 PWM:

      500KHz 时的 PWM 

    1MHz 时的 PWM:

    我仍然从上面屏幕截图中的 eCAP 计算中获得合理的占空比。

    您是否正在将 eCAP 同步到 ePWM? 您能否为我提供您的 ECAP 初始化代码? 这里是 eCAP 代码的初始化、我确保禁用 加载计数器、因为我没有与 ePWM 同步:

    //
    // Disable ,clear all capture flags and interrupts
    //
    ECAP_disableInterrupt(ECAP1_BASE,
                          (ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
                           ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
                           ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
                           ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
                           ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
                           ECAP_ISR_SOURCE_COUNTER_PERIOD   |
                           ECAP_ISR_SOURCE_COUNTER_COMPARE));
    ECAP_clearInterrupt(ECAP1_BASE,
                        (ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
                         ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
                         ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
                         ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
                         ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
                         ECAP_ISR_SOURCE_COUNTER_PERIOD   |
                         ECAP_ISR_SOURCE_COUNTER_COMPARE));
    
    //
    // Disable CAP1-CAP4 register loads
    //
    ECAP_disableTimeStampCapture(ECAP1_BASE);
    
    //
    // Configure eCAP
    //    Enable capture mode.
    //    One shot mode, stop capture at event 4.
    //    Set polarity of the events to rising, falling, rising, falling edge.
    //    Set capture in time difference mode.
    //    Select input from XBAR7.
    //    Enable eCAP module.
    //    Enable interrupt.
    //
    ECAP_stopCounter(ECAP1_BASE);
    ECAP_enableCaptureMode(ECAP1_BASE);
    
    ECAP_setCaptureMode(ECAP1_BASE, ECAP_ONE_SHOT_CAPTURE_MODE, ECAP_EVENT_4);
    
    ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_1, ECAP_EVNT_RISING_EDGE);
    ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_2, ECAP_EVNT_FALLING_EDGE);
    ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_3, ECAP_EVNT_RISING_EDGE);
    ECAP_setEventPolarity(ECAP1_BASE, ECAP_EVENT_4, ECAP_EVNT_FALLING_EDGE);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_1);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_2);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_3);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_4);
    
    XBAR_setInputPin(XBAR_INPUT7, 16);
    
    //    ECAP_enableLoadCounter(ECAP1_BASE);
    ECAP_disableLoadCounter(ECAP1_BASE);
    ECAP_setSyncOutMode(ECAP1_BASE, ECAP_SYNC_OUT_SYNCI);
    ECAP_startCounter(ECAP1_BASE);
    ECAP_enableTimeStampCapture(ECAP1_BASE);
    ECAP_reArm(ECAP1_BASE);
    
    ECAP_enableInterrupt(ECAP1_BASE, ECAP_ISR_SOURCE_CAPTURE_EVENT_4);

    需要注意的一点是、可以通过另一种方式解决占空比问题。  

    例如、如果我们有50kHz PWM 信号、并在向上计数模式下将 CMPA (999)设置为 TBPRD (1999)的一半。 我们预计占空比为50%。

    CAP1_COUNT = ECAP_getEventTimeStamp (ECAP1_BASE、ECAP_EVENT_1);//第一个上升沿

    CAP2_COUNT = ECAP_getEventTimeStamp (ECAP1_BASE、ECAP_EVENT_2);//第一个下降沿

    CAP1_COUNT 将在到达第一个上升沿时返回计数器值、而 CAP2_COUNT 将在到达下降沿时返回计数器值。

    当我们启用事件1和事件2上的计数器复位时、我们应该为这两个事件获得相同的计数器。 如下面的屏幕截图所示。 这意味着 PWM 以相同的计数打开/关闭。 这也意味着它具有50%的占空比。

    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_1);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_2);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_3);
    ECAP_enableCounterResetOnEvent(ECAP1_BASE, ECAP_EVENT_4);

    您可能会注意到 cap1_count 是2*CMPA (CMPA 是发生上升沿的地方),这是因为 ePWM 由 SYSCLK /2计时。 ECAP 由 SYSCLK 计时。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ryan、您好、感谢您提供如此详细的解释

    [引用 userid="531667" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1173156/launchxl-f28379d-measure-dc-bus-via-the-ecap-module-from-gate-driver-ucc21710-pwm-pulse-train/4418989 #4418989">您是否正在将 eCAP 同步到 ePWM? 您能否为我提供您的 ECAP 初始化代码? 这里是我的 eCAP 代码初始化、我确保禁用 加载计数器、因为我没有与 ePWM 同步:[/quot]

    这是我的初始化代码、我使用 SysConfig 生成初始代码、但设置看起来与您的初始化类似。在结构中、我计划将 eCAP 与 PWM 开关频率同步。 如果 我错了、但同步是通过从 PWM ISR 重新布防 eCAP 模块来完成的、请纠正我的问题?

    /*
     * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     */
    
    #include "board.h"
    
    void Board_init()
    {
    	EALLOW;
    
    	PinMux_init();
    	INPUTXBAR_init();
    	SYNC_init();
    	CPUTIMER_init();
    	ECAP_init();
    	GPIO_init();
    	SCI_init();
    	INTERRUPT_init();
    
    	EDIS;
    }
    
    void PinMux_init()
    {
    	// GPIO31 -> blue_led Pinmux
    	GPIO_setPinConfig(GPIO_31_GPIO31);
    	//
    	// SCIA -> mySCI0 Pinmux
    	//
    	GPIO_setPinConfig(GPIO_43_SCIRXDA);
    	GPIO_setPinConfig(GPIO_42_SCITXDA);
    
    }
    
    void CPUTIMER_init(){
    	//myCPUTIMER0 initialization 
    	CPUTimer_setEmulationMode(myCPUTIMER0_BASE, CPUTIMER_EMULATIONMODE_STOPAFTERNEXTDECREMENT);
    	CPUTimer_setPreScaler(myCPUTIMER0_BASE, 0U);
    	CPUTimer_setPeriod(myCPUTIMER0_BASE, 30000U);
    	CPUTimer_enableInterrupt(myCPUTIMER0_BASE);
    	CPUTimer_stopTimer(myCPUTIMER0_BASE);
    
    	CPUTimer_reloadTimerCounter(myCPUTIMER0_BASE);
    	CPUTimer_startTimer(myCPUTIMER0_BASE);
    }
    void ECAP_init(){
    
    	//myECAP0 initialization
        // Disable ,clear all capture flags and interrupts
        ECAP_disableInterrupt(myECAP0_BASE,
    		(ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
    		 ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
    		 ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
    		 ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
    		 ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
    		 ECAP_ISR_SOURCE_COUNTER_PERIOD   |
    		 ECAP_ISR_SOURCE_COUNTER_COMPARE));
    	ECAP_clearInterrupt(myECAP0_BASE,
    	  	(ECAP_ISR_SOURCE_CAPTURE_EVENT_1  |
    		ECAP_ISR_SOURCE_CAPTURE_EVENT_2  |
    		ECAP_ISR_SOURCE_CAPTURE_EVENT_3  |
    		ECAP_ISR_SOURCE_CAPTURE_EVENT_4  |
    		ECAP_ISR_SOURCE_COUNTER_OVERFLOW |
    		ECAP_ISR_SOURCE_COUNTER_PERIOD   |
    		ECAP_ISR_SOURCE_COUNTER_COMPARE));
    	// Disables time stamp capture.
    	ECAP_disableTimeStampCapture(myECAP0_BASE);
    	// Stops Time stamp counter.
    	ECAP_stopCounter(myECAP0_BASE);
    	// Sets eCAP in Capture mode.
    	ECAP_enableCaptureMode(myECAP0_BASE);
    	// Sets the capture mode.
    	ECAP_setCaptureMode(myECAP0_BASE,ECAP_ONE_SHOT_CAPTURE_MODE,ECAP_EVENT_4);
    	// Sets the Capture event prescaler.
    	ECAP_setEventPrescaler(myECAP0_BASE, 0U);
    	// Sets the Capture event polarity.
    	ECAP_setEventPolarity(myECAP0_BASE,ECAP_EVENT_1,ECAP_EVNT_RISING_EDGE);
    	ECAP_setEventPolarity(myECAP0_BASE,ECAP_EVENT_2,ECAP_EVNT_FALLING_EDGE);
    	ECAP_setEventPolarity(myECAP0_BASE,ECAP_EVENT_3,ECAP_EVNT_RISING_EDGE);
    	ECAP_setEventPolarity(myECAP0_BASE,ECAP_EVENT_4,ECAP_EVNT_FALLING_EDGE);
    	// Configure counter reset on events 
    	ECAP_disableCounterResetOnEvent(myECAP0_BASE,ECAP_EVENT_1);
    	ECAP_disableCounterResetOnEvent(myECAP0_BASE,ECAP_EVENT_2);
    	ECAP_disableCounterResetOnEvent(myECAP0_BASE,ECAP_EVENT_3);
    	ECAP_enableCounterResetOnEvent(myECAP0_BASE,ECAP_EVENT_4);	
    	// Sets a phase shift value count.
    	ECAP_setPhaseShiftCount(myECAP0_BASE,0U);
    	// Disable counter loading with phase shift value.
    	ECAP_disableLoadCounter(myECAP0_BASE);
    	// Configures Sync out signal mode.
    	ECAP_setSyncOutMode(myECAP0_BASE,ECAP_SYNC_OUT_SYNCI);
    	// Configures emulation mode.
    	ECAP_setEmulationMode(myECAP0_BASE,ECAP_EMULATION_STOP);
    
    	// Starts Time stamp counter for myECAP0.
    	ECAP_startCounter(myECAP0_BASE);
    	// Enables time stamp capture for myECAP0.
    	ECAP_enableTimeStampCapture(myECAP0_BASE);
    	// Re-arms the eCAP module for myECAP0.
    	ECAP_reArm(myECAP0_BASE);
    
    	// Enables interrupt source for myECAP0.
    	ECAP_enableInterrupt(myECAP0_BASE,(ECAP_ISR_SOURCE_CAPTURE_EVENT_4));
    
    }
    void GPIO_init(){
    		
    	//blue_led initialization
    	GPIO_setDirectionMode(blue_led, GPIO_DIR_MODE_OUT);
    	GPIO_setPadConfig(blue_led, GPIO_PIN_TYPE_STD);
    	GPIO_setMasterCore(blue_led, GPIO_CORE_CPU1);
    	GPIO_setQualificationMode(blue_led, GPIO_QUAL_SYNC);
    	GPIO_writePin(blue_led, 0);
    }
    void INPUTXBAR_init(){
    	
    	//myINPUTXBAR0 initialization
    	XBAR_setInputPin(XBAR_INPUT7, 61);
    }
    void INTERRUPT_init(){
    	
    	// Interrupt Setings for INT_myECAP0
    	Interrupt_register(INT_myECAP0, &INT_myECAP0_ISR);
    	Interrupt_enable(INT_myECAP0);
    	
    	// Interrupt Setings for INT_mySCI0_RX
    	Interrupt_register(INT_mySCI0_RX, &INT_mySCI0_RX_ISR);
    	Interrupt_enable(INT_mySCI0_RX);
    	
    	// Interrupt Setings for INT_mySCI0_TX
    	Interrupt_register(INT_mySCI0_TX, &INT_mySCI0_TX_ISR);
    	Interrupt_enable(INT_mySCI0_TX);
    }
    
    void SCI_init(){
    	
    	//mySCI0 initialization
    	SCI_clearInterruptStatus(mySCI0_BASE, SCI_INT_RXFF | SCI_INT_TXFF | SCI_INT_FE | SCI_INT_OE | SCI_INT_PE | SCI_INT_RXERR | SCI_INT_RXRDY_BRKDT | SCI_INT_TXRDY);
    	SCI_clearOverflowStatus(mySCI0_BASE);
    
    	SCI_disableFIFO(mySCI0_BASE);
    	SCI_resetChannels(mySCI0_BASE);
    
    	SCI_setConfig(mySCI0_BASE, DEVICE_LSPCLK_FREQ, mySCI0_BAUDRATE, (SCI_CONFIG_WLEN_8|SCI_CONFIG_STOP_ONE|SCI_CONFIG_PAR_NONE));
    	SCI_disableLoopback(mySCI0_BASE);
    	SCI_performSoftwareReset(mySCI0_BASE);
    	SCI_enableInterrupt(mySCI0_BASE, SCI_INT_RXRDY_BRKDT);
    	SCI_enableModule(mySCI0_BASE);
    }
    void SYNC_init(){
    	SysCtl_setSyncOutputConfig(SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT);
    	// For EPWM1, the sync input is: SYSCTL_SYNC_IN_SRC_EXTSYNCIN1
    	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM4, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM7, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM10, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_ECAP1, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    	SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_ECAP4, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
    	// SOCA
    	SysCtl_enableExtADCSOCSource(0);
    	// SOCB
    	SysCtl_enableExtADCSOCSource(0);
    }
    

    [引用 userid="531667" URL"~/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1173156/launchxl-f28379d-measure-dc-bus-via-the-ecap-module-from-gate-driver-ucc21710-pwm-pulse-train/4418989 #4418989">当我们启用计数器在事件1和事件2上复位时,我们应该得到相同的计数器。 如下面的屏幕截图所示。 这意味着 PWM 以相同的计数打开/关闭。 这也意味着它具有50%的占空比。[/报价]

    我看到、基本上我们只需等待事件1和2、然后检查两个时间计数之间的偏差以测量占空比...这里的优势是我们不需要等待所有4个事件发生?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、AK、

    当你为 eCAP 启用负载计数器时、同步完成。 如果您计划将 eCAP 用作非对称 PWM 信号、则可以启用负载计数器。 但是、如果您计划使用 eCAP 来捕获占空比、请确保禁用负载计数器。

    '一旦启用、eCAP 模块等待1-4 (由停止值定义)个捕捉事件、然后再冻结这两个事件
    Mod4计数器和 CAP1-4寄存器的内容(时间戳)。
    重新布防为另一个捕捉序列准备 eCAP 模块。 此外、重新布防会清除(归零)
    Mod4计数器、并允许再次加载 CAP1-4寄存器、前提是 CAPLDEN 位被置位。"

    第二点、是的、您回答正确!

    希望这对您有所帮助。

    最棒的

    Ryan Ma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢 Ryan,我终于能够让它在高频下工作了。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    没问题!

    此致、

    Ryan Ma