This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025C:CAN 接收帧配置、发送正常(轮询模式)

Guru**** 2531480 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1190425/tms320f280025c-can-receive-frame-configuration-transmit-is-ok-polling-mode

器件型号:TMS320F280025C

各位专家、您好!

我需要您的帮助^对于我的程序、我想配置我目前开发第一个节点的电路板和第二个节点的具有峰值 CAN 探针的 PC 的 CAN 通信。

此时我想发送一个对象并接收第二个对象 、但接下来我需要配置更多对象。 传输很好、我看到我的帧从板到 PC、但 Opposit 在 CAN_IF2DATA /  CAN_IF2DATB 中不起作用 、我从未看到数据。

我正在尝试在传入 ID 上设置一个筛选器、我只想接受我从 PC 发送的 ID、在这种情况下、ID = 0x010为标准格式。

我在您的文档和论坛上做了大量研究、但没有成功。  我尝试通过不加掩码而不成功地在 ID 上进行配置、因此我不确定问题是否来自 ID 的筛选(以查看我是否没有犯错)

因此我配置:  

CANARegs.CAN_IF2MSK.bit.MSK = 0x1FFFFFFF;

CanaRegs.CAN_IF2ARB.bit.ID =(msgid << 18);

CANaRegs.CAN_IF2CMD.bit.DIR = 0;

CANaRegs.CAN_IF2ARB.bit.Dir = 0;

这行是正确的? 对我来说是的,但是……

您可以看到屏幕截图和我的代码:  

void can_init(void)
{
    EALLOW;
    /// Configure CANA_RX
    GpioCtrlRegs.GPAPUD.bit.GPIO3 = 1;     /// Disable the pullup on GPIO3
    GpioCtrlRegs.GPAGMUX1.bit.GPIO3 = 3;    /// To define mux position, mux position equal GPAGMUX(2bits) - GPAMUX(2bits) 0 to 15 number, here mux position equal 14 so GPAGMUX1 = 11b and GPAMUX1 = 10b.
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 2;    /// GPIO3 = CANA_RX, see pin attributes documentation for mux position.
    GpioCtrlRegs.GPADIR.bit.GPIO3 = 0;     /// GPIO3 = input
    GpioCtrlRegs.GPAINV.bit.GPIO3 = 0;   /// Not inverted GPIO input

    /// Configure CANA_TX
    GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1;     /// Disable the pullup on GPIO2
    GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;     /// GPIO2 = output
    GpioCtrlRegs.GPAODR.bit.GPIO2 = 0;     /// Normal output not open drain
    GpioCtrlRegs.GPAQSEL1.bit.GPIO2 = 0;   /// Synchronous
    GpioCtrlRegs.GPAGMUX1.bit.GPIO2 = 3;   /// To define mux position, mux position equal GPBGMUX(2bits) - GPBMUX(2bits) 0 to 15 number, here mux position equal 14 so GPAGMUX1 = 11b and GPAMUX1 = 10b.
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 2;    /// GPIO2 = CANA_TX, see pin attributes documentation  for mux position.
    /// Place CAN controller in init state, regardless of previous state.
    /// This will put controller in idle, and allow the message object RAM to be programmed.
    /// CAN module ignore bus activity during configuration.
    CanaRegs.CAN_CTL.bit.Init = 1;
    /// CAN software reset.
    CanaRegs.CAN_CTL.bit.SWR = 1;
    /// The CPU has write access to the configuration register.
    CanaRegs.CAN_CTL.bit.CCE = 1;
    /// Clock and timing bit configuration
    ClkCfgRegs.CLKSRCCTL2.bit.CANABCLKSEL = 0;
    /// Set up the bit rate for the CAN bus, with 250kbit/s.
    /// Bit time (Tq) = 8
    /// Bit clock prescaler = 49dec = 0x31
    /// Propagation segment (Tq) = 1
    /// Phase segment 1 (Tq) = 3dec = 0x3
    /// Phase segment 2 (Tq) = 2dec = 0x2
    /// Synchronization jump width (Tq) = 2dec = 0x2
    /// Sampling point = 62.5%
    /// Oscillator tolerance = 1.48%
    /// Set Baud rate prescaler.
    CanaRegs.CAN_BTR.bit.BRP = 0x31;
    /// Synchronization jump width.
    CanaRegs.CAN_BTR.bit.SJW = 0x2;
    /// Time segment before the sample point.
    CanaRegs.CAN_BTR.bit.TSEG1 = 0x3;
    /// Time segment after the sample point.
    CanaRegs.CAN_BTR.bit.TSEG2 = 0x2;

    /// CAN module processes messages normally
    CanaRegs.CAN_CTL.bit.Init = 0;

    //setupMessageObject(1, 0x100, MSG_OBJ_TYPE_TRANSMIT);
    setupMessageObject(2, 0x010, MSG_OBJ_TYPE_RECEIVE);
    EDIS;
}

...
    /// Receive message
    else
    {
        /// Wait for busy bit to clear.
        while(CanaRegs.CAN_IF2CMD.bit.Busy)
        {
        }
        /// Clear and Write out the registers to program the message object.
        CanaRegs.CAN_IF2CMD.all = 0;
        CanaRegs.CAN_IF2MSK.all = 0;
        CanaRegs.CAN_IF2ARB.all = 0;
        CanaRegs.CAN_IF2MCTL.all = 0;

        /// Use mask (Msk, MXtd and Mdir) for acceptance filtering.
        CanaRegs.CAN_IF2MCTL.bit.UMask = 1;
        /// Set the data length since this is set for all transfers. This is also a single transfer and not a FIFO transfer so set EOB bit.
        /// Data frame has 8 data bytes
        CanaRegs.CAN_IF2MCTL.bit.DLC = 9;
        /// The message object is a single message object or the last message object in a FIFO buffer.
        CanaRegs.CAN_IF2MCTL.bit.EoB = 1;
        /// Extended identifier bit has no effect on the acceptance filtering (standard mode is used).
        CanaRegs.CAN_IF2MSK.bit.MXtd = 0;
        /// The message direction bit has no effect on the acceptance filtering.
        CanaRegs.CAN_IF2MSK.bit.MDir = 0;
        /// The corresponding bit in the identifier of the message object is used for acceptance filtering.
        CanaRegs.CAN_IF2MSK.bit.Msk = 0x1FFFFFFF;

        /// IF command registers configure and initiate the transfer between the IF register sets and the message RAM.
        /// Set the Control, Mask, and Arb bit so that they get transferred to the message object.
        /// The message control bits will be transferred from the IF2 register set to the message object.
        CanaRegs.CAN_IF2CMD.bit.Control = 1;
        /// The arbitration bits will be transferred from the IF2 register set to the message object.
        CanaRegs.CAN_IF2CMD.bit.Arb = 1;
        /// The mask bits (Identifier mask + Mdir + MXtd) will be transferred from the IF2 register to the message object.
        CanaRegs.CAN_IF2CMD.bit.Mask = 1;
        /// Read message object (mail box).
        CanaRegs.CAN_IF2CMD.bit.DIR = 0;
        /// Transfer data to message object RAM
        CanaRegs.CAN_IF2CMD.bit.MSG_NUM = objID;

        /// Arbitration
        /// Transmit direction = receive, a remote frame with the identifier of this message object is transmitted.
        CanaRegs.CAN_IF2ARB.bit.Dir = 0;
        /// Set Message ID.
        CanaRegs.CAN_IF2ARB.bit.ID = (msgID << 18);
        /// Standard identifier is used for this message object.
        CanaRegs.CAN_IF2ARB.bit.Xtd = 0;
        /// Mail box is enabled after mask configuration.
        CanaRegs.CAN_IF2ARB.bit.MsgVal = 1;
    }
}

Read data function
bool receive_CAN_message()
{
    bool status;

    /// Detect for mail box number 2 (receive)
    //if(CanaRegs.CAN_NDAT_21 == 2)
    //{
        // Set the Message Data A, Data B to be read on request for data from the message object.
        CanaRegs.CAN_IF2CMD.bit.DATA_A = 1;
        CanaRegs.CAN_IF2CMD.bit.DATA_B = 1;

        // Wait for busy bit to clear.
        while(CanaRegs.CAN_IF2CMD.bit.Busy)
        {
        }

        // Read out the data from the CAN registers.
        uint16_t index;
        for(index = 0; index < 8; index++)
        {
            switch(index)
            {
                case 0:
                    rx_data[index] = CanaRegs.CAN_IF2DATA.bit.Data_0;
                break;
                case 1:
                    rx_data[index] = CanaRegs.CAN_IF2DATA.bit.Data_1;
                break;
                case 2:
                    rx_data[index] = CanaRegs.CAN_IF2DATA.bit.Data_2;
                break;
                case 3:
                    rx_data[index] = CanaRegs.CAN_IF2DATA.bit.Data_3;
                break;
                case 4:
                    rx_data[index] = CanaRegs.CAN_IF2DATB.bit.Data_4;
                break;
                case 5:
                    rx_data[index] = CanaRegs.CAN_IF2DATB.bit.Data_5;
                break;
                case 6:
                    rx_data[index] = CanaRegs.CAN_IF2DATB.bit.Data_6;
                break;
                case 7:
                    rx_data[index] = CanaRegs.CAN_IF2DATB.bit.Data_7;
                break;
            }
        }

        status = true;
    /*}
    else
    {
        status = false;
    }*/
    // Clear New Data Flag
    CanaRegs.CAN_IF2CMD.bit.TxRqst = 1;

    return(status);
}

谢谢

Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Damien:

    您能澄清几个问题吗?  我假设您 没有使用中断来触发帧接收。  上述代码(第55行)中的注释 显示///接收消息、但后续代码似乎正在配置消息对象。  有一个函数 READ_CAN_MESSAGE(),但对 NewDat 的检查注释掉。  您如何检查邮箱2的新数据是否出现?

    此致、

    Joseph

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joseph、  

    您是我希望使用轮询模式触发火焰接收而不是中断的原因。 我在第55行的注释不适合它是用于接收邮件的邮箱配置。 邮箱1我配置用于传输消息、但这里不显示、因为它可以正常工作、邮箱2用于接收。  

    我使用 CAN_ndat_21第113行测试邮件 box2的新数据是否出现,但该寄存器始终为0,因此我认为接收时没有帧会通过掩码过滤器 no 触发?  

    如果我不想使用这一个读功能,只需验证一个邮箱配置的 Candata 寄存器,它将不起作用? 当我配置更多接收邮箱时、将进行此检测。  

    我的邮箱2配置良好,可以接收消息吗?  

    我不明白为什么 CAN_ndat_21等于0? 我认为触发器不起作用。  

    谢谢

    Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Damien:

    您能否移动以下语句:

    CANARegs.CAN_IF2CMD.bit.DATA_A = 1;
    CANARegs.CAN_IF2CMD.bit.DATA_B = 1;

    这当前位于先前已定义消息对象2以查看其是否起作用的例程中的 Receive_CAN_message 中?  我在您发送的快照中看不到这些位在 IF2CMD 寄存器中设置。

    此致、

    Joseph

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joseph、

    我正在调试中取得进展、但我遇到了一个问题。 我仍然配置了 ID 为0x100 (µC -> PC)的发送帧和 ID 为0x010 (PC ->µC)的另一帧。 我想在 CAN_IF1DATx 寄存器中查看 ID 为0x100的帧上发送的数据、并在第二个 CAN_IF2DAT 缓冲区中查看 ID 为0x010的 PC 发送的数据。 但在调试器模式下、我在 CAN_IF1DAT 和 CAN_IF2DAT 中看到 Tx 中 ID 0x100上传输的相同数据。 我不访问 CAN_Rx 中帧0x010的数据。
    为什么在 CAN_IF2DAT 中看不到 CAN_Rx 中的数据? 我肯定在配置上犯了错误?
    I defined CAN_IF1CMD.bit.DIR = 1 (发送方向)
                    CAN_IF1ARB.bit.Dir = 1 (发送方向)
                    CAN_IF1ARB.bit.ID = 0x100 << 18
                    CAN_IF1CMD.bit.MSG_NUM = 1

                    CAN_IF1CMD DIR = 0 (接收方向)
                    CAN_IF1ARB.bit.Dir = 0 (接收方向)
                    CAN_IF1ARB.bit.ID = 0x010 << 18
                    CAN_IF1CMD.bit.MSG_NUM = 2

    我看不到问题、可以帮我吗?

    #include "f28002x_device.h"
    #include "HPTS100_can.h"
    
    uint16_t rx_data[8];
    
    void can_init(void)
    {
        EALLOW;
        /// Configure CANA_RX
        GpioCtrlRegs.GPAPUD.bit.GPIO3 = 1;     /// Disable the pullup on GPIO3
        GpioCtrlRegs.GPAGMUX1.bit.GPIO3 = 3;    /// To define mux position, mux position equal GPAGMUX(2bits) - GPAMUX(2bits) 0 to 15 number, here mux position equal 14 so GPAGMUX1 = 11b and GPAMUX1 = 10b.
        GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 2;    /// GPIO3 = CANA_RX, see pin attributes documentation for mux position.
        GpioCtrlRegs.GPADIR.bit.GPIO3 = 0;     /// GPIO3 = input
        GpioCtrlRegs.GPAINV.bit.GPIO3 = 0;   /// Not inverted GPIO input
    
        /// Configure CANA_TX
        GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1;     /// Disable the pullup on GPIO2
        GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;     /// GPIO2 = output
        GpioCtrlRegs.GPAODR.bit.GPIO2 = 0;     /// Normal output not open drain
        GpioCtrlRegs.GPAQSEL1.bit.GPIO2 = 0;   /// Synchronous
        GpioCtrlRegs.GPAGMUX1.bit.GPIO2 = 3;   /// To define mux position, mux position equal GPBGMUX(2bits) - GPBMUX(2bits) 0 to 15 number, here mux position equal 14 so GPAGMUX1 = 11b and GPAMUX1 = 10b.
        GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 2;    /// GPIO2 = CANA_TX, see pin attributes documentation  for mux position.
        /// Place CAN controller in init state, regardless of previous state.
        /// This will put controller in idle, and allow the message object RAM to be programmed.
        /// CAN module ignore bus activity during configuration.
        CanaRegs.CAN_CTL.bit.Init = 1;
        /// The CPU has write access to the configuration register.
        CanaRegs.CAN_CTL.bit.CCE = 1;
        /// Clock and timing bit configuration
        ClkCfgRegs.CLKSRCCTL2.bit.CANABCLKSEL = 0;
        /// Set up the bit rate for the CAN bus, with 250kbit/s.
        /// Bit time (Tq) = 8
        /// Bit clock prescaler = 49dec = 0x31
        /// Propagation segment (Tq) = 1
        /// Phase segment 1 (Tq) = 3dec = 0x3
        /// Phase segment 2 (Tq) = 2dec = 0x2
        /// Synchronization jump width (Tq) = 2dec = 0x2
        /// Sampling point = 62.5%
        /// Oscillator tolerance = 1.48%
        /// Set Baud rate prescaler.
        CanaRegs.CAN_BTR.bit.BRP = 0x31;
        /// Synchronization jump width.
        CanaRegs.CAN_BTR.bit.SJW = 0x2;
        /// Time segment before the sample point.
        CanaRegs.CAN_BTR.bit.TSEG1 = 0x3;
        /// Time segment after the sample point.
        CanaRegs.CAN_BTR.bit.TSEG2 = 0x2;
    
        /// CAN module processes messages normally
        CanaRegs.CAN_CTL.bit.Init = 0;
    
        setupMessageObject(1, 0x100, MSG_OBJ_TYPE_TRANSMIT);
        setupMessageObject(2, 0x010, MSG_OBJ_TYPE_RECEIVE);
        EDIS;
    }
    
    void setupMessageObject(uint32_t objID, uint32_t msgID, msgObjType msgType)
    {
        if(msgType == MSG_OBJ_TYPE_TRANSMIT)
        {
            /// Use Shadow variable for IF1CMD. IF1CMD should be written to in single 32-bit write.
            union CAN_IF1CMD_REG CAN_IF1CMD_SHADOW;
            /// Wait for busy bit to clear.
            while(CanaRegs.CAN_IF1CMD.bit.Busy)
            {
            }
            /// Clear and Write out the registers to program the message object.
            CAN_IF1CMD_SHADOW.all = 0;
            CanaRegs.CAN_IF1MSK.all = 0;
            CanaRegs.CAN_IF1ARB.all = 0;
            CanaRegs.CAN_IF1MCTL.all = 0;
    
            /// Set the Control, Mask, and Arb bit so that they get transferred to the message object.
            /// The message control bits will be transferred from the IF1 register set to the message object.
            CAN_IF1CMD_SHADOW.bit.Control = 1;
            /// The arbitration bits will be transferred from the IF1 register set to the message object.
            CAN_IF1CMD_SHADOW.bit.Arb = 1;
            /// The mask bits (Identifier mask + Mdir + MXtd) will be transferred from the IF1 register to the message object.
            CAN_IF1CMD_SHADOW.bit.Mask = 1;
            /// Transfer direction is transferred to the message object : write
            CAN_IF1CMD_SHADOW.bit.DIR = 1;
    
            /// Transmit direction
            CanaRegs.CAN_IF1ARB.bit.Dir = 1;
            /// Set Message ID.
            CanaRegs.CAN_IF1ARB.bit.ID = (msgID << 18);
            /// Mail box is enabled.
            CanaRegs.CAN_IF1ARB.bit.MsgVal = 1;
    
            /// Set the data length since this is set for all transfers. This is also a single transfer and not a FIFO transfer so set EOB bit.
            /// Data frame has 8 data bytes
            CanaRegs.CAN_IF1MCTL.bit.DLC = 9;
            /// The message object is a single message object or the last message object in a FIFO buffer.
            CanaRegs.CAN_IF1MCTL.bit.EoB = 1;
    
            /// Transfer data to message object RAM
            CAN_IF1CMD_SHADOW.bit.MSG_NUM = objID;
            CanaRegs.CAN_IF1CMD.all = CAN_IF1CMD_SHADOW.all;
        }
        else
        {
            /// Use Shadow variable for IF1CMD. IF1CMD should be written to in single 32-bit write.
            union CAN_IF2CMD_REG CAN_IF2CMD_SHADOW;
            /// Wait for busy bit to clear.
            while(CanaRegs.CAN_IF2CMD.bit.Busy)
            {
            }
            /// Clear and Write out the registers to program the message object.
            CAN_IF2CMD_SHADOW.all = 0;
            CanaRegs.CAN_IF2MSK.all = 0;
            CanaRegs.CAN_IF2ARB.all = 0;
            CanaRegs.CAN_IF2MCTL.all = 0;
    
            /// Set the Control, Mask, and Arb bit so that they get transferred to the message object.
            /// The message control bits will be transferred from the IF1 register set to the message object.
            CAN_IF2CMD_SHADOW.bit.Control = 1;
            /// The arbitration bits will be transferred from the IF1 register set to the message object.
            CAN_IF2CMD_SHADOW.bit.Arb = 1;
            /// The mask bits (Identifier mask + Mdir + MXtd) will be transferred from the IF1 register to the message object.
            CAN_IF2CMD_SHADOW.bit.Mask = 1;
            /// Transfer direction is transferred to the message object : read
            CAN_IF2CMD_SHADOW.bit.DIR = 0;
    
            /// Receive direction
            CanaRegs.CAN_IF2ARB.bit.Dir = 0;
            /// Set Message ID.
            CanaRegs.CAN_IF2ARB.bit.ID = (msgID << 18);
            /// Mail box is enabled.
            CanaRegs.CAN_IF2ARB.bit.MsgVal = 1;
    
            /// Set the data length since this is set for all transfers. This is also a single transfer and not a FIFO transfer so set EOB bit.
            /// Data frame has 8 data bytes
            CanaRegs.CAN_IF2MCTL.bit.DLC = 9;
            /// The message object is a single message object or the last message object in a FIFO buffer.
            CanaRegs.CAN_IF2MCTL.bit.EoB = 1;
    
            /// Transfer data to message object RAM
            CAN_IF2CMD_SHADOW.bit.MSG_NUM = objID;
            CanaRegs.CAN_IF2CMD.all = CAN_IF2CMD_SHADOW.all;
        }
    }
    
    void send_CAN_message()
    {
        // Use Shadow variable for IF1CMD. IF1CMD should be written to in single 32-bit write.
        union CAN_IF1CMD_REG CAN_IF1CMD_SHADOW;
    
        // Wait for busy bit to clear.
        while(CanaRegs.CAN_IF1CMD.bit.Busy)
        {
        }
    
        CanaRegs.CAN_IF1DATA.bit.Data_0 = 0x1;
        CanaRegs.CAN_IF1DATA.bit.Data_1 = 0x2;
        CanaRegs.CAN_IF1DATA.bit.Data_2 = 0x3;
        CanaRegs.CAN_IF1DATA.bit.Data_3 = 0x4;
        CanaRegs.CAN_IF1DATB.bit.Data_4 = 0x5;
        CanaRegs.CAN_IF1DATB.bit.Data_5 = 0x6;
        CanaRegs.CAN_IF1DATB.bit.Data_6 = 0x7;
        CanaRegs.CAN_IF1DATB.bit.Data_7 = 0x8;
    
        // Set Direction to write and set DATA-A/DATA-B to be transfered to message object
        CAN_IF1CMD_SHADOW.all = 0;
        CAN_IF1CMD_SHADOW.bit.DIR = 1;
        CAN_IF1CMD_SHADOW.bit.DATA_A = 1;
        CAN_IF1CMD_SHADOW.bit.DATA_B = 1;
    
        // Set Tx Request Bit
        CAN_IF1CMD_SHADOW.bit.TXRQST = 1;
    
        // Transfer the message object to the message object specified by objID.
        CAN_IF1CMD_SHADOW.bit.MSG_NUM = 1;//obj id;
        CanaRegs.CAN_IF1CMD.all = CAN_IF1CMD_SHADOW.all;
    }
    
    void receive_CAN_message()
    {
        //CanaRegs.CAN_IF2CMD.bit.Arb = 1;
        CanaRegs.CAN_IF2CMD.all = 0;
        CanaRegs.CAN_IF2CMD.bit.Control = 1;
        CanaRegs.CAN_IF2CMD.bit.DATA_A = 1;
        CanaRegs.CAN_IF2CMD.bit.DATA_B = 1;
        /// Obj ID
        CanaRegs.CAN_IF2CMD.bit.MSG_NUM = 2;
    
        // Wait for busy bit to clear.
        while(CanaRegs.CAN_IF2CMD.bit.Busy)
        {
        }
    
        if(CanaRegs.CAN_IF2MCTL.bit.NewDat == 1)
        {
            rx_data[0] = CanaRegs.CAN_IF2DATA.bit.Data_0;
            rx_data[1] = CanaRegs.CAN_IF2DATA.bit.Data_1;
            rx_data[2] = CanaRegs.CAN_IF2DATA.bit.Data_2;
            rx_data[3] = CanaRegs.CAN_IF2DATA.bit.Data_3;
            rx_data[4] = CanaRegs.CAN_IF2DATB.bit.Data_4;
            rx_data[5] = CanaRegs.CAN_IF2DATB.bit.Data_5;
            rx_data[6] = CanaRegs.CAN_IF2DATB.bit.Data_6;
            rx_data[7] = CanaRegs.CAN_IF2DATB.bit.Data_7;
        }
        CanaRegs.CAN_IF2CMD.bit.TxRqst = 1;
        // Transfer the message object to the message object IF register.
        //CanaRegs.CAN_IF2CMD.bit.MSG_NUM = 2;
    }
    

    谢谢

    Damien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    最佳屏幕截图

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Damien:

    很高兴听到您在代码方面取得了良好的进展。  我看到您开始接收 CAN 帧。  在随附的代码上、您可以参考影子寄存器。  我们的 F28002x 示例目前使用 driverlib 代码编写、您似乎使用 了一些旧代码来引用不同类型 CAN (eCAN)的影子寄存器。  F28002x DCAN 中没有影子寄存器。  我只想确保您正在对正确的 CAN 寄存器进行编程。  您能否澄清一下您在 F28002x 上使用过哪些影子寄存器?

    谢谢、

    Joseph