This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F2800137:如何将 EPWM A 和 B 极性更改为 DRV8323连接驱动器

Guru**** 2988540 points

Other Parts Discussed in Thread: LAUNCHXL-F2800137

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1322800/tms320f2800137-how-to-change-epwm-a-and-b-polarity-to-drv8323-gatedriver

器件型号:TMS320F2800137
主题中讨论的其他器件:LAUNCHXL-F2800137

大家好!

我一直在针对特定的电机控制应用使用 LAUNCHXL-F2800137和 BOOSTXL-DRV8323S 进行测试。

现在、一名硬件工程师基于上述板制作了定制 PCB、但来回翻转某些内容。

在 LAUNCHXL 板上、ePWM A 输出进入 DRV8323S 的高侧相位输入。 有关阐释、请参阅下表。

名称 LAUNCHXL 引脚
HIN A GPIO 0 (EPWM1 A)
LIN A GPIO 1 (EPWM1 B)
HIN B GPIO 2 (EPWM2 A)
线 B GPIO 3 (EPWM2 B)
HIN C GPIO 10 (EPWM6 A)
LIN C GPIO 11 (EPWM6 B)

现在、在我们的硬件上、A 和 B 通道被切换(错误)。

问题是、如何在电机控制实验的 hal.c 文件中的 PWM 设置中更改两个通道的极性? 我已将代码放在下面。 我认为它与死区发生器有关。 但我不确定。 有人能说明这两个渠道是如何相互关联的吗? 因为在 PWM 写入函数中、相同的比较值被写入通道 A 和 B。

提前感谢!

PWM 设置功能:

void HAL_setupPWMs(HAL_MTR_Handle handle)
{
    HAL_MTR_Obj *obj = (HAL_MTR_Obj *)handle;
    uint16_t cnt;

    uint16_t pwmPeriodCycles = (uint16_t)(MOTORCONFIG_PWM_TBPRD_NUM);
    uint16_t numPWMTicksPerISRTick = MOTORCONFIG_NUM_PWM_TICKS_PER_ISR_TICK;

    // disable the ePWM module time base clock sync signal
    // to synchronize all of the PWMs
    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    // turns off the outputs of the EPWM peripherals which will put the power
    // switches into a high impedance state.
    EPWM_forceTripZoneEvent(obj->pwmHandle[0], EPWM_TZ_FORCE_EVENT_OST);
    EPWM_forceTripZoneEvent(obj->pwmHandle[1], EPWM_TZ_FORCE_EVENT_OST);
    EPWM_forceTripZoneEvent(obj->pwmHandle[2], EPWM_TZ_FORCE_EVENT_OST);

    for(cnt=0; cnt<3; cnt++)
    {
        // setup the Time-Base Control Register (TBCTL)
        EPWM_setTimeBaseCounterMode(obj->pwmHandle[cnt],
                                    EPWM_COUNTER_MODE_UP_DOWN);

        EPWM_disablePhaseShiftLoad(obj->pwmHandle[cnt]);

        EPWM_setPeriodLoadMode(obj->pwmHandle[cnt], EPWM_PERIOD_DIRECT_LOAD);

        EPWM_enableSyncOutPulseSource(obj->pwmHandle[cnt],
                                      EPWM_SYNC_OUT_PULSE_ON_SOFTWARE);

        EPWM_setClockPrescaler(obj->pwmHandle[cnt], EPWM_CLOCK_DIVIDER_1,
                                 EPWM_HSCLOCK_DIVIDER_1);

        EPWM_setCountModeAfterSync(obj->pwmHandle[cnt],
                                   EPWM_COUNT_MODE_UP_AFTER_SYNC);

        EPWM_setEmulationMode(obj->pwmHandle[cnt], EPWM_EMULATION_FREE_RUN);

        // setup the Timer-Based Phase Register (TBPHS)
        EPWM_setPhaseShift(obj->pwmHandle[cnt], 0);

        // setup the Time-Base Counter Register (TBCTR)
        EPWM_setTimeBaseCounter(obj->pwmHandle[cnt], 0);

        // setup the Time-Base Period Register (TBPRD)
        // set to zero initially
        EPWM_setTimeBasePeriod(obj->pwmHandle[cnt], 0);

        // setup the Counter-Compare Control Register (CMPCTL)
        EPWM_setCounterCompareShadowLoadMode(obj->pwmHandle[cnt], EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);
        EPWM_setCounterCompareShadowLoadMode(obj->pwmHandle[cnt], EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO);
        EPWM_setCounterCompareShadowLoadMode(obj->pwmHandle[cnt], EPWM_COUNTER_COMPARE_C, EPWM_COMP_LOAD_ON_CNTR_ZERO);
        EPWM_setCounterCompareShadowLoadMode(obj->pwmHandle[cnt], EPWM_COUNTER_COMPARE_D, EPWM_COMP_LOAD_ON_CNTR_ZERO);

        // setup the Action-Qualifier Output A Register (AQCTLA)
        EPWM_setActionQualifierAction(obj->pwmHandle[cnt],
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_HIGH,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);

        EPWM_setActionQualifierAction(obj->pwmHandle[cnt],
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_HIGH,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);

        EPWM_setActionQualifierAction(obj->pwmHandle[cnt],
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_LOW,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);

        EPWM_setActionQualifierAction(obj->pwmHandle[cnt],
                                      EPWM_AQ_OUTPUT_A,
                                      EPWM_AQ_OUTPUT_LOW,
                                      EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);



        // setup the Dead-Band Generator Control Register (DBCTL)
        EPWM_setDeadBandDelayMode(obj->pwmHandle[cnt], EPWM_DB_RED, true);
        EPWM_setDeadBandDelayMode(obj->pwmHandle[cnt], EPWM_DB_FED, true);

        // select EPWMA as the input to the dead band generator
        EPWM_setRisingEdgeDeadBandDelayInput(obj->pwmHandle[cnt],
                                             EPWM_DB_INPUT_EPWMA);

        // configure the right polarity for active high complementary config.
        EPWM_setDeadBandDelayPolarity(obj->pwmHandle[cnt],
                                      EPWM_DB_RED,
                                      EPWM_DB_POLARITY_ACTIVE_HIGH);
        EPWM_setDeadBandDelayPolarity(obj->pwmHandle[cnt],
                                      EPWM_DB_FED,
                                      EPWM_DB_POLARITY_ACTIVE_LOW);

        // setup the Dead-Band Rising Edge Delay Register (DBRED)
        EPWM_setRisingEdgeDelayCount(obj->pwmHandle[cnt], MTR1_PWM_DBRED_CNT);

        // setup the Dead-Band Falling Edge Delay Register (DBFED)
        EPWM_setFallingEdgeDelayCount(obj->pwmHandle[cnt], MTR1_PWM_DBFED_CNT);

        // setup the PWM-Chopper Control Register (PCCTL)
        EPWM_disableChopper(obj->pwmHandle[cnt]);

        // setup the Trip Zone Select Register (TZSEL)
        EPWM_disableTripZoneSignals(obj->pwmHandle[cnt], HAL_TZSEL_SIGNALS_ALL);
    }

    // setup the Event Trigger Selection Register (ETSEL)
    EPWM_setInterruptSource(obj->pwmHandle[0], EPWM_INT_TBCTR_ZERO);

    EPWM_enableInterrupt(obj->pwmHandle[0]);

    EPWM_setADCTriggerSource(obj->pwmHandle[0],
                             EPWM_SOC_A, EPWM_SOC_TBCTR_D_CMPC);

    EPWM_enableADCTrigger(obj->pwmHandle[0], EPWM_SOC_A);

    // setup the Event Trigger Prescale Register (ETPS)
    if(numPWMTicksPerISRTick > 15)
    {
        numPWMTicksPerISRTick = 15;
    }
    else if(numPWMTicksPerISRTick < 1)
    {
        numPWMTicksPerISRTick = 1;
    }

    EPWM_setInterruptEventCount(obj->pwmHandle[0], numPWMTicksPerISRTick);

    EPWM_setADCTriggerEventPrescale(obj->pwmHandle[0], EPWM_SOC_A,
                                    numPWMTicksPerISRTick);
    EPWM_setADCTriggerEventPrescale(obj->pwmHandle[0], EPWM_SOC_B,
                                    numPWMTicksPerISRTick);

    // setup the Event Trigger Clear Register (ETCLR)
    EPWM_clearEventTriggerInterruptFlag(obj->pwmHandle[0]);
    EPWM_clearADCTriggerFlag(obj->pwmHandle[0], EPWM_SOC_A);
    EPWM_clearADCTriggerFlag(obj->pwmHandle[0], EPWM_SOC_B);

    // since the PWM is configured as an up/down counter, the period register is
    // set to one-half of the desired PWM period
    EPWM_setTimeBasePeriod(obj->pwmHandle[0], pwmPeriodCycles);
    EPWM_setTimeBasePeriod(obj->pwmHandle[1], pwmPeriodCycles);
    EPWM_setTimeBasePeriod(obj->pwmHandle[2], pwmPeriodCycles);

    // write the PWM data value  for ADC trigger
    EPWM_setCounterCompareValue(obj->pwmHandle[0], EPWM_COUNTER_COMPARE_C, 10);

    return;
}

写入 PWM 函数:

//! \brief     Writes PWM data to the PWM comparators for motor control
//! \param[in] handle    The hardware abstraction layer (HAL) handle
//! \param[in] pPWMData  The pointer to the PWM data
static inline void
HAL_writePWMData(HAL_MTR_Handle handle, HAL_PWMData_t *pPWMData)
{
    HAL_MTR_Obj *obj = (HAL_MTR_Obj *)handle;

    float32_t period = (float32_t)(EPWM_getTimeBasePeriod(obj->pwmHandle[0]));

    uint16_t pwmCnt;

    for(pwmCnt=0; pwmCnt<3; pwmCnt++)
    {
      // compute the value
        float32_t V_pu = -pPWMData->Vabc_pu.value[pwmCnt];      // Negative
        float32_t V_sat_pu = __fsat(V_pu, 0.5, -0.5);           // -0.5~0.5
        float32_t V_sat_dc_pu = V_sat_pu + 0.5;                 // 0~1.0
        pPWMData->cmpValue[pwmCnt]  = (int16_t)(V_sat_dc_pu * period);  //

        if(pPWMData->cmpValue[pwmCnt] < pPWMData->minCMPValue)
        {
            pPWMData->cmpValue[pwmCnt] = pPWMData->minCMPValue;
        }

        // write the PWM data value
        EPWM_setCounterCompareValue(obj->pwmHandle[pwmCnt],
                                    EPWM_COUNTER_COMPARE_A,
                                    pPWMData->cmpValue[pwmCnt]);

        EPWM_setCounterCompareValue(obj->pwmHandle[pwmCnt],
                                    EPWM_COUNTER_COMPARE_B,
                                    pPWMData->cmpValue[pwmCnt]);
    }

    return;
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    PWM 死区子模块确实有针对此问题的内置选项!  DBCTL[OUTSWAP]寄存器以显式方式执行该函数。

    要启用该寄存器、插入以下代码:

    EPWM_setDeadBandOutputSwapMode(obj->pwmHandle[cnt], EPWM_DB_OUTPUT_A, true);

    EPWM_setDeadBandOutputSwapMode(obj->pwmHandle[cnt], EPWM_DB_OUTPUT_B, true);

    在 ePWM 配置期间、将此内容添加到您提供的第一个代码摘录的第99行附近。 这将切换全部3个 ePWM 的高/低侧。 希望这对您有所帮助!

    此致、
    杰森·奥斯博尔恩

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢! 我将必须在硬件上尝试、以验证它。 但是在阅读完函数标题后、我确实认为这正是我所需要的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    更新;我在硬件上对它进行了测试、它做了应有的工作! 再次感谢。

    以前;

    添加行后;