请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F2800157-Q1 主题中讨论的其他器件:UNIFLASH
工具与软件:
当我使用 uniflash 工具编程一个十六进制文件,我发现工具总是给我这个错误.
[2024/9/4 下午4:47:55] [INFO] C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... [2024/9/4 下午4:47:56] [INFO] C28xx_CPU1: GEL Output: ... DCSM Initialization Done ... [2024/9/4 下午4:47:56] [INFO] C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... [2024/9/4 下午4:47:57] [INFO] C28xx_CPU1: GEL Output: ... DCSM Initialization Done ... [2024/9/4 下午4:48:02] [ERROR] C28xx_CPU1: Error during Flash Programming. Address 0x00088000, FMSTAT (STATCMD on some devices) 0x00000101
[2024/9/4 下午4:48:02] [ERROR] C28xx_CPU1: Error during Flash Programming. Address 0x00088000, FMSTAT (STATCMD on some devices) 0x00000101