主题中讨论的其他器件:SysConfig
工具与软件:
Im 使用了 spi_ex3_external_loopback 示例并对其进行了修改、使 Im 在 SPIB 上仅传输16字节的数据、并通过手动控制 SPISTE 引脚。 代码如下:
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"
#include "f28003x_device.h"
//
//Macros
//
static inline void GPIO_SPI_FLASH_CS_CLEAR(void){
GpioDataRegs.GPACLEAR.bit.GPIO15 = 1;
}
static inline void GPIO_SPI_FLASH_CS_SET(void)
{
GpioDataRegs.GPASET.bit.GPIO15 = 1;
}
//
//Prototype
//
uint16_t spi_transmit_byte(uint16_t data_tx);
//
// Main
//
void main(void)
{
uint16_t i;
uint16_t TxData_SPIB[] = {0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F};
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Board initialization
//
Board_init();
//
// Loop forever. Suspend or place breakpoints to observe the buffers.
//
// for(i = 0; i < 16; i++)
// {
// spi_transmit_byte(TxData_SPIB[i]);
// }
spi_transmit_multi_byte(TxData_SPIB, 16);
//
// Loop forever
//
while(1);
}
uint16_t spi_transmit_byte(uint16_t data_tx)
{
uint16_t ret_val = 0U;
/* Shift the data to MSbyte as the 8bit setting discards the LSbyte and transmits only MSbyte
* Assert the CS low
* Transmit the data and dummy read
* Drive the CS high
*/
data_tx = data_tx << 8U;
GPIO_SPI_FLASH_CS_CLEAR();
SPI_writeDataNonBlocking(SPIB_BASE, data_tx);
SPI_readDataNonBlocking(SPIB_BASE);
GPIO_SPI_FLASH_CS_SET();
return ret_val;
}
uint16_t spi_transmit_multi_byte(uint16_t *buffer_tx, uint16_t len)
{
uint16_t i, data_tx;
uint16_t ret_val = 0U;
/* Shift each data to be sent to MSbyte as the 8bit setting discards the LSbyte and transmits only MSbyte
* Assert the CS low
* Transmit all the data while dummy reading at the same time
* Drive the CS high
*/
GPIO_SPI_FLASH_CS_CLEAR();
for (i = 0; i < len; i++)
{
data_tx = buffer_tx[i] << 8U;
SPI_writeDataNonBlocking(SPIB_BASE, data_tx);
SPI_readDataNonBlocking(SPIB_BASE);
}
GPIO_SPI_FLASH_CS_SET();
return ret_val;
}
SysConfig 如下所示:

以下是 Im 在逻辑分析仪上观察到的情况:

我的问题是 、将 GPIO 用作 SPISTE 引脚会发生什么情况? Im 希望引脚 在整个 for 循环中保持低电平有效、直到传输完成。 我在这里遗漏了什么?