This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我将在 DisplayPort 应用中设计采用 DP159的电路。 从应用报告 SLLA358中、"在 X 模式下、DP159可以支持高达5.4Gbps (HBR2)的 DisplayPort 数据速率。"
我需要在 PCB 布局中确定长度匹配和阻抗匹配设置。 由于 DisplayPort 具有4个具有嵌入式时钟的数据通道、因此没有专用时钟通道、我应该在这些数据通道上使用5.4GHz 吗?
换言之,如果数据通道正在传输“010101...... "序列、等效频率为5.4GHz?
谢谢你
您能提供更多的解释或理论吗? 为什么在5.4Gbpts 数据速率下为2.7GHz?
谢谢你。