This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、TI 专家!
我正在使用:适用于1Gbps 介质转换器的 DP83TG720评估模块;并将其连接到 LAN8650 PHY
我知道、DP83TG720 PHY 的速度为 1Gbps 、速度为
LAN8650 PHY 的 速率为10兆位/秒
我无法建立这两个 PHY 之间的连接。
那么我的问题是:2个 PHY 的速度必须相同=>能够连接2个 PHY 吗?
另外、请给我一些有关连接2个 PHY 的指南:设置、...
非常感谢!
Dinh