请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8825 您好,TI:
参考DRV8825数据表,应用于每个绕组的最大RMS输出电流为1.75安有效值或2.5A峰值。
最大2.5A峰值是指以下其中一个电机绕组测量值的正电流还是负电流?
测量值是否低于1.36A峰值电流,且在DRV8825 2.5A峰值规格范围内?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.