请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8305 尊敬的各位:
我测试了DRV8305并有问题。
*我附加了测试文件
通道1:黄色= PVDD电压(=24V输入)
CH2:绿色= SHA电压
接通电源时,我认为SHA输出12V=24V/2。 不过,民政事务局局长的表现却是24V。
这是否是正确的行为?
此致,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.