This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
工具:CCS 12.7.1
大家好!
C.
有人 给我一个关于这个代码的手?
#include <msp430.h> #define MCLK_FREQ_MHZ 1 // MCLK = 1MHz void Software_Trim(); // Software Trim to get the best DCOFTRIM value void UARTConf(void); /** * main.c */ int main(void) { WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer __bis_SR_register(SCG0); // Disable FLL CSCTL3 = SELREF__REFOCLK; // Set REFO as FLL reference source CSCTL1 = DCOFTRIMEN | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_0;// DCOFTRIM=3, DCO Range = 1MHz CSCTL2 = FLLD_0 + 30; // DCODIV = 1MHz __delay_cycles(3); __bic_SR_register(SCG0); // Enable FLL Software_Trim(); // Software Trim to get the best DCOFTRIM value CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz // default DCODIV as MCLK and SMCLK source PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode // to activate previously configured port settings UARTConf(); __bis_SR_register(LPM3_bits|GIE); // Enter LPM3, interrupts enabled __no_operation(); // For debugger return 0; } void UARTConf(void) { // Configure UART pins P1SEL0 |= BIT4 | BIT5; // set 2-UART pin as second function // Configure UART UCA0CTLW0 |= UCSWRST; // Put eUSCI in reset UCA0CTLW0 |= UCSSEL__SMCLK; // Baud Rate calculation (infos in UG table 22-5) UCA0BR0 = 6; // 1000000/16/9600 = 6.51 UCA0BR1 = 0; UCA0MCTLW = 0x2000 | UCOS16 | UCBRF_8; // 1000000/16/9600 - INT(1000000/16/9600)=0.51 // UCBRFx = int (0.51*16) = 8; 16 bcz of UCOS16 // UCBRSx value = 0x20 UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt void USCI_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG)) { case USCI_NONE: break; case USCI_UART_UCRXIFG: while(!(UCA0IFG&UCTXIFG)); UCA0TXBUF = UCA0RXBUF; __no_operation(); break; case USCI_UART_UCTXIFG: break; case USCI_UART_UCSTTIFG: break; case USCI_UART_UCTXCPTIFG: break; default: break; } } void Software_Trim() { unsigned int oldDcoTap = 0xffff; unsigned int newDcoTap = 0xffff; unsigned int newDcoDelta = 0xffff; unsigned int bestDcoDelta = 0xffff; unsigned int csCtl0Copy = 0; unsigned int csCtl1Copy = 0; unsigned int csCtl0Read = 0; unsigned int csCtl1Read = 0; unsigned int dcoFreqTrim = 3; unsigned char endLoop = 0; do { CSCTL0 = 0x100; // DCO Tap = 256 do { CSCTL7 &= ~DCOFFG; // Clear DCO fault flag }while (CSCTL7 & DCOFFG); // Test DCO fault flag __delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock status (FLLUNLOCK) to be stable // Suggest to wait 24 cycles of divided FLL reference clock while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0)); csCtl0Read = CSCTL0; // Read CSCTL0 csCtl1Read = CSCTL1; // Read CSCTL1 oldDcoTap = newDcoTap; // Record DCOTAP value of last time newDcoTap = csCtl0Read & 0x01ff; // Get DCOTAP value of this time dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value if(newDcoTap < 256) // DCOTAP < 256 { newDcoDelta = 256 - newDcoTap; // Delta value between DCPTAP and 256 if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim--; CSCTL1 = (csCtl1Read & (~DCOFTRIM0)) | (dcoFreqTrim<<4); } } else // DCOTAP >= 256 { newDcoDelta = newDcoTap - 256; // Delta value between DCPTAP and 256 if(oldDcoTap < 256) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim++; CSCTL1 = (csCtl1Read & (~DCOFTRIM0)) | (dcoFreqTrim<<4); } } if(newDcoDelta < bestDcoDelta) // Record DCOTAP closest to 256 { csCtl0Copy = csCtl0Read; csCtl1Copy = csCtl1Read; bestDcoDelta = newDcoDelta; } }while(endLoop == 0); // Poll until endLoop == 1 CSCTL0 = csCtl0Copy; // Reload locked DCOTAP CSCTL1 = csCtl1Copy; // Reload locked DCOFTRIM while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked } // End of file
它只应该回显从连接到 GPS 模块的 RX 引脚接收到的数据。 我可以进行检查、中断没有触发、并且已经检查了导线电路。
感谢您的任何帮助!
你从 main ()返回,它关闭所有-包括中断。 您需要一个 while (1){}无限循环。
> __ bis_SR_register (LPM3_bits |GIE);//进入 LPM3、中断被启用
在 LPM3中、SMCLK 被关闭。 请尝试改用:
> __ bis_SR_register (LPM0_bits|GIE);//进入 LPM0、中断被启用
时钟请求系统在串行端口需要时不能启用 SMCLK? 这可能会因检测到起始位时的时钟启动延迟而导致时序问题。 这会导致数据错误、而不是完全缺少数据。
此外、ISR 不会导致从 LPM3退出、因此 main 中缺少 while (1)应该无关紧要。
我想知道代码是否会将其用于 UART init。 可能会卡在所有这些时钟系统的抖动中。 尝试使用调试器进行检查。
更新了:我移除了 J101接头的 RX/TX 引脚、现在触发 RX 中断。 但来自 GPS 的数据不回传。 我将使用逻辑分析仪来监控引脚。 还有其他建议吗?
你是否在 UCA0TXBUF = UCA0RXBUF 上放置了一个中断以确保你到达那里?
听起来 您想要通过 UCA0 Rx 侧接受 GPS 输出、然后通过 UCA0 Tx 侧将其回显到反向通道 UART (PC 终端)。
如果是、您应该(仅限)将 TXD 跳线放回 J101上。