请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28881 工具与软件:
您好、根据应用手册 slVaej3 (图5)、是否可能从降压/升压配置开始向 UCC28881添加反相输出? 在 Alternately 中、哪种是将15V 至48V 输入转换为+/-20V 输出(0.2A)的最佳解决方案?
谢谢
应用手册:

UCC28881数据表

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.