Other Parts Discussed in Thread: BQ25798, BQ25723
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25798 主题中讨论的其他器件: BQ25723
工具/软件:
您好:
我们正在寻找具有直通模式的9V VBUS 至2节3A 电池充电 iFET 降压/升压充电器。
请告诉我 BQ25798是否内置了直通模式或类似功能?
此致<
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.