请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS922051 工具/软件:
LED 驱动器团队、
IL 的(max)和 IL (peak)定义在数据表中不是100%清晰。 您是否有任何图片可以帮助您更详细地解释这一点?
此外、您建议用于以下目的的电感器值:
Vin = 24V
VLED = 17.1V
Fsw = 2 MHz
Iled = 1.1A
谢谢、
Darren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.