请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8865X-Q1 工具/软件:
您好、
有14个-500mA 需要提升 LED 驱动器芯片、电流预计为200 LED。
如果14个元件串联、则电压预计为49V、如果方案电压分为两种方式、则为25V。 请帮助推荐合适的产品,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
您好、
有14个-500mA 需要提升 LED 驱动器芯片、电流预计为200 LED。
如果14个元件串联、则电压预计为49V、如果方案电压分为两种方式、则为25V。 请帮助推荐合适的产品,谢谢~