请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61165 工具/软件:
可从数据表中设置的频率范围为5kHz 至100kHz。

是否可以在整个频率范围内将占空比设置为1%至100%?
(可以设置的占空比是否会根据该频率范围内的频率而变化?)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
可从数据表中设置的频率范围为5kHz 至100kHz。

是否可以在整个频率范围内将占空比设置为1%至100%?
(可以设置的占空比是否会根据该频率范围内的频率而变化?)