This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25619E:在低温下充电完成计时器不会翻倍

Guru**** 2387830 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1498202/bq25619e-top-off-timer-not-double-at-cool-temperature

器件型号:BQ25619E

工具/软件:

您好:

我将在低温(5°C)下对电池进行充电测试、并测量流入电池的电流。

编程的充电完成计时器为30分钟。

我预计在凉温下、安全计时器会减慢2、因此充电完成计时器也会减慢(1小时)。

但30分钟后充电仍然停止。

下面是我在充电停止之前读取的 I2C 寄存器:

进行登记 0x05
REG01 0x1A
REG02 0x8A
REG03 0x00
REG04 0x9D
REG05 0x8F
REG06 0x66
REG07 0x55
REG08 0x3C
REG09 0x03
REG0A 0x88
REG0B 0x44
REG0C 0xA5

您是否知道加注计时器在低温条件下不会变为1小时?

谢谢