请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8868Z-Q1 工具/软件:
在第8.2.3.2.1节的底部、最后一段指出"ILED = 2A、考虑效率为0.9"、列出了0.741A 的电感器电流最大值
在哪里以及如何得出该值0.741A 来实现最大电感电流?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
在第8.2.3.2.1节的底部、最后一段指出"ILED = 2A、考虑效率为0.9"、列出了0.741A 的电感器电流最大值
在哪里以及如何得出该值0.741A 来实现最大电感电流?