请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS552892 工具/软件:
你(们)好
客户在95%湿度下测试时发现输出异常 JEDEC 标准是 RH 85%、这是否意味着 TPS552892不会受到85%湿度下的外部湿度的影响?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.